Flash Layout for Dual-Image OAD¶
This section will describe the method for placing images in internal flash when using dual-image OAD.
Constraints and Requirements for Dual-Image¶
The following points must be considered for Dual-Image OAD applications:
The user application must be sufficiently small in order to fit into the flash layout system described below.
Only one operational user application image may be stored in flash at any time.
Internal Flash Memory Layout¶
The internal flash of the device contains the active application, the download application and the MCUboot bootloader. Each application’s role is defined below.
Application Name |
Description |
MCUboot bootloader |
|
Download application |
|
Active application |
|

The location of the download application varies depending on the flash size available for the selected device variant. This is done to maximize the active application space.
Refer to the linker command file (.cmd) define to further determine where precisely the each application is located.
Warning
The description above provides the starting flash layout for dual images.