EnergyTrace User Guide

EnergyTrace™ technology is a power analyzer tool for CCS that measures the application’s current consumption. The tool can be used stand-alone as a power profiling tool to help optimize the application for ultra-low-power consumption.

For further information regarding the EnergyTrace Tool, see the EnergyTrace Tool page. Additionally, please visit further EnergyTrace documentation at EnergyTrace overview.

EnergyTrace stand-alone Instructions

The following discusses the necessary steps to use EnergyTrace in stand-alone-mode on CC23xx LaunchPad. In stand-alone mode (EnergyTrace mode), the debugger is not active and the displayed current consumption is what to expect for the final application.

  1. Flash the target device with the application to be analyzed.

  2. Make sure no debug session is active and click the EnergyTrace Button as seen in Figure 193.

    ../_images/fig-energytrace-standalone-button.png

    Figure 193. Start EnergyTrace

  3. A dialog with instructions on how to use EnergyTrace Stand-alone Measurement Mode will pop-up. Click Proceed to continue.

  4. The first time EnergyTrace is being used within a CCS Workspace some settings needs to be set. In the EnergyTrace Window, click on the Advanced Menu icon and select Preferences, as Figure 194. shows.

    ../_images/fig-energytrace-preferences-button.png

    Figure 194. EnergyTrace Preferences menu

  5. Under Target Connection, set Connection to XDS110 and Voltage to 3300.0 mV. ET-HDR Range Selector shall be set to Low current, narrower range higher accuracy. If you want to save the captured data to a .cvs-file for further analysis, select Raw data to CSV file. You can also select the battery cell type the application will be using to get an estimated life time of the application. Click Ok to save the preferences.

    ../_images/fig-energytrace-standalone-settings.png

    Figure 195. EnergyTrace Settings

  6. Select how long you want to capture data by clicking the Select Measurement Duration button as in Figure 196.

    ../_images/fig-energytrace-standalone-time.png

    Figure 196. Select Measurement Duration

  7. To start capturing data, click the green play button.

    ../_images/fig-energytrace-standalone-start.png

    Figure 197. Start trace collection

  8. When EnergyTrace is finished capturing data, review the application’s power profile and have a closer look in the Current graph. Figure 198. shows a zoomed-in current graph of BLE advertising.

    ../_images/fig-energytrace-standalone-graph.png

    Figure 198. EnergyTrace Current Graph

Using EnergyTrace on a Modular Launchpad™ Design

Connect just the 3.3 V and GND lines.

../_images/Mod_LP_Config_2.png

Figure 199. Modular LP EnergyTrace stand-alone Configuration

Using EnergyTrace with an External Target

The power profile of an external target can be measured using EnergyTrace and a compatible debugger: an XDS110 ETHDR Debug Probe or a CC26x2R LaunchPad Kit (the debug probe is embedded on the LaunchPad board). In this section, we will use a CC26x2R LaunchPad to measure the power profile of a CC23xx LaunchPad.

Note

Other types of LaunchPad that include a XDS110 ETHDR Debug Probe may be used instead of CC26x2R LaunchPad

Before getting started, make sure the external target is already flashed with the application firmware to be tested.

The following steps are required to use EnergyTrace with an external target:

  1. Remove all the jumpers from the top row of the CC26x2R LaunchPad as shown in Figure 200..

  2. Use jumper wires to supply power to the CC23xx LaunchPad from the CC26x2R LaunchPad as shown below.

  3. At this point, connect only the CC26x2R LaunchPad to the PC via a USB cable. The external target will receive power from the CC26x2R LaunchPad.

  4. Follow the steps in EnergyTrace stand-alone Instructions to measure the power profile of the external target.

Tip

Ensure that only one CC26x2R LaunchPad is connected to the PC at a time to ensure the correct LaunchPad is automatically selected by EnergyTrace.

../_images/fig-energytrace-external-target-cc23xx.png

Figure 200. External Target Hardware Configuration

The above diagram shows the hardware setup required to use EnergyTrace to measure the power profile of the CC23xx LaunchPad.

Note

With the jumpers removed, a 10-pin JTAG cable can be connected to the external target for debugging purposes. If UART is required, jumper wires should be placed to connect the TX/RX lines of the external target to the CC26x2R LaunchPad.

Troubleshooting

  • If EnergyTrace is not able to properly setup remote controls for the device, try closing CCS, resetting your Evaluation Board and starting again.

  • The CC23xx or CC27xx does NOT support EnergyTrace++. Please refer to EnergyTrace Tool page for details.