Data Fields
LGPTimerLPF3_ChannelConf Struct Reference

LGPTimerLPF3 channel dependent pin configuration struct. More...

#include <LGPTimerLPF3.h>

Data Fields

uint8_t pin
 
uint8_t pinMux
 
uint8_t nPin
 
uint8_t nPinMux
 

Detailed Description

LGPTimerLPF3 channel dependent pin configuration struct.

LGPTimer struct used by the LGPTimerLPF3_HWAttrs.

Field Documentation

§ pin

uint8_t LGPTimerLPF3_ChannelConf::pin

Channel pin

§ pinMux

uint8_t LGPTimerLPF3_ChannelConf::pinMux

Channel pin mux

§ nPin

uint8_t LGPTimerLPF3_ChannelConf::nPin

Complementary channel pin

§ nPinMux

uint8_t LGPTimerLPF3_ChannelConf::nPinMux

Complementary channel pin mux


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale