![]() |
![]() |
AESCCMLPF3 Object. More...
#include <AESCCMLPF3.h>

Data Fields | |
| AESCommonLPF3_Object | common |
| const uint8_t * | aad |
| const uint8_t * | input |
| uint8_t * | output |
| const uint8_t * | nonce |
| uint8_t * | mac |
| volatile uint32_t | intermediateCounter [AES_IV_LENGTH_BYTES/4] |
| volatile uint32_t | intermediateTag [AES_TAG_LENGTH_BYTES/4] |
| AESCCM_CallbackFxn | callbackFxn |
| AESCCM_OperationUnion * | operation |
| size_t | inputLength |
| volatile size_t | inputCBCMACLengthRemaining |
| volatile size_t | inputCTRLengthRemaining |
| size_t | totalAADLength |
| size_t | totalDataLength |
| size_t | aadBytesProcessed |
| volatile size_t | totalCBCMACLengthRemaining |
| volatile size_t | totalCTRLengthRemaining |
| AESCCM_OperationType | operationType |
| uint8_t | bufferedAAD [2U] |
| uint8_t | bufferedAADLength |
| uint8_t | macLength |
| uint8_t | nonceLength |
| size_t | aadLength |
| volatile size_t | totalDataLengthRemaining |
| volatile size_t | totalAADLengthRemaining |
| int_fast16_t | hsmStatus |
| The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly. More... | |
| uint32_t | tempAssetID |
| bool | segmentedOperationInProgress |
AESCCMLPF3 Object.
The application must not access any member variables of this structure!
| AESCommonLPF3_Object AESCCMLPF3_Object::common |
| const uint8_t* AESCCMLPF3_Object::aad |
| const uint8_t* AESCCMLPF3_Object::input |
| uint8_t* AESCCMLPF3_Object::output |
| const uint8_t* AESCCMLPF3_Object::nonce |
| uint8_t* AESCCMLPF3_Object::mac |
| volatile uint32_t AESCCMLPF3_Object::intermediateCounter[AES_IV_LENGTH_BYTES/4] |
| volatile uint32_t AESCCMLPF3_Object::intermediateTag[AES_TAG_LENGTH_BYTES/4] |
| AESCCM_CallbackFxn AESCCMLPF3_Object::callbackFxn |
| AESCCM_OperationUnion* AESCCMLPF3_Object::operation |
| size_t AESCCMLPF3_Object::inputLength |
| volatile size_t AESCCMLPF3_Object::inputCBCMACLengthRemaining |
| volatile size_t AESCCMLPF3_Object::inputCTRLengthRemaining |
| size_t AESCCMLPF3_Object::totalAADLength |
| size_t AESCCMLPF3_Object::totalDataLength |
| size_t AESCCMLPF3_Object::aadBytesProcessed |
| volatile size_t AESCCMLPF3_Object::totalCBCMACLengthRemaining |
| volatile size_t AESCCMLPF3_Object::totalCTRLengthRemaining |
| AESCCM_OperationType AESCCMLPF3_Object::operationType |
| uint8_t AESCCMLPF3_Object::bufferedAAD[2U] |
| uint8_t AESCCMLPF3_Object::bufferedAADLength |
| uint8_t AESCCMLPF3_Object::macLength |
| uint8_t AESCCMLPF3_Object::nonceLength |
| size_t AESCCMLPF3_Object::aadLength |
| volatile size_t AESCCMLPF3_Object::totalDataLengthRemaining |
| volatile size_t AESCCMLPF3_Object::totalAADLengthRemaining |
| int_fast16_t AESCCMLPF3_Object::hsmStatus |
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
| uint32_t AESCCMLPF3_Object::tempAssetID |
| bool AESCCMLPF3_Object::segmentedOperationInProgress |