70 #ifndef ti_drivers_aesccm_AESCCMLPF3__include 71 #define ti_drivers_aesccm_AESCCMLPF3__include 79 #include <ti/devices/DeviceFamily.h> 80 #include DeviceFamily_constructPath(driverlib/aes.h) 86 #define AESCCMLPF3_AAD_BUFFER_SIZE 2U 110 volatile uint32_t intermediateCounter[AES_IV_LENGTH_BYTES / 4];
111 volatile uint32_t intermediateTag[AES_TAG_LENGTH_BYTES / 4];
127 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) 144 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) AESCommonLPF3_HWAttrs AESCCMLPF3_HWAttrs
AESCCMLPF3 Hardware Attributes.
Definition: AESCCMLPF3.h:94
const uint8_t * input
Definition: AESCCMLPF3.h:106
AESCommonLPF3_Object common
Definition: AESCCMLPF3.h:104
#define AESCCMLPF3_AAD_BUFFER_SIZE
Definition: AESCCMLPF3.h:86
int_fast16_t AESCCMLPF3HSM_setMac(AESCCM_Handle handle, const uint8_t *mac, size_t macLength)
Function to set the mac for an AES CCM segmented operation. This API needs to be called only when the...
volatile size_t totalCTRLengthRemaining
Definition: AESCCMLPF3.h:121
AESCCM_CallbackFxn callbackFxn
Definition: AESCCMLPF3.h:112
AES Global configuration.
Definition: AESCommon.h:154
AESCCM_OperationUnion * operation
Definition: AESCCMLPF3.h:113
size_t totalDataLength
Definition: AESCCMLPF3.h:118
volatile size_t totalAADLengthRemaining
Definition: AESCCMLPF3.h:130
const uint8_t * nonce
Definition: AESCCMLPF3.h:108
size_t aadLength
Definition: AESCCMLPF3.h:128
AESCCMLPF3 Object.
Definition: AESCCMLPF3.h:101
size_t totalAADLength
Definition: AESCCMLPF3.h:117
size_t inputLength
Definition: AESCCMLPF3.h:114
uint8_t * output
Definition: AESCCMLPF3.h:107
AESCCM_OperationType operationType
Definition: AESCCMLPF3.h:122
void(* AESCCM_CallbackFxn)(AESCCM_Handle handle, int_fast16_t returnValue, AESCCM_OperationUnion *operation, AESCCM_OperationType operationType)
The definition of a callback function used by the AESCCM driver when used in AESCCM_RETURN_BEHAVIOR_C...
Definition: AESCCM.h:1132
AESCommonLPF3 Hardware Attributes.
Definition: AESCommonLPF3.h:80
const uint8_t * aad
Definition: AESCCMLPF3.h:105
bool segmentedOperationInProgress
Definition: AESCCMLPF3.h:140
volatile size_t totalDataLengthRemaining
Definition: AESCCMLPF3.h:129
Union containing a reference to a one step, segmented AAD, segmented data, or segmented finalize oper...
Definition: AESCCM.h:1090
AESCommon driver implementation for the Low Power F3 family.
volatile size_t inputCBCMACLengthRemaining
Definition: AESCCMLPF3.h:115
uint32_t tempAssetID
Definition: AESCCMLPF3.h:137
uint8_t macLength
Definition: AESCCMLPF3.h:125
volatile size_t totalCBCMACLengthRemaining
Definition: AESCCMLPF3.h:120
volatile size_t inputCTRLengthRemaining
Definition: AESCCMLPF3.h:116
size_t aadBytesProcessed
Definition: AESCCMLPF3.h:119
AESCCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESCCM.h:1102
uint8_t * mac
Definition: AESCCMLPF3.h:109
int_fast16_t hsmStatus
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
Definition: AESCCMLPF3.h:136
uint8_t nonceLength
Definition: AESCCMLPF3.h:126
AESCommonLPF3 Object.
Definition: AESCommonLPF3.h:102
uint8_t bufferedAADLength
Definition: AESCCMLPF3.h:124