![]() |
![]() |
AESCommon driver implementation for the Low Power F3 family.
==========================================================================
The AESCommonLPF3 module provides common functionality used by the AES mode-specific implementations for the Low Power F3 family.
#include <stdbool.h>
#include <stdint.h>
#include <ti/drivers/AESCommon.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(inc/hw_types.h)>
Go to the source code of this file.
Data Structures | |
struct | AESCommonLPF3_HWAttrs |
AESCommonLPF3 Hardware Attributes. More... | |
struct | AESCommonLPF3_Object |
AESCommonLPF3 Object. More... | |
Macros | |
#define | AESCommonLPF3_UNALIGNED_IO_SUPPORT_ENABLE 0 |
#define | DMA_CH4 4U |
#define | DMA_CH5 5U |
#define | AESCommonLPF3_DMA_CHA_BITMASK ((uint32_t)1U << DMA_CH4) |
#define | AESCommonLPF3_DMA_CHB_BITMASK ((uint32_t)1U << DMA_CH5) |
#define AESCommonLPF3_UNALIGNED_IO_SUPPORT_ENABLE 0 |
#define DMA_CH4 4U |
#define DMA_CH5 5U |
#define AESCommonLPF3_DMA_CHA_BITMASK ((uint32_t)1U << DMA_CH4) |
#define AESCommonLPF3_DMA_CHB_BITMASK ((uint32_t)1U << DMA_CH5) |