![]() |
![]() |
Basic SemaphoreP Parameters. More...
#include <SemaphoreP.h>
Data Fields | |
SemaphoreP_Mode | mode |
void(* | callback )(void) |
Basic SemaphoreP Parameters.
Structure that contains the parameters are passed into SemaphoreP_create when creating a SemaphoreP instance. The SemaphoreP_Params_init function should be used to initialize the fields to default values before the application sets the fields manually. The SemaphoreP default parameters are noted in SemaphoreP_Params_init.
SemaphoreP_Mode SemaphoreP_Params::mode |
Mode for the semaphore
void(* SemaphoreP_Params::callback) (void) |
Callback while pending for semaphore post