![]() |
![]() |
Semaphore module for the RTOS Porting Interface.
============================================================================
Semaphores can be counting semaphores or binary semaphores. Counting semaphores keep track of the number of times the semaphore has been posted with post functions. This is useful, for example, if you have a group of resources that are shared between tasks. Such tasks might call pend() to see if a resource is available before using one. A count of zero for a counting semaphore denotes that it is not available. A positive count denotes how many times a SemaphoreP_pend can be called before it is blocked (or returns SemaphoreP_TIMEOUT).
Binary semaphores can have only two states: available (count = 1) and unavailable (count = 0). They can be used to share a single resource between tasks. They can also be used for a basic signalling mechanism, where the semaphore can be posted multiple times. Binary semaphores do not keep track of the count; they simply track whether the semaphore has been posted or not.
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
Go to the source code of this file.
Data Structures | |
union | SemaphoreP_Struct |
SemaphoreP structure. More... | |
struct | SemaphoreP_Params |
Basic SemaphoreP Parameters. More... | |
Macros | |
#define | SemaphoreP_STRUCT_SIZE (80) |
Number of bytes greater than or equal to the size of any RTOS SemaphoreP object. More... | |
#define | SemaphoreP_WAIT_FOREVER ~(0) |
Wait forever define. More... | |
#define | SemaphoreP_NO_WAIT (0) |
No wait define. More... | |
Typedefs | |
typedef union SemaphoreP_Struct | SemaphoreP_Struct |
SemaphoreP structure. More... | |
typedef void * | SemaphoreP_Handle |
Opaque client reference to an instance of a SemaphoreP. More... | |
Enumerations | |
enum | SemaphoreP_Status { SemaphoreP_OK = 0, SemaphoreP_TIMEOUT = -1 } |
Status codes for SemaphoreP APIs (for backwards compatibility) More... | |
enum | SemaphoreP_Mode { SemaphoreP_Mode_COUNTING = 0x0, SemaphoreP_Mode_BINARY = 0x1 } |
Mode of the semaphore. More... | |
Functions | |
SemaphoreP_Handle | SemaphoreP_construct (SemaphoreP_Struct *handle, unsigned int count, SemaphoreP_Params *params) |
SemaphoreP_Handle | SemaphoreP_constructBinary (SemaphoreP_Struct *handle, unsigned int count) |
void | SemaphoreP_destruct (SemaphoreP_Struct *semP) |
SemaphoreP_Handle | SemaphoreP_create (unsigned int count, SemaphoreP_Params *params) |
Function to create a semaphore. More... | |
SemaphoreP_Handle | SemaphoreP_createBinary (unsigned int count) |
Function to create a binary semaphore. More... | |
SemaphoreP_Handle | SemaphoreP_createBinaryCallback (unsigned int count, void(*callback)(void)) |
Function to create a binary semaphore. More... | |
void | SemaphoreP_delete (SemaphoreP_Handle handle) |
Function to delete a semaphore. More... | |
void | SemaphoreP_Params_init (SemaphoreP_Params *params) |
Initialize params structure to default values. More... | |
SemaphoreP_Status | SemaphoreP_pend (SemaphoreP_Handle handle, uint32_t timeout) |
Function to pend (wait) on a semaphore. More... | |
void | SemaphoreP_post (SemaphoreP_Handle handle) |
Function to post (signal) a semaphore from task of ISR context. More... | |
Variables | |
SemaphoreP_Params | SemaphoreP_defaultParams |
Default SemaphoreP instance parameters. More... | |
#define SemaphoreP_STRUCT_SIZE (80) |
Number of bytes greater than or equal to the size of any RTOS SemaphoreP object.
NoRTOS: 16 BIOS 6.x: 28 BIOS 7.x: 28 FreeRTOS: 80
#define SemaphoreP_WAIT_FOREVER ~(0) |
Wait forever define.
#define SemaphoreP_NO_WAIT (0) |
No wait define.
typedef union SemaphoreP_Struct SemaphoreP_Struct |
SemaphoreP structure.
Opaque structure that should be large enough to hold any of the RTOS specific SemaphoreP objects.
typedef void* SemaphoreP_Handle |
Opaque client reference to an instance of a SemaphoreP.
A SemaphoreP_Handle returned from the SemaphoreP_create represents that instance and is used in the other instance based functions (e.g. SemaphoreP_post or SemaphoreP_pend, etc.).
enum SemaphoreP_Status |
enum SemaphoreP_Mode |
SemaphoreP_Handle SemaphoreP_construct | ( | SemaphoreP_Struct * | handle, |
unsigned int | count, | ||
SemaphoreP_Params * | params | ||
) |
SemaphoreP_Handle SemaphoreP_constructBinary | ( | SemaphoreP_Struct * | handle, |
unsigned int | count | ||
) |
void SemaphoreP_destruct | ( | SemaphoreP_Struct * | semP | ) |
SemaphoreP_Handle SemaphoreP_create | ( | unsigned int | count, |
SemaphoreP_Params * | params | ||
) |
Function to create a semaphore.
count | Initial count of the semaphore. For binary semaphores, only values of 0 or 1 are valid. |
params | Pointer to the instance configuration parameters. NULL denotes to use the default parameters (SemaphoreP default parameters as noted in SemaphoreP_Params_init. |
SemaphoreP_Handle SemaphoreP_createBinary | ( | unsigned int | count | ) |
Function to create a binary semaphore.
This can be used instead of SemaphoreP_create() to create a binary semaphore.
count | Initial count of the binary semaphore. Only values of 0 or 1 are valid. |
SemaphoreP_Handle SemaphoreP_createBinaryCallback | ( | unsigned int | count, |
void(*)(void) | callback | ||
) |
Function to create a binary semaphore.
This can be used instead of SemaphoreP_create() to create a binary semaphore.
count | Initial count of the binary semaphore. Only values of 0 or 1 are valid. |
callback | Callback while pending for semaphore post |
void SemaphoreP_delete | ( | SemaphoreP_Handle | handle | ) |
Function to delete a semaphore.
handle | A SemaphoreP_Handle returned from SemaphoreP_create |
void SemaphoreP_Params_init | ( | SemaphoreP_Params * | params | ) |
Initialize params structure to default values.
The default parameters are:
params | Pointer to the instance configuration parameters. |
SemaphoreP_Status SemaphoreP_pend | ( | SemaphoreP_Handle | handle, |
uint32_t | timeout | ||
) |
Function to pend (wait) on a semaphore.
handle | A SemaphoreP_Handle returned from SemaphoreP_create |
timeout | Timeout (in ClockP ticks) to wait for the semaphore to be posted (signalled). |
void SemaphoreP_post | ( | SemaphoreP_Handle | handle | ) |
Function to post (signal) a semaphore from task of ISR context.
handle | A SemaphoreP_Handle returned from SemaphoreP_create |
SemaphoreP_Params SemaphoreP_defaultParams |
Default SemaphoreP instance parameters.
SemaphoreP_defaultParams represents the default parameters that are used when creating or constructing a SemaphoreP instance. SemaphoreP_Params_init() will use the contents of this structure for initializing the SemaphoreP_Params instance.
SemaphoreP_defaultParams is exposed to the application for the purpose of allowing the application to change the default parameters for all SemaphoreP instances created thereafter. The main intent for allowing the default parameters to be changed is for setting a semaphore's callback function to Power_idleFunc(), so that the SOC can enter low power mode when pending on a semaphore.