Data Fields
ComparatorLPF3LP_Object Struct Reference

ComparatorLPF3LP Object. More...

#include <ComparatorLPF3LP.h>

Collaboration diagram for ComparatorLPF3LP_Object:
Collaboration graph
[legend]

Data Fields

HwiP_Struct hwi
 
Comparator_CallBackFxn callbackFxn
 
Comparator_Trigger trigger
 
bool isOpen
 
bool isRunning
 

Detailed Description

ComparatorLPF3LP Object.

The application must not access any member variables of this structure!

Field Documentation

§ hwi

HwiP_Struct ComparatorLPF3LP_Object::hwi

Hwi used for handling comparator events

§ callbackFxn

Comparator_CallBackFxn ComparatorLPF3LP_Object::callbackFxn

User callback function

§ trigger

Comparator_Trigger ComparatorLPF3LP_Object::trigger

Condition on which comparator triggers an event

§ isOpen

bool ComparatorLPF3LP_Object::isOpen

Determine if comparator is open

§ isRunning

bool ComparatorLPF3LP_Object::isRunning

Determine if comparator instance is already running


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale