Comparator parameters. More...
#include <Comparator.h>
Data Fields | |
Comparator_CallBackFxn | callbackFxn |
Comparator_Trigger | trigger |
Comparator parameters.
Comparator parameters are used by the Comparator_open() call. Default values for these parameters are set using Comparator_Params_init().
Comparator_CallBackFxn Comparator_Params::callbackFxn |
Callback function called when events happen in the Comparator driver
Comparator_Trigger Comparator_Params::trigger |
Interrupt trigger of the Comparator module