Comprehensive List of Fixed Issues¶
This section will provide a comprehensive list of the issues that have been fixed with each release of the SimpleLink Low Power F3 SDK.
Note
For more information regarding new features, fixed issues, or known issues
for a specific SDK, please reference the respective Core SDK release notes.
These can be found online through the links provided in each section, or
within the SDK at:
{SDK_INSTALL_DIR}/docs/simplelink_mcu_sdk/release_notes_coresdk_lpf3_x_xx_xx_xx.html
v7x SDKs¶
7.20.01.10 (Oct 2023)¶
ID |
Summary |
---|---|
Device stops responding after multiple connections |
7.20.00.29 (Aug 2023)¶
ID |
Summary |
---|---|
CC2340R5 basic_ble_oad_offchip_peripheral Link Terminate when start OAD using bTool |
|
Tx Power value in advertisements is not updated after the advertisement are started |
|
Bonding fails if LTK not updated in the linkDB |
|
HCI_EXT_SetTxPowerDbmCmd() does not change txPower on CC23XX device |
|
Repeatedly changing connection PHY sometimes causes connection timeout during long-term stability testing |
|
[basic_ble_oad_onchip] GATT caching can cause OAD to fail |
|
CC2340R5: Canceling ongoing OAD via BTool causes retryOAD to fail |
|
[OAD] CC23xx device does not indicate to Android/ iOS device to not cache GATT table |
|
[Basic BLE Profiles - CGM] Notifications are not sent after large amount of measurements are added |
|
Basic BLE central device uses a peer’s RP address after bonding |
|
basic_ble not using SysConfig parameters for scan and connection parameters |
|
HCI_LE_ReadRfPathCompCmd and HCI_LE_WriteRFPathCompCmd not supported |
|
[Basic Example] Basic Broadcaster Doesn’t Advertise |
|
[SysConfig] Disable the display module checkbox is missing. |
7.10.00.35 (May 2023)¶
ID |
Summary |
---|---|
Central failed to establish connectionWL to peer with RPA from white list |
|
Basic BLE project with multirole BLE role advertises intermittently |
|
[macOS Build] imgtool command not found - build post process step for OAD examples fails |
|
TERMINATION_IND sometimes missed when using ADV Interval < 100ms |
|
CC2340R5 current consumption increased by ~1uA due to longer duration of ‘IDLE’ state |
|
GAP_ADV_EVT_MASK_SCAN_REQ_NOTI is not processed in the controller |
|
CC23X0 hangs after calling scan_enable |
|
[PSIRT-145] Accepts PairConfirmSend with wrong values |
|
[PSIRT-144] Accepts PairRandomSend before exchanging public key |
|
[PSIRT-143] BLE secure pairing: Accepts DHKeyCheckSend with all fields zero |