Radio Control Layer (RCL)
|
#include <ti/drivers/dpl/HwiP.h>
#include <ti/devices/DeviceFamily.h>
#include <ti/drivers/rcl/hal/hal.h>
#include <ti/log/Log.h>
Macros | |
#define | RCL_DEFAULT_HFTRACKCTL_RATIO 0x00400000U |
Enumerations | |
enum | { SYSTIM_CH2_SETUP = 1, SYSTIM_CH2_START = 2, SYSTIM_CH2_STOP = 3 } |
Variables | |
static HwiP_Struct | schedHwi |
void(* | halSchedFsmCb )(void) = NULL |
static HwiP_Struct | dispatchHwi |
void(* | halDispatchFsmCb )(void) = NULL |
static HwiP_Struct | commandHwi |
void(* | halCommandFsmCb )(void) = NULL |
enum { ... } | channel2usage = SYSTIM_CH2_SETUP |
#define RCL_DEFAULT_HFTRACKCTL_RATIO 0x00400000U |
Referenced by hal_get_hfxt_ratio(), and hal_get_hfxt_ratio_default().
|
static |
References halSchedFsmCb.
Referenced by hal_init_fsm().
|
static |
References halDispatchFsmCb.
Referenced by hal_init_fsm().
|
static |
References halCommandFsmCb.
Referenced by hal_init_fsm().
uint32_t hal_get_ifg_reg | ( | void | ) |
void hal_init_fsm | ( | void(*)(void) | dispatchFsmCb, |
void(*)(void) | schedFsmCb, | ||
void(*)(void) | commandFsmCb | ||
) |
References commandHwi, dispatchHwi, halCommandFsmCb, halDispatchFsmCb, halSchedFsmCb, RF_commandHwi(), RF_dispatchHwi(), RF_schedHwi(), and schedHwi.
void hal_trigger_command_fsm | ( | void | ) |
void hal_trigger_dispatch_fsm | ( | void | ) |
void hal_trigger_scheduler_fsm | ( | void | ) |
uint32_t hal_get_current_time | ( | void | ) |
void hal_enable_setup_time_irq | ( | void | ) |
void hal_setup_setup_time | ( | uint32_t | startTime | ) |
References channel2usage, and SYSTIM_CH2_SETUP.
void hal_setup_start_time | ( | uint32_t | startTime | ) |
References channel2usage, and SYSTIM_CH2_START.
void hal_setup_hard_stop_time | ( | uint32_t | stopTime | ) |
References channel2usage, and SYSTIM_CH2_STOP.
void hal_enable_hard_stop_time_irq | ( | void | ) |
void hal_setup_graceful_stop_time | ( | uint32_t | stopTime | ) |
void hal_enable_graceful_stop_time_irq | ( | void | ) |
void hal_cancel_setup_time | ( | void | ) |
References hal_cancel_lrfd_systim0().
void hal_cancel_start_time | ( | void | ) |
References hal_cancel_lrfd_systim0().
void hal_cancel_hard_stop_time | ( | void | ) |
References hal_cancel_lrfd_systim0().
void hal_cancel_graceful_stop_time | ( | void | ) |
void hal_setup_sync_found_cap | ( | void | ) |
HalTimerEvent hal_check_clear_timer_compare | ( | void | ) |
void hal_disable_radio_interrupts | ( | void | ) |
void hal_set_clkctl | ( | uint32_t | clkctl | ) |
void hal_enable_clk_buffer | ( | void | ) |
void hal_power_set_constraint | ( | void | ) |
void hal_power_release_constraint | ( | void | ) |
void hal_power_open | ( | void(*)(RCL_PowerEvent) | f | ) |
References hal_power_post_notify_fxn(), powerAwakeStandbyObj, and rclPowerNotify.
void hal_power_close | ( | void | ) |
References powerAwakeStandbyObj.
void hal_temperature_init | ( | void | ) |
__attribute__ | ( | (weak) | ) |
uint32_t hal_get_hfxt_ratio | ( | void | ) |
References RCL_DEFAULT_HFTRACKCTL_RATIO.
uint32_t hal_get_hfxt_ratio_default | ( | void | ) |
References RCL_DEFAULT_HFTRACKCTL_RATIO.
|
static |
Referenced by hal_init_fsm().
void(* halSchedFsmCb) (void) = NULL |
Referenced by hal_init_fsm(), and RF_schedHwi().
|
static |
Referenced by hal_init_fsm().
void(* halDispatchFsmCb) (void) = NULL |
Referenced by hal_init_fsm(), and RF_dispatchHwi().
|
static |
Referenced by hal_init_fsm().
void(* halCommandFsmCb) (void) = NULL |
Referenced by hal_init_fsm(), and RF_commandHwi().
enum { ... } channel2usage |