38 void hal_init_fsm(
void (*setupFsmCb)(
void),
void (*schedFsmCb)(
void),
39 void (*commandFsmCb)(
void));
void hal_enable_hard_stop_time_irq(void)
Definition: hal_cc23x0.c:205
void hal_disable_radio_interrupts(void)
Definition: hal_cc23x0.c:317
void hal_arm_cmd_done_cap(void)
void hal_arm_cmd_start_cap(void)
uint32_t hal_get_hfxt_ratio_default(void)
Definition: hal_cc23x0.c:429
void hal_enable_setup_time_irq(void)
Definition: hal_cc23x0.c:171
void hal_setup_cmd_start_cap(void)
void hal_setup_start_time(uint32_t startTime)
Definition: hal_cc23x0.c:189
void hal_power_open(void(*f)(RCL_PowerEvent))
Definition: hal_cc23x0.c:391
uint32_t hal_get_sync_found_cap(void)
void hal_power_close(void)
Definition: hal_cc23x0.c:401
RCL_PowerEvent
Definition: hal.h:70
void hal_setup_setup_time(uint32_t setupTime)
Definition: hal_cc23x0.c:176
uint32_t hal_get_current_time(void)
Definition: hal_cc23x0.c:160
void hal_set_clkctl(uint32_t clkctl)
Definition: hal_cc23x0.c:324
void hal_init_fsm(void(*setupFsmCb)(void), void(*schedFsmCb)(void), void(*commandFsmCb)(void))
Definition: hal_cc23x0.c:121
uint32_t hal_get_cmd_done_cap(void)
void hal_setup_cmd_done_cap(void)
void hal_cancel_start_time(void)
Definition: hal_cc23x0.c:240
void hal_enable_graceful_stop_time_irq(void)
Definition: hal_cc23x0.c:217
void hal_trigger_scheduler_fsm()
Definition: hal_cc23x0.c:154
int16_t hal_get_temperature(void)
void hal_trigger_command_fsm(void)
Definition: hal_cc23x0.c:142
void hal_cancel_setup_time(void)
Definition: hal_cc23x0.c:235
void hal_power_release_constraint(void)
Definition: hal_cc23x0.c:382
uint32_t hal_get_ifg_reg(void)
Definition: hal_cc23x0.c:105
uint32_t hal_get_hfxt_ratio(void)
Definition: hal_cc23x0.c:424
void hal_enable_clk_buffer(void)
Definition: hal_cc23x0.c:258
void hal_trigger_dispatch_fsm(void)
Definition: hal_cc23x0.c:148
void hal_power_set_constraint(void)
Definition: hal_cc23x0.c:373
void hal_setup_graceful_stop_time(uint32_t stopTime)
Definition: hal_cc23x0.c:210
HalTimerEvent hal_check_clear_timer_compare(void)
Definition: hal_cc23x0.c:277
void hal_temperature_init(void)
Definition: hal_cc23x0.c:409
void hal_setup_hard_stop_time(uint32_t stopTime)
Definition: hal_cc23x0.c:197
void hal_cancel_hard_stop_time(void)
Definition: hal_cc23x0.c:245
void hal_arm_sync_found_cap(void)
HalTimerEvent
Definition: hal.h:62
void hal_setup_sync_found_cap(void)
Definition: hal_cc23x0.c:266
void hal_cancel_graceful_stop_time(void)
Definition: hal_cc23x0.c:250
uint32_t hal_get_cmd_start_cap(void)