Data Fields
PWMTimerLPF3_HwAttrs Struct Reference

PWMTimerLPF3 Hardware attributes. More...

#include <PWMTimerLPF3.h>

Data Fields

uint8_t lgpTimerInstance
 
uint8_t preScalerDivision
 

Detailed Description

PWMTimerLPF3 Hardware attributes.

These fields are used by the driver to set up the underlying LGPTimer driver statically.

Field Documentation

§ lgpTimerInstance

uint8_t PWMTimerLPF3_HwAttrs::lgpTimerInstance

LGPTimer unit index (0, 1, 2..)

§ preScalerDivision

uint8_t PWMTimerLPF3_HwAttrs::preScalerDivision

LGPTimer prescaler divider


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale