132 #ifndef ti_drivers_pwm__PWMTimerLPF3_include 133 #define ti_drivers_pwm__PWMTimerLPF3_include 153 #define PWMTimerLPF3_CMD_DEBUG_STALL (PWM_CMD_RESERVED + 0) 158 #define CMD_ARG_DEBUG_STALL_OFF ((uint32_t)LGPTimerLPF3_DEBUG_STALL_OFF) 159 #define CMD_ARG_DEBUG_STALL_ON ((uint32_t)LGPTimerLPF3_DEBUG_STALL_IMMEDIATE) LGPTimer Global configuration.
Definition: LGPTimerLPF3.h:768
PWMTimerLPF3 Object.
Definition: PWMTimerLPF3.h:188
PWM_Duty_Units
PWM duty cycle unit definitions. Refer to device specific implementation if using PWM_DUTY_COUNTS (ra...
Definition: PWM.h:306
bool isOpen
Definition: PWMTimerLPF3.h:199
uint8_t lgpTimerInstance
Definition: PWMTimerLPF3.h:175
PWM_Period_Units periodUnit
Definition: PWMTimerLPF3.h:195
struct PWMTimerLPF3_Object PWMTimerLPF3_Object
PWMTimerLPF3 Object.
LGPTimerLPF3_Handle hTimer
Definition: PWMTimerLPF3.h:194
Pulse Width Modulation (PWM) driver.
PWM_Period_Units
PWM period unit definitions. Refer to device specific implementation if using PWM_PERIOD_COUNTS (raw ...
Definition: PWM.h:294
uint32_t periodValue
Definition: PWMTimerLPF3.h:190
uint32_t periodCounts
Definition: PWMTimerLPF3.h:191
uint32_t dutyValue
Definition: PWMTimerLPF3.h:192
PWM_IdleLevel idleLevel
Definition: PWMTimerLPF3.h:198
LGPTimerLPF3_ChannelNo chNumber
Definition: PWMTimerLPF3.h:197
uint32_t dutyCounts
Definition: PWMTimerLPF3.h:193
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:409
bool isRunning
Definition: PWMTimerLPF3.h:200
const PWM_FxnTable PWMTimerLPF3_fxnTable
LGPTimer driver implementation for Low Power F3 devices.
LGPTimerLPF3_ChannelNo
Definitions for supported LGPTimer channel numbers.
Definition: LGPTimerLPF3.h:283
uint8_t preScalerDivision
Definition: PWMTimerLPF3.h:176
struct PWMTimerLPF3_HwAttrs PWMTimerLPF3_HwAttrs
PWMTimerLPF3 Hardware attributes.
PWM_Duty_Units dutyUnit
Definition: PWMTimerLPF3.h:196
PWMTimerLPF3 Hardware attributes.
Definition: PWMTimerLPF3.h:173
PWM_IdleLevel
Idle output level when PWM is not running (stopped / not started).
Definition: PWM.h:321