Data Fields
ANSIX936KDF_Params Struct Reference

ANSIX936KDF Parameters. More...

#include <ANSIX936KDF.h>

Data Fields

ANSIX936KDF_ReturnBehavior returnBehavior
 
uint32_t timeout
 

Detailed Description

ANSIX936KDF Parameters.

ANSIX936KDF Parameters are used to with the ANSIX936KDF_open() call. Default values for these parameters are set using ANSIX936KDF_Params_init().

See also
ANSIX936KDF_Params_init()

Field Documentation

§ returnBehavior

ANSIX936KDF_ReturnBehavior ANSIX936KDF_Params::returnBehavior

Blocking or polling return behavior

§ timeout

uint32_t ANSIX936KDF_Params::timeout

Timeout before the driver returns an error in ANSIX936KDF_RETURN_BEHAVIOR_BLOCKING


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale