Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
ANSIX936KDF.h File Reference

Detailed Description

ANSIX936KDF driver header.


Overview

The ANSI X9.63 Key Derivation Function (KDF) driver utilizes the SHA-256 hash function to derive a key from a shared secret value and optional shared info. See ANSI X9.63-2011 or SEC-1 v2.0 standard for more information.

Usage

Before starting a ANSIX936KDF operation, the application must do the following:

Synopsis

// Import ANSIX936KDF Driver definitions
// Import driver configuration
#include "ti_drivers_config.h"
// Initialize driver
// Open driver instance
handle = ANSIX936KDF_open(CONFIG_ANSIX936KDF_0, NULL);
// Perform key derivation
result = ANSIX936KDF_deriveKey(handle, input, sizeof(input), sharedInfo,
sizeof(sharedInfo), output, sizeof(output));
// Close driver instance

Example

The ANSIX936KDF_deriveKey() function performs a key derivation operation in a single call.

After a ANSIX936KDF operation completes, the application may either start another operation or close the driver by calling ANSIX936KDF_close().

int_fast16_t result;
uint8_t sharedInfo[] = {0x75, 0xee, 0xf8, 0x1a, 0xa3, 0x04, 0x1e, 0x33,
0xb8, 0x09, 0x71, 0x20, 0x3d, 0x2c, 0x0c, 0x52};
uint8_t input[] = {0x22, 0x51, 0x8b, 0x10, 0xe7, 0x0f, 0x2a, 0x3f, 0x24, 0x38, 0x10, 0xae,
0x32, 0x54, 0x13, 0x9e, 0xfb, 0xee, 0x04, 0xaa, 0x57, 0xc7, 0xaf, 0x7d};
uint8_t output[32] = {0};
handle = ANSIX936KDF_open(CONFIG_ANSIX936KDF_0, &params);
assert(handle != NULL);
result = ANSIX936KDF_deriveKey(handle, input, sizeof(input), sharedInfo,
sizeof(sharedInfo), output, sizeof(output));
assert(result == ANSIX936KDF_STATUS_SUCCESS);
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/SHA2.h>
Include dependency graph for ANSIX936KDF.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ANSIX936KDF_Config
 ANSIX936KDF Global configuration. More...
 
struct  ANSIX936KDF_Params
 ANSIX936KDF Parameters. More...
 

Macros

#define ANSIX936KDF_STATUS_RESERVED   ((int_fast16_t)-32)
 
#define ANSIX936KDF_STATUS_SUCCESS   ((int_fast16_t)0)
 Successful status code. More...
 
#define ANSIX936KDF_STATUS_ERROR   ((int_fast16_t)-1)
 Generic error status code. More...
 
#define ANSIX936KDF_STATUS_RESOURCE_UNAVAILABLE   ((int_fast16_t)-2)
 An error status code returned if the hardware or software resource is currently unavailable. More...
 

Typedefs

typedef ANSIX936KDF_ConfigANSIX936KDF_Handle
 A handle that is returned from an ANSIX936KDF_open() call. More...
 

Enumerations

enum  ANSIX936KDF_ReturnBehavior { ANSIX936KDF_RETURN_BEHAVIOR_BLOCKING = SHA2_RETURN_BEHAVIOR_BLOCKING, ANSIX936KDF_RETURN_BEHAVIOR_POLLING = SHA2_RETURN_BEHAVIOR_POLLING }
 The way in which ANSIX936KDF function calls return after performing an operation. More...
 

Functions

void ANSIX936KDF_init (void)
 Initializes the ANSIX936KDF driver module. More...
 
void ANSIX936KDF_Params_init (ANSIX936KDF_Params *params)
 Initializes params with default values. More...
 
ANSIX936KDF_Handle ANSIX936KDF_open (uint_least8_t index, const ANSIX936KDF_Params *params)
 Initializes a ANSIX936KDF driver instance and returns a handle. More...
 
void ANSIX936KDF_close (ANSIX936KDF_Handle handle)
 Closes a ANSIX936KDF peripheral specified by handle. More...
 
int_fast16_t ANSIX936KDF_deriveKey (ANSIX936KDF_Handle handle, const void *input, size_t inputLen, const void *sharedInfo, size_t sharedInfoLen, void *output, size_t outputLen)
 Derives a key with the SHA-256 hash function. More...
 
ANSIX936KDF_Handle ANSIX936KDF_construct (ANSIX936KDF_Config *config, const ANSIX936KDF_Params *params)
 Constructs a new ANSIX936KDF object. More...
 

Variables

const ANSIX936KDF_Config ANSIX936KDF_config []
 Global ANSIX936KDF configuration struct. More...
 
const uint_least8_t ANSIX936KDF_count
 Global ANSIX936KDF configuration count. More...
 
const ANSIX936KDF_Params ANSIX936KDF_defaultParams
 Default ANSIX936KDF_Params structure. More...
 

Macro Definition Documentation

§ ANSIX936KDF_STATUS_RESERVED

#define ANSIX936KDF_STATUS_RESERVED   ((int_fast16_t)-32)

Common ANSIX936KDF status code reservation offset. ANSIX936KDF driver implementations should offset status codes with ANSIX936KDF_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define ANSIX936KDFXYZ_STATUS_ERROR0 ANSIX936KDF_STATUS_RESERVED - 0
#define ANSIX936KDFXYZ_STATUS_ERROR1 ANSIX936KDF_STATUS_RESERVED - 1
#define ANSIX936KDFXYZ_STATUS_ERROR2 ANSIX936KDF_STATUS_RESERVED - 2

§ ANSIX936KDF_STATUS_SUCCESS

#define ANSIX936KDF_STATUS_SUCCESS   ((int_fast16_t)0)

Successful status code.

Functions return ANSIX936KDF_STATUS_SUCCESS if the function was executed successfully.

§ ANSIX936KDF_STATUS_ERROR

#define ANSIX936KDF_STATUS_ERROR   ((int_fast16_t)-1)

Generic error status code.

Functions return ANSIX936KDF_STATUS_ERROR if the function was not executed successfully and no more specific error is applicable.

§ ANSIX936KDF_STATUS_RESOURCE_UNAVAILABLE

#define ANSIX936KDF_STATUS_RESOURCE_UNAVAILABLE   ((int_fast16_t)-2)

An error status code returned if the hardware or software resource is currently unavailable.

ANSIX936KDF driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

Typedef Documentation

§ ANSIX936KDF_Handle

A handle that is returned from an ANSIX936KDF_open() call.

Enumeration Type Documentation

§ ANSIX936KDF_ReturnBehavior

The way in which ANSIX936KDF function calls return after performing an operation.

Not all ANSIX936KDF operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

ANSIX936KDF functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
ANSIX936KDF_RETURN_BEHAVIOR_BLOCKING X
ANSIX936KDF_RETURN_BEHAVIOR_POLLING X X X
Enumerator
ANSIX936KDF_RETURN_BEHAVIOR_BLOCKING 

The function call will block while the ANSIX936KDF operation goes on in the background. ANSIX936KDF operation results are available after the function returns.

ANSIX936KDF_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while the ANSIX936KDF operation goes on in the background. ANSIX936KDF operation results are available after the function returns.

Function Documentation

§ ANSIX936KDF_init()

void ANSIX936KDF_init ( void  )

Initializes the ANSIX936KDF driver module.

Precondition
The ANSIX936KDF_config structure must exist and be persistent before this function can be called. This function must also be called before any other ANSIX936KDF driver APIs. This function call does not modify any peripheral registers.

§ ANSIX936KDF_Params_init()

void ANSIX936KDF_Params_init ( ANSIX936KDF_Params params)

Initializes params with default values.

Parameters
paramsA pointer to ANSIX936KDF_Params structure for initialization

Default values:
returnBehavior = ANSIX936KDF_RETURN_BEHAVIOR_BLOCKING
timeout = SemaphoreP_WAIT_FOREVER

§ ANSIX936KDF_open()

ANSIX936KDF_Handle ANSIX936KDF_open ( uint_least8_t  index,
const ANSIX936KDF_Params params 
)

Initializes a ANSIX936KDF driver instance and returns a handle.

Precondition
ANSIX936KDF controller has been initialized using ANSIX936KDF_init()
Parameters
indexLogical peripheral number for the ANSIX936KDF indexed into the ANSIX936KDF_config table
paramsPointer to a parameter block, if NULL it will use default values.
Returns
A ANSIX936KDF_Handle on success or a NULL on an error or if it has been opened already.
See also
ANSIX936KDF_init()
ANSIX936KDF_close()

§ ANSIX936KDF_close()

void ANSIX936KDF_close ( ANSIX936KDF_Handle  handle)

Closes a ANSIX936KDF peripheral specified by handle.

Precondition
ANSIX936KDF_open() has to be called first.
Parameters
handleA ANSIX936KDF_Handle returned from ANSIX936KDF_open()
See also
ANSIX936KDF_open()

§ ANSIX936KDF_deriveKey()

int_fast16_t ANSIX936KDF_deriveKey ( ANSIX936KDF_Handle  handle,
const void *  input,
size_t  inputLen,
const void *  sharedInfo,
size_t  sharedInfoLen,
void *  output,
size_t  outputLen 
)

Derives a key with the SHA-256 hash function.

Uses the SHA-256 hash function to derives a key from a shared secret value and optional shared information.

Precondition
ANSIX936KDF_open() has to be called first.
Parameters
handleA ANSIX936KDF_Handle returned from ANSIX936KDF_open()
inputA pointer to the input (i.e. shared secret value)
inputLenThe length of input in bytes.
sharedInfoA pointer to the shared info. May be NULL if there is no shared info.
sharedInfoLenThe length of the sharedInfo in bytes. Set to zero if sharedInfo is NULL.
outputA pointer to the location to write the output (i.e. derived key).
outputLenOutput length in bytes.
Return values
ANSIX936KDF_STATUS_SUCCESSThe operation succeeded.
ANSIX936KDF_STATUS_ERRORThe operation failed.
ANSIX936KDF_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
See also
ANSIX936KDF_open()

§ ANSIX936KDF_construct()

ANSIX936KDF_Handle ANSIX936KDF_construct ( ANSIX936KDF_Config config,
const ANSIX936KDF_Params params 
)

Constructs a new ANSIX936KDF object.

Unlike ANSIX936KDF_open(), ANSIX936KDF_construct() does not require the hwAttrs and object to be allocated in a ANSIX936KDF_Config array that is indexed into. Instead, the ANSIX936KDF_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Parameters
configANSIX936KDF_Config describing the location of the object and hwAttrs.
paramsANSIX936KDF_Params to configure the driver instance.
Returns
Returns a ANSIX936KDF_Handle on success or NULL on failure.
Precondition
The object struct config points to must be zeroed out prior to calling this function. Otherwise, unexpected behavior may ensue.

Variable Documentation

§ ANSIX936KDF_config

const ANSIX936KDF_Config ANSIX936KDF_config[]

Global ANSIX936KDF configuration struct.

Specifies context objects and hardware attributes for every driver instance.

This variable is supposed to be defined in the board file.

§ ANSIX936KDF_count

const uint_least8_t ANSIX936KDF_count

Global ANSIX936KDF configuration count.

Specifies the number of available ANSIX936KDF driver instances.

This variable is supposed to be defined in the board file.

§ ANSIX936KDF_defaultParams

const ANSIX936KDF_Params ANSIX936KDF_defaultParams

Default ANSIX936KDF_Params structure.

See also
ANSIX936KDF_Params_init()
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale