OAD Application

The application layer is responsible for plugging the OAD service. The OAD profile and communication with the BLE-Stack is encapsulated inside the OAD module. An application developer wishing to implement use the TI OAD solution will not need to worry about implementing the OAD state machine. The details of the OAD application layer are documented here for completeness and to aide in debugging.

OAD Software Architecture

The building blocks of the OAD software architecture are detailed below. In the figure below the following terms have been abbreviated for compactness in the image.

  • CB : Callback

  • SVC: BLE Service

  • Func: Function

../_images/ditaa-9797b8cc3c498e4805881d9a2ea6dcc4eca28904.png

Internally the OAD service is responsible for the following:

  • Implementing the OAD profile

  • Plugging the GATT read and write callback from the BLE5-Stack

  • Serializing and de-serializing structures from over the messages

  • Sending OAD related requests and responses to the BLE5-Stack to be sent over the air

  • Queuing up messages from stack callbacks to be processed later by the application

  • Implementing the OAD state machine, and ensuring proper state transitions

  • Implementing the OAD inactivity timers

  • Implementing getter/setter functions for the application to use and configure the OAD service

External to the OAD service the application task is responsible for the following. For more information, see the OAD Advanced lab of the SimpleLink Academy.

  • Plugging an OAD event handler

  • Calling the OAD event processing function in a task context when events are posted.

  • Resetting the device when the OAD_DL_COMPLETE event is received.

A message sequence chart is included below to show a sample of an application’s interaction with the OAD service.

@startuml
hide footbox

participant app_task.c as app
participant oad.c as oad
participant "BLE Stack" as BLE
participant "OAD Queue" as OADQ

box "BLE-Stack Context"
    participant "GATT R/W Callback" as GATT
end box

activate app

group Initialize OAD service
    app -> oad : OAD_open()

    activate oad
    oad -> BLE : GATTServApp_InitCharCfg() (repeat for each char CCCD)
    oad -> BLE : GATTServApp_RegisterService()

    oad -> OADQ : Queue_construct()
    deactivate oad

    app -> oad : OAD_register()
end

BLE -> app : ATT_MTU_UPDATED_EVENT
app -> oad : OAD_setBlockSize()


group Processing OAD Service Messages
    note over oad, BLE
        Peer device sends OTA command/write
    end note

    activate GATT
    GATT -> oad : oadWriteAttrCB()

    activate oad
    oad -> OADQ : oadEnqueueMsg()
    oad -> app : Execute (*oadWriteCB_t)
    deactivate OAD
    deactivate GATT

    app -> oad : OAD_processQueue()
    oad -> OADQ : Queue_get()

    note over oad
        Process event
    end note
end

group
@enduml

Figure 137. OAD service/ Application interaction

OAD State Machine

The OAD service implements an ‘OAD State Machine’ for performing the OAD. The following state machine depicts the OAD service state transitions and its interactions with the OAD communication profile messages for both on-chip and off-chip OAD.

../_images/oad_state_machine.png

Figure 138. OAD Types Overview

The states and state transitions are encapsulated inside the OAD service, but some of the critical states are described below to aide in understanding.

Note these sections refer to internal state handling and transitions local to the target device. For a summary of the over the air sequence see Sequence diagram for OAD process and for a breakdown of the different types of profile messages and how to interpret them over the air please see BLE-Stack OAD Profile.

Image Validation

After establishing a new connection, updating the connection interval for a faster OAD and enabling notifications of OAD Image Identify and OAD Image Block characteristics on the OAD target, the OAD distributor shall write to the Image Identify characteristic of the OAD target. The message data will be the header retrieved from the OAD Image available for OAD.

On receiving the Image Identify message, the OAD target will get ready for OAD process. The image validation is done by secure bootloader. That means, there is no image validation in the OAD application.

Image Block Transfers

Once the OAD target is ready for receiving image, it will switch to the configuration state. There it will get the block size and set image count. When the OAD distributor sends the Start OAD Command to the Control Characteristic (for more details see OAD Control Characteristic Supported Commands.), the OAD target will respond with a Control characteristic notification requesting the first block. The OAD distributor will then send the first block to the OAD target.

This process continues with the OAD target notifying the OAD distributor of the next block it needs and the OAD distributor sending the requested image block until all blocks have been transferred.

Completion of the OAD Process

After receiving the complete image, OAD application will transit to OAD_COMPLETE state and then trigger a reset. After reset the secure bootloader will start the new image validation.