Debugging

Debug Interfaces

The CC23xx platform supports SWD interfaces. Debug probe that support SWD like the TI XDS110 can work natively with the CC23xx. The hardware resources included on the devices for debugging are listed as follows. Not all debugging functionality is available in all combinations of debug probe and IDE.

  • Flash Patch and Breakpoint Unit (FPB) - 6 instruction comparators, 2 literal comparators

  • Data Watchpoint and Trace Unit (DWT) - 5 watchpoints on memory access

  • Instrumentation Trace Macrocell (ITM) - 32 x 32 bit stimulus registers

  • Trace Port Interface Unit (TPIU) - serialization and time-stamping of DWT and ITM events

XDS110 Debug Probe

The CC23xx LaunchPad support a 20-pin LP-EM debug connector, and the XDS110ET LaunchPad is the assumed debug probe for most development.

The XDS110 is the latest entry level debug probe (emulators) for TI embedded processors. Designed to be a complete solution that delivers JTAG and SWD connectivity at a low cost, the XDS110 is the debug probe of choice for entry-level debugging of TI microcontrollers, processors and SimpleLink devices. Also, both Core Processor and System Trace are available for all Arm and DSP devices that support Embedded Trace Buffer (ETB).

It is also possible to buy the XDS110 JTAG Debug Probe or use the XDS110 existing on-board another SimpleLink LaunchPad.

Configuring Debugger in Code Composer Studio

If only one debug probe is attached, CCS will automatically select the connected debug probe when a debug session is started. You can start a debug session by clicking the debug icon img_icon_debug_ccs on the toolbar.

If more than one debug probe is attached when a debug session is started, CCS will prompt you to select a debug probe as seen in Figure 115. CCS will save the selected debug probe in the target configuration for the project.

../_images/ccs_probe_select.png

Figure 115. CCS Probe Selection

To set or change the selected debug probe for a project, it is necessary to set the serial number for the probe in the project’s target configuration.

Find The Serial Number

To find the serial number for XDS110 debug probe, open a command prompt and run the xdsdfu.exe command for your CCS version, e.g. <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -e. For Uniflash, the command will be: <UNIFLASH_INSTALL_DIR>\deskdb\content\TICloudAgent\win\ccs_base\common\uscif\xds110\xdsdfu.exe -e. This will enumerate all the attached XDS110 debug probes. This should result in output like the following.

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -e

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...


<<<< Device 0 >>>>

VID: 0x0451    PID: 0xbef3
Device Name:   XDS110 Embed with CMSIS-DAP
Version:       3.0.0.22
Manufacturer:  Texas Instruments
Serial Num:    LS420073
Mode:          Runtime
Configuration: Standard

Found 1 devices.

C:\>

Configure Serial Number

It may be necessary to set or unset the selected debug probe. Use the following steps to do this.

  1. Open the target configuration file.

../_images/ccs_targetconfig_file_cc23xx.png
  1. Open the Advanced pane.

  1. Choose the top-level debugger entry.

../_images/ccs_targetconfig_probe_cc23xx.png
  1. Enter the serial number.

../_images/ccs_targetconfig_serial.png

It can be done also by open a command prompt and run the xdsdfu.exe command for your CCS version, e.g.

  • <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -m

  • <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -s LS470000 -r

These will first switch XDS110 to DFU mode if it is already in runtime mode, then set the serial number to the LS470000. The output should be like the following.

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -m

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...


<<<< Device 0 >>>>

VID: 0x0451    PID: 0xbef3
Device Name:   XDS110 Embed with CMSIS-DAP
Version:       3.0.0.22
Manufacturer:  Texas Instruments
Serial Num:    L1100JU9
Mode:          Runtime
Configuration: Standard

Switching device into DFU mode.

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -s LS470000 -r

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...

Setting serial number to "LS470000"...

C:\>

Note

More information of the tool can be found in <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\XDS110SupportReadMe.pdf

For XDS100 series debug probes, open a command prompt and run the xds100serial.exe command for your CCS version, e.g. <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds100serial.exe. This should result in output like the following:

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds100serial.exe
Scanning for XDS100 emulators...

VID/PID    Type            Serial #    Description
0403/a6d1  XDS100v3        06EB12213144  Texas Instruments XDS100v3

C:\>

Program Board ID on LP-EM Boards

It is possible that in some very rare circumstances different LP-EM Boards are with the same Board ID or with empty Board ID. In this case:

  • Uniflash may not identify the device correctly

  • CCS may not identify the board correctly

Programming the different Board ID to each board should help. It can be done also by open a command prompt and run the xdsdfu.exe command. Plug only one LP-EM board to the host PC. Unplug all other boards. For CCS version, e.g. <CCS_INSTALL_DIR>\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -p. For Uniflash, the command will be: <UNIFLASH_INSTALL_DIR>\deskdb\content\TICloudAgent\win\ccs_base\common\uscif\xds110\xdsdfu.exe -p. This should result in output like the following:

C:\>c:\ti\ccs1210\ccs\ccs_base\common\uscif\xds110\xdsdfu.exe -p LS47XXXX

USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated.  All rights reserved.

Scanning USB buses for supported XDS110 devices...

Setting serial number prefix to "LS47XXXX"...

The serial prefix was set in EEPROM.
Power cycle the XDS110 for the change to take effect.

After running the command, unplug and re-plug the LP-EM board to the host PC to acknowledge the new Board ID to the host PC.

Getting started with CCS debug interface

This section describes the debug interface offered by CCS. More extensive documentation is provided in the CCS Debug Environment Guide.

Start a debug session

To start a debug session, click on the debug icon. If enabled to do and required, this will trigger a software build. It will also automatically download the binary on the CC23xx device.

Note

The small arrow next to the debug button offers the possibility to modify the Debug Configurations.

If needed, make sure to select the proper process in the Debug View.

../_images/start_debug_session_cc2340.png

Reset the device while debugging

TI recommends to use the default reset command (i.e. click on the img_icon_reset_ccs button or use the shortcut Ctrl+Shift+R). Using other reset commands may lead to unexpected device behavior.

Breakpoints

Comparators in the Flash Patch and Breakpoint Unit (FPB) of the CC23xx LaunchPad are used to break on an instruction fetch. This can be used to patch a function as it is fetched from instruction memory. Or these comparators can be used to supply a Breakpoint (BKPT) instruction to the CPU. These instructions halt the processors operation, waiting for the debug probe.

Considerations

While breakpoints are a useful tool for debugging code online, they have the possibility of altering the execution flow of a piece of code.

Breakpoints and Timing

Synchronous RF protocols are timing sensitive. Breakpoints can easily halt the execution long enough to lose network timing and break the link.

To still be able to debug, place breakpoints as close as possible to where the relevant debug information can be read or step through the relevant code segment to debug.

After you hit a breakpoint and read out the necessary debug information, it is recommended that you reset the device and re-establish the connection.

Breakpoints and Optimization

When compiler optimizations are enabled, toggling a breakpoint on a line of C code may not result in the expected behavior. Some examples include the following.

Code is removed or not compiled in

Toggling a breakpoint in the IDE results in a breakpoint somewhere other than the intended line. Some IDEs disable breakpoints on nonexistent code.

Code block is part of a common subexpression

A breakpoint might be trigged from a function or piece of code near the marked line. This might have been due to the compiler reusing sections.

An if clause is represented by a conditional branch in assembly

A breakpoint inside an if clause always breaks on the conditional statement, even when the condition is not true.

TI recommends selecting an optimization level as low as possible when debugging. See Optimizations for information on modifying optimization levels.

Note

Due to limitation of Cotex-CM0+, the number of breakpoints for CC23xx devices is 4. Check breakpoints limitation of ARM Cortex-CM0+. During programming stage, debugger will use 3. Breakpoints set by application will be ignored if more than one breakpoint is used by the application. It is possible to gain one more breakpoint back by implementing the following steps. Right click on the project, go to Debug As->Debug Configuration->Target, unchecked ‘Enable CIO function use’.

../_images/gain_one_more_breakpoint.png

Breakpoints in CCS

Note

CCS reserves one hardware breakpoint for instruction stepping.

To toggle a breakpoint, do any of the following.

  • Double-click the area to the left of the line number.

  • Press Ctrl + Shift + B.

  • Right-click on the line.

A breakpoint set on line 207 looks like the following.

../_images/ccs_breakpoint_ex.png

Figure 116. Breakpoint on line 207. Debugger halted at start of main().

For an overview of the active and inactive breakpoints, click on ViewBreakpoints.

../_images/ccs_breakpoint_list.png

Figure 117. List of breakpoints. Right-click to edit options, or de-select to deactivate.

To set a conditional break, do as follows.

  1. Right-click the breakpoint in the overview.

  2. Choose Properties.

When debugging, Skip Count and Condition can help skip a number of breaks or only break if a variable is a certain value.

Note

Conditional breaks require a debugger response and may halt the processor long enough to break an active RF connection, or otherwise disrupt timing on the debug target.

Watching Variables and Registers

Debuggers offer several ways of viewing the state of a halted program. Global variables are statically placed during link-time and can end up anywhere in the RAM or Flash of the chip. These variables can be viewed when then target is halted by the debugger through the Watch and Expression windows.

Unless removed due to optimizations, global variables are always available in these views. Local variables or variables that are only valid inside a limited scope are only viewable in that scope. Such variables can also be viewed with the Watch or Expression views, and may also be automatically displayed when breaking or stepping through code.

Considerations

Local variables are often placed in CPU registers and not on the stack. These variables also have a limited lifetime even within the scope in which they are valid. Depending on the optimization performed, a variable placed in a register may not have a cohesive view of the current state of the variable. Some possible solutions are:

  • Move the variable to global scope, so it remains accessible in RAM.

  • Make the variable volatile, so the compiler doesn’t place the value in a register.

  • Make a shadow copy of the variable that is global and volatile.

Variables in CCS

You can view Global Variables by doing either of the following.

  • Select ViewExpressions.

  • Select a variable name in code.

  • Right-click and select Add Watch Expression.

../_images/ccs_watch.png

Figure 118. Variable watch window. Note that you can cast values, get address and sizeof, etc.

  • Select ViewVariables to auto-variables that are present at the current location when stepping through code.

../_images/ccs_locals.png

Figure 119. Local variables. This screenshot is taken during execution of an application function.

Memory Watchpoints

As mentioned in Debug Interfaces, the Data Watchpoint and Trace Unit (DWT module) contains four memory watchpoints that allow breakpoints on memory access. The hardware match functionality looks only at the address. If intended for use on a variable, the variable must be statically allocated.

Note

If a data watchpoint with value match is used, two of the four watchpoints are used.

Watchpoints in CCS

  1. Right-click on a global variable.

  2. Select BreakpointHardware Watchpoint.

  3. Go to the list of breakpoints (ViewBreakpoints).

  4. Right-click and edit the Breakpoint Properties to configure the watchpoint.

../_images/ccs_watchpoint_add.png

Figure 120. Adding a watchpoint on a variable.

This example configuration ensures that if 0x42 is written to the memory location for Characteristic 1 in the Bluetooth Low Energy basic_ble example project the device halts execution.

../_images/ccs_watchpoint_configure.png

Figure 121. Configuring a hardware watchpoint to break on 8-bit write with value 0x42.

Enabling Logging in CCS

The log driver may be used to easily add debug logging capabilities to any project. The main benefit of the log driver is operates entirely through JTAG which means that no UART peripherals are necessary to enable the logging functionality. In other words, you do not have to use up a UART peripheral or modify your project’s UART operation to enable debug logging for your debugging purposes.

Setting up the Logging Functionality

  1. To start, import the desired project into CCS.

    • For this example, Basic BLE project will be used.

  2. Next, add ${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/log/lib/ticlang/m0p/log_cc23x0r5.a to the File Search Path, which is found by right clicking the project → PropertiesBuildArm LinkerFile Search. Click the add icon to add the path. The properties tab should look like the image below when completed correctly. After adding the file path, click Apply and Close.

    ../_images/logging_include_path.png
  3. Add ti_log_Log_ENABLE to the Predefined Symbols. This is also found within the properties of the project. Right click the project → propertiesBuild``|rarr| ``Arm CompilerPredefined Symbols. Add this with the paper icon with the green plus. The properties tab should look like the image below when completed correctly. After adding the predefined symbol, click Apply and Close.

    ../_images/logging_predefined_symbols.png

Setting up Log Modules

  1. Open the Basic BLE SysConfig file. The logging module is configured through SysConfig. Under LOGGING, is a section for log modules. Here, the log modules will be added. Once in the Log Modules SysConfig section, click on ADD to add a Log Module instance. Name the module LogModule_App1. Within this module, make sure the Enable Module check box is checked. Next check the Enable Level DEBUG, Enable Level VERBOSE, and Enable Level INFO. Make set the sink to /ti/log/LogSinkBuf and ensure Logger Sink Instance is set to CONFIG_ti_log_LogSinkBuf_0.

    The module will look like the following if the previous steps are followed.

    ../_images/log_module.png
  2. Add an additional module named LogModule_App2. This module will have the same settings as the first module. Additionally, the Global Parameters section, at the top of the Log Modules needs to be configured. Within the Global Parameters section, check Global Enable Module, then under the Global Log Level Configuration subsection, check Enable Level DEBUG, Enable Level VERBOSE, and Enable Level INFO

  3. Check LOG SINKS module in SysConfig, and verify the name is properly set:

    ../_images/logsink_settings.png

    To test the log function, add the code below into the main function.

    1Log_printf(LogModule_App1, Log_DEBUG, "Hello world")
    
  4. Once this is done, debug and flash the program to the board. While the board is in debug mode, you may open the log by going to ToolsRuntime Object View. After ROV is open, click on LogSinkBuf within ROV, and set the LogSinkBuf to Records, and then click the continuous refresh button to keep the log constantly updating. It should look like this:

    ../_images/log_rov.png

This completes the basic set up for the logging functionality. Additionally, more Log_printf can be added in various locations to indicate different tasks. The debug level may be changed or outright disabled during debugging depending on which parts of the programs you want to debug or would like to receive messages for.

For more information on the log function, make sure to reference the Log Example for a drivers-only example that contains the logging functinoality. The readme for the example also provides valuable insight into how the log driver works and how you can use it in your custom project.

Runtime Object Viewer

Debuggers may include the Runtime Object Viewer (ROV) plug-in that provides insight into the current state of FreeRTOS, including task states, stacks, and so forth.

This section discusses some ROV views useful for debugging and profiling.

Viewing the State of Each Task

The Task Detailed view is useful for seeing the state of each task and its related runtime stack usage. This picture below shows the state the first time the user-thread is called.

../_images/rov_task_detailed_cc2340.png

Figure 122. ROV Task Detail View

The following table explains the column in ROV Task Detail View

Table 28. Task Detail View Item Explanation

Address

The memory location of the Task_Struct instance for each task.

TaskName

The name of the entry function of the task.

Priority

The RTOS priority for the task.

State

Current state of the task.

StackSize

The size of the runtime stack, configured when instantiating a task.

StackPeak

The maximum run-time stack memory used based on watermark in RAM, where the stacks are prefilled with 0xBE and there is a sentinel word at the end of the run-time stack.

StackLimit

The logical top of the runtime stack of the task.

Note

Function calls may push the stack pointer out of the run-time stack, but not actually write to the entire area. A stack peak near stackSize but not exceeding it may indicate stack overflow.

ROV in CCS

To access the ROV while in a debug session in CCS:

../_images/ccs_rov_enable.png

Attention

You can enable live watch on ROV to automatically retrieve up to date information, however, the refreshing rate is not frequent. You can also pause the debugger or manually click refresh button to enforce a ROV information update.

Using the Memory Browser

Debuggers are able to show a representation of the memory on the CC23xx. In CCS, you can index by address or by symbol name.

Basic BLE Task’s stack. Note A5 watermark.

GAPRole Task’s stack has probably overflowed as it is completly filled.

../_images/mem_browser_sbp_stack-cc23xx.png
../_images/mem_browser_gaprole_stack.png

The solution in this case would be to increase the stack size for the failing task and see what the stack peak really is. The stackPeak reported in Figure 122. is relying on how many watermark bytes are overwritten, so it can’t know how much the overrun amounts to.

Because stacks are utilized from higher addresses towards lower addressed (upwards in the picture), stacks that overrun will tend to overwrite data at locations immediately before the stack.

Read CC2340R5 MAC Address via UniFlash

The MAC address of a specific CC2340R5 device may be read through UniFlash. This can be done through the UniFlash GUI or through the UniFlash CLI.

Prerequisites

The user is expected to have/do the following:

  • CC23xx

  • A computer running a supported operating system listed in the Release Notes

  • Latest version of UniFlash

  • Read the UniFlash QuickStart Guide located in {UNIFLASH_INSTALL_DIR}/docs/quick_start_guide/uniflash_quick_start_guide.html

Reading MAC Address through UniFlash GUI

Reading the MAC address through the UniFlash GUI is most useful when the MAC address needs to be read once for testing or documentation. If the value needs to be read as part of some automation process or manufacturing process, then the CLI method discussed in Reading MAC Address through UniFlash CLI.

This step-by-step guide will help you to read the MAC address written to your device through the UniFlash GUI.

  1. While the CC23xx is connected to your computer, open UniFlash.

  2. Launch the device configuration of the CC23xx by using the auto-detect feature or by manually searching for the CC23xx in the New Configuration section and clicking on Start.

    ../_images/cc23xx_Uniflash_Device_Configuration.jpg
  3. Once the device configuration has been launched, navigate to to the Memory tab on the left and click on Read Target Device

    ../_images/cc23xx_Read_Target_Memory.jpg
  4. On the Address search bar on the top left, type 0x4E000058 and click on Go

  5. The device memory will be read and the 0x4E000058 address will be highlighted in the browser.

    ../_images/cc23xx_Uniflash_GUI_Address.jpg
  6. The highlighted data will contain the MAC address of the device.

Reading MAC Address through UniFlash CLI

If the MAC Address must be read due to a fabrication workflow or as part of an automated testing process, then reading the address through the UniFlash Command Line Interface (CLI) will likely be the most useful method.

This step-by-step guide will help you to read the MAC address written to your device through the UniFlash CLI

  1. While the CC23xx is connected to your computer, open UniFlash.

  2. Launch the device configuration of the CC23xx by using the auto-detect feature or by manually searching for the CC23xx in the New Configuration section and clicking on Start.

    ../_images/cc23xx_Uniflash_Device_Configuration.jpg
  3. Once the device configuration has been launched, navigate to to the Standalone Command Line tab on the left and click on Generate Package. This may take a few minutes.

    ../_images/cc23xx_generate_Uniflash_CLI_package.jpg
  4. On the save the generated package to a known location (for example, C:\ti) and unzip the archive that the known location. The newly extracted folder, should look like the following image:

    ../_images/cc23xx_extracted_CLI_package.jpg
  5. Run the one_time_setup.bat script. This script will generated all the necessary setup-files to use the CLI.

  6. Open a command-line and navigate to the newly extracted folder.

    ../_images/cc23xx_extracted_CLI_package_commandline.jpg
  7. Type and run the following command:

    .\dslite-Cortex_M0P.bat --mode memory --config .\user_files\configs\cc2340r5.ccxml --range=0x4E000058,1 --output=result.hex

    The command will read one entire word at memory address 0x4E000058 which will contain the MAC address of the device. The read data will be written to a result.hex file located in the extracted folder.

    ../_images/cc23xx_extracted_CLI_package_command_ran.jpg
    ../_images/cc23xx_extracted_CLI_package_command_output_file.jpg
  8. The file may be read through a hex viewer/editor program. Looking into the file, we see the following:

    ../_images/cc23xx_extracted_CLI_package_command_output_hex_viewer.jpg

The commands specified in this section may be utilized in scripting languages to allow for easy automation.

More information about the UniFlash Command Line Interface may be found in the Quick Start Guide included with your UniFlash installation.

Connect the debugger to a running target

Connecting the debugger to a target can help when you want to see the status of your target after it has been running for several hours, or even days; or if you cannot reproduce a crash with the debugger attached. Once the debugger connected to the target, all the usual functionalities (break points, step-by-step, variable view, memory view…) are available.

This step-by-step guide will help you to configure CCS in order to connect to a running target

  1. While the CC23xx is running the desired project, open CCS.

  2. Open the Target Configurations window by click on View → Target Configurations.

  3. In the Target Configurations window, expand the Projects folder.

  4. Expand your project within the Projects folder inside the Target Configurations window.

  5. Expand the targetConfigs folder.

  6. Right click on CC2340R5.ccxml and click on Launch Selected Configuration

    ../_images/cc23xx_target_configuration_launch.jpg
  7. After a few seconds, CCS will connect to the target and the core will be visible in the Debug window.

  8. Right click on the core and select Connect Target

    ../_images/cc23xx_core_connect_target.jpg
  9. Click on Run → Load → Load Symbols…

  10. Click on Browse Project.

  11. Select your project’s out file and press OK.

  12. Press OK on Load Symbols window.

  13. At this point you are connected to the target and should see where in the project the target is currently located.

Optimizations

Compiler optimizations are great for saving space or speeding up execution. However, these optimizations can be very difficult to debug around. There are multiple levels at which optimization can be turned on or off.

Project-wide optimization settings are the most general. Sometimes, given the constraints of the device, it is impossible to lower the size optimization level. File-wide optimization settings can be used like project-wide optimizations to turn on or off certain settings. The most granular control is using compiler directives to control optimization at a function level.

Optimizations in CCS

Project-Wide Optimizations

Open the project optimization settings by going to Project PropertiesCCS BuildARM CompilerOptimization

../_images/ccs_optim_level_project.png

Figure 123. Project-level optimization setting in CCS

Single-File Optimizations

Note

Do single-file optimizations with care because this also overrides the project-wide preprocessor symbols.

  1. Right-click on the file in the Workspace pane.

  2. Choose Properties.

  3. Change the optimization level of the file using the same menu in the CCS project-wide optimization menu.

Single-Function Optimizations

Warning

Care must be taken when using pragmas, since they are very specific to the toolchain and may render non-reusable code.

Important

The TI ARM Clang compiler does not support single-function optimizations. Use Single File optimizations instead.

For additional details, check section 3 of the TI ARM Clang User’s Guide.

Listing 141. Function-level optimization setting in gcc
#pragma GCC push_options
#pragma GCC optimize ("O0")
static void myFunction(int number)
{
    // ...
    return yourFunction(other_number);
}
#pragma GCC pop_options

Deciphering Exceptions

Several possible exception causes exist. If an exception is caught, an exception handler function can be called. Arm Cortex User Guide describes more about exception handler. There are ways to determine whether the hang up is due to the hard fault. One is to watch the Program Counter (PC) register which will indicate operation in the hard fault handler. The second method is to watch the special-purpose program status registers (xPSR).

../_images/exception_registers.png

Figure 124. Exception Registers

Debugging Memory Problems

This section describes how to debug a situation where the program runs out of memory, either on the heap or on the runtime stack for the individual thread contexts. Exceeding array bounds or dynamically allocating too little memory for a structure corrupts the memory and can cause an exception like INVPC, INVSTATE, IBUSERR to appear in the CFSR register.

Task and System Stack Overflow

If an overflow on the runtime stack of the task or the system stack occurs (as found using the ROV plug-in), perform the following steps.

  1. Note the current size of the runtime stack of each task.

  2. Increase by a few 100 bytes

  3. Reduce the runtime stack sizes so that they are larger than their respective stackPeaks to save some memory.

Check System Flash and RAM Usage With Map File

Both application and stack projects produce a map file which can be used to compute the combined flash and RAM system memory usage. Both projects have their own memory space and both map files must be analyzed to determine the total system memory usage. The map file is in the output folder of the respective project in IAR. To compute the total memory usage, do as follows.

  1. Open the application map file (that is, application.map).

Note

At the end of the file, three lines contain a breakdown of memory usage for read-only code, read-only data, and read/write data.

  1. Add the two values for read-only code and read-only data memory.

Note

This sum is the total flash memory usage for the application project. The read/write data memory is the total RAM usage by the application project.

  1. Note these values.

  2. Open the stack map file.

  3. Compute the same flash and RAM values for the stack project.

  4. Add the total flash memory value from the application with the total flash usage of the stack to determine the total system flash usage.

  5. Add the total RAM usage from the application with the stack to get the total system RAM usage.

For CCS, the map file of the respective project gives a summary of flash and RAM usage. To determine the remaining available memory for each project, see Flash and RAM. Due to section placement and alignment requirements, some remaining memory may be unavailable. The map file memory usage is valid only if the project builds and links successfully.

Debugging Common Heap Issues

The BLE5-Stack uses FreeRTOS heap_4 module for its memory allocation and the memory usage can be viewed using Runtime Object Viewer.

../_images/ccs_heap4_cc2340.png

However, ROV does not provide you where in the software the heap statistics was updated. To have full control on where you want to see the heap usage, you can take advantage of vPortGetHeapStats. Here is an example showing the heap information under advertising and upon connection established using basic_ble example.

  1. Include #include <FreeRTOS.h> and declare global heapStats in app_peripheral.c

    1#include <FreeRTOS.h>
    2
    3// Struct to hold the heap statistics
    4HeapStats_t heapStats;
    
  2. Register for BLEAPPUTIL_ADV_END mask

    1BLEAppUtil_EventHandler_t peripheralAdvHandler =
    2{
    3    .handlerType    = BLEAPPUTIL_GAP_ADV_TYPE,
    4    .pEventHandler  = Peripheral_AdvEventHandler,
    5    .eventMask      = BLEAPPUTIL_ADV_START_AFTER_ENABLE |
    6                      BLEAPPUTIL_ADV_END_AFTER_DISABLE |
    7                      BLEAPPUTIL_ADV_END
    8};
    
  3. Add the following code under Peripheral_AdvEventHandler to handle BLEAPPUTIL_ADV_END mask

     1void Peripheral_AdvEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
     2{
     3    BLEAppUtil_AdvEventData_t *advData = (BLEAppUtil_AdvEventData_t *)pMsgData;
     4
     5    switch(event)
     6    {
     7        case BLEAPPUTIL_ADV_END:
     8        {
     9            //get heap status here
    10            vPortGetHeapStats(&heapStats);
    11            break;
    12        }
    
  4. Add the following code under Peripheral_GAPConnEventHandler to get heap information when connection is established

    1void Peripheral_GAPConnEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
    2{
    3    case BLEAPPUTIL_LINK_ESTABLISHED_EVENT:
    4    {
    5        gapEstLinkReqEvent_t *gapEstMsg = (gapEstLinkReqEvent_t *)pMsgData;
    6        vPortGetHeapStats( &heapStats );
    

After programming the device, you can go to Expressions and enable live watch. You can then observe that the xNumberOfSuccessfulAllocations and xNumberOfSuccessfulFrees continue increasing when the advertising event is ongoing where the rest of the fields stay constant, this indicates that there is no memory leak during advertising.

../_images/ccs_heap4_cc2340_adv_end_stats.png

After connection established, you will see that the xAvailableHeapSpaceInBytes decrease which is due to BLE5-Stack allocates memory for connection related information.

../_images/ccs_heap4_cc2340_conn_est_stats.png

Troubleshooting Heap Problems

Issues with dynamic allocated memory can be notoriously hard to track down and debug; this section aims to give tips on how to debug the most common issues with dynamic memory.

Writing to already freed memory

Pointers to memory which have already been freed using ICall_free() should not be used. A common practice is to set pointers to NULL after they have been freed, and check them for NULL before using them. Writing a an already freed pointer will cause assert.

 1  // Allocate Memory
 2  uint32_t *myPtr = ICall_malloc(500);
 3
 4  //..
 5
 6  // Later free the pointer, set it to NULL
 7  ICall_free(myPtr);
 8  myPtr = NULL;
 9
10  // This check will protect against writing to already freed memory
11  if( NULL != myPtr)
12  {
13    *myPtr = 42;
14  }

Freeing Already freed Memory

The cause of this bug is the same as the one from the previous section, double frees will trigger assert in heap_4.

1  // Allocate Memory
2  uint32_t *myPtr = ICall_malloc(500);
3
4  //..
5
6  ICall_free(myPtr);
7  ICall_free(myPtr);

ICall Abort

ICall abort is a function call used to indicate a serious failure in the ICall or OSAL mechanism used by the stack.

The BLE Stack will call ICall_abort() when one of the below happens:

  • Calling a stack function through ICall in a stack callback or TI-RTOS/FreeRTOS SWI or HWI

  • Misconfiguring of additional ICall tasks or entities (usually when OSAL_MAX_NUM_PROXY_TASKS + 1 < than number of ICall tasks)

  • Incorrect ICall task registering

  • Stack API call timed out while ICall is waiting for a response

  • ICall encountered an error while executing a stack API

  • ICall_primSetTimer() or ICall_setTimer() are unable to create a clock object

By default ICall_abort() will raise a HAL assert if they are enabled. You can set a breakpoint in the HAL assert handler and inspect the call stack to understand the function that called the abort. If HAL asserts are not enabled then the abort function will spin lock. The user can set a breakpoint in ICall abort to see what is causing the abort. See the HAL Assert Handling section for more information.

HAL Assert Handling

The HAL Assert module defines a mechanism for handling undesirable or unrecoverable state states in the code. The HAL Assert module is intended to be configurable and shared between the application and stack.

HAL Assert Design

The HAL_ASSERT() macro from hal_assert.h can be used to process a failure state or condition. The way this macro is evaluated corresponds to how the HAL assert module is configured. There are two types of HAL Assert:

  • Legacy HAL Assert

  • Extended HAL Assert

Legacy HAL assert will execute the halAssertHandler() from hal_assert.c. The implementation of halAssertHandler() is controlled by preprocessor defines that are explained in the next section.

Extended HAL assert will execute halAssertHandlerExt() from hal_assert.c. This extended handler will execute any user provided callbacks before executing the default halAssertHandler(). The user provided callback will contain information including the cause and subcause of the error. The subcause can be set with the HAL_ASSERT_SET_SUBCAUSE() macro before executing HAL_ASSERT().

Attention

TI recommends that extended HAL asserts are always used whenever possible to ensure the most debugging features.

HAL Assert configuration

The behavior of the HAL Assert module is based on both the selection of preprocessor defines and the call to halAssertInit().

  • EXT_HAL_ASSERT: Enables extended HAL asserts

  • HAL_ASSERT_RESET: Reset on assert using HAL_SYSTEM_RESET()

  • HAL_ASSERT_SPIN: Spinlock on assert using halAssertSpinlock()

  • HAL_ASSERT_LIGHTS should never be used.

To fully enable extended HAL Asserts halAssertInit() must be called with HAL_ASSERT_LEGACY_MODE_DISABLED, otherwise the user supplied callback will not be executed.

Adding HAL Assert Support To the Application

Single Project

Define EXT_HAL_ASSERT in the app project predefined symbols list. halAssertInit() is initilized by the stack in ble_user_config_stack.c for examples that do not have a stack project.

Stack Library

In the stack library configuration, the stack and application images are combined, and no action is needed to use HAL asserts in the application layer or to plug the user call back using RegisterAssertCback(). (For stack library configuration, there is no need to define EXT_HAL_ASSERT in the app project.)

Split Image

The HAL assert code must live on both the stack and the application side in order for the user to supply a callback via RegisterAssertCback() or to use HAL asserts in the application. This includes

  • Adding hal_assert.c to the application project

  • Defining EXT_HAL_ASSERT in the application project as a preprocessor symbol

HAL Assert Causes and Explanation

As mentioned above, the BLE-Stack will use HAL_ASSERT() to trap in the case a failure state is encountered. By default, asserts will be sent to the AssertHandler() function that is provided in main.c of the TI sample applications. The table below describes the various HAL assert types that are used in the stack and what they mean. This table assumes EXT_HAL_ASSERT is defined as recommended above.

HAL Assert Cause

Reason

HAL_ASSERT_CAUSE_OUT_OF_MEMORY

Malloc failed when HEAPMGR_METRICS and MEM_ALLOC_ASSERT are defined

HAL_ASSERT_CAUSE_OUT_OF_MEMORY

Critical callbacks cannot be allocated by the GAP central or peripheral link managers or SM

HAL_ASSERT_CAUSE_RF_DRIVER_ERROR

RF error callback is executed by RF driver.

HAL_ASSERT_CAUSE_ICALL_ABORT

ICall has encountered a critical error and needs to abort using ICall_abort(). See ICall Abort section for more information

HAL_ASSERT_CAUSE_ICALL_TIMEOUT

A stack API that was executed via ICall took longer than ICALL_TIMEOUT_PREDEFINE to return. This usually means that the stack has hung.

HAL_ASSERT_CAUSE_INTERNAL_ERROR

When a split image application executes an API call that is not available in the stack image.

HAL_ASSERT_CAUSE_UNEXPECTED_ERROR

Used by NPI UART and SPI transport layers to indicate the the driver is already in use

HCI Hardware Errors

HCI Hardware errors are another mechanism by which the BLE-Stack may indicate that it has encountered an unrecoverable or unexpected state.

The stack will use ICall/OSAL to send a message to the app’s message queue with more information about the failure.

HCI hardware errors can be masked by the application using the HCI_SetEventMaskCmd(), but this is not the default behavior.

Registering for HCI Hardware Errors

By default the TI provided sample applications will register for HCI events, and process them using the _processStackMsg function within the application.

HCI hardware errors will be sent to the application as HCI_GAP_EVENT_EVENT with an event code of HCI_BLE_HARDWARE_ERROR_EVENT_CODE. For more on processing HCI events in the application, please see Host Controller Interface (HCI).

By default the sample applications will assert when a HCI Hardware error is received, using the same assert handler as the extended HAL asserts (AssertHandler()).

Decoding Hardware Error Reason

In the application’s _processStackMsg(ICall_Hdr *pMsg) function, there is a case for HCI_GAP_EVENT_EVENT which has a subcase where HCI_BLE_HARDWARE_ERROR_EVENT_CODE is processed.

The case for the hardware error processing can be enhanced to expose the error code like so:

case HCI_BLE_HARDWARE_ERROR_EVENT_CODE:
{
    hciEvt_HardwareError_t *hardCode =(hciEvt_HardwareError_t*)pMsg;
    AssertHandler(HAL_ASSERT_CAUSE_HARDWARE_ERROR, hardCode->hardwareCode);
}

A breakpoint can be set in this function to determine the error code. This code should be reported to a TI engineer when experiencing a HCI hardware assert. These error codes are defined in ll_common.h and hci.h.

Debugging RF Output

As mentioned in the CC23xx SimpleLink Wireless MCU Technical Reference Manual, the RF output can be mapped to pins on the LaunchPad for RF signal debugging. These pins are intended to be used when connecting an RF range extender. However, they can also help in instances where it is unclear if the device is transmitting or receiving in the right window.

To enable RF output debugging, you will need to map the RF Core LNA enable and PA enable output or Tx start signals to a GPIO. The code snippet below shows how to use DIO11 (radio TX) and DIO21 (radio RX). By connecting a logic analyzer to these pins, the RF activity over time can be recorded.

  1. Initialize these IOs in your main function with the following content:

    Listing 143. Initialize IOs
    /*******************************************************************************
     * INCLUDES
    */
    #include DeviceFamily_constructPath(inc/hw_types.h)
    #include DeviceFamily_constructPath(inc/hw_ioc.h)
    #include DeviceFamily_constructPath(inc/hw_memmap.h)
    
    // ...
    
    int main()
    {
        // ...
    
        /*
         * Add the following after Board_init();
         * Be sure IOIDs used below are not used by any entries in PIN or
         * GPIO tables from the board files
         */
    
        /* IO for TX Indication */
        HWREG(IOC_BASE + IOC_O_IOC11) |= IOC_IOC11_PORTCFG_PFUNC4;
    
        /* IO for RX Indication */
        HWREG(IOC_BASE + IOC_O_IOC21) |= IOC_IOC21_PORTCFG_PFUNC5;
    
        // ...
    }
    
  2. Declare the RCL_Tracer_enable function in your application file with the following content:

    Listing 144. Enable RF Observables
    /*******************************************************************************
     * INCLUDES
    */
    #include DeviceFamily_constructPath(driverlib/dbell_regs.h)
    
    // ...
    
    /* ======== RCL_Tracer_enable ======== */
    void RCL_Tracer_enable(void)
    {
      /* TX, RX Indication */
      HWREG_WRITE_LRF(LRFDDBELL_BASE + LRFDDBELL_O_GPOSEL0) = HWREG_READ_LRF(LRFDDBELL_BASE + LRFDDBELL_O_GPOSEL0) | LRFDDBELL_GPOSEL0_SRC0_RFEGPO0;
      HWREG_WRITE_LRF(LRFDDBELL_BASE + LRFDDBELL_O_GPOSEL0) = HWREG_READ_LRF(LRFDDBELL_BASE + LRFDDBELL_O_GPOSEL0) | LRFDDBELL_GPOSEL0_SRC1_RFEGPO1;
    }
    
    // ...
    

Note

There is no retention of S_DBELL_GPOSEL0, therefore, the setting will disappear after entering standby. This is why we use RCL_Tracer_enable to circumvent losing the configuration. This function will automatically be called by the Radio Control Layer (RCL) each time the radio is restarting. By default it is defined as weak function in the RCL and can be overriden by application code.

Warning

The pins used for the RF observables cannot be changed.

Packet Sniffer

In order to determine what is going on over the air, it’s recommended to have a packet sniffer that can track BLE advertisement packets as well as an established BLE connection.

Note

SmartRF Protocol Packet Sniffer and SmartRF Packet Sniffer 2 can be used for Bluetooth LE debugging when working with any Bluetooth LE compatible devices, including the CC23xx devices. However, the CC23xx devices cannot be used as sampling device for the Packet Sniffer tools. Refer to the “Required Hardware” section for more details.

Install the Required Software

Download and install the following software:

Important

It is important that you use the appropriate version of Wireshark. Please find the version you need in the SmartRF Packet Sniffer 2 User’s Guide, under ‘Getting Started > Installation’.

Required Hardware

Any device from the CC13xx and CC26xx family which supports BLE commands can be used as a sniffer. Following is a list of all supported development boards:

Uniflash Setup

  1. Connect the LaunchPad via USB

  2. Start Uniflash

  3. Connected device should be under ‘Detected Devices’. Click Start.

    • If it is not, choose your device type from ‘New Configuration’. Click Start.

../_images/uniflash_connected_devices.png

Figure 125. Connected Devices Displayed on Uniflash.

  1. Browse for the Flash image corresponding to your device under <SmartRF Tools installpath>\SmartRF Packet Sniffer 2\sniffer_fw\bin. Click Load Image.

../_images/browse_flash_image.png

Figure 126. Browse for and Load Image on Uniflash.

SmartRF Sniffer Agent Setup

  1. Start SmartRF Sniffer Agent.

  2. Select Options->Data->Data Out. Check Use Pipe and click ‘OK’.

../_images/smartrf_sniffer_use_pipe.png

Figure 127. Select Use Pipe for Data Out

  1. Click Detect Devices to find the sniffer device.

    -If it does not show up, disconnect and reconnect the device and try again.

  2. Once your device is discovered click the checkbox under ‘Use’ and then click ‘Configure’.

../_images/smartrf_configure_device.png

Figure 128. Configure the Sniffer Device

  1. Use the settings shown for BLE configuration.

    -For BLE, use advertising channel 37, 38, or 39. -The sniffer can be configured to follow a connection between a specific BLE Central (initiator) and Peripheral device. Click the checkbox next to ‘Connect to Initiator Address’ and write the address of the Central (Initiator) device. The address of the device is printed to the display in most of our examples, but can also be found using an external tool such as the SimpleLink Starter mobile app. If this option is not selected, the device will follow the first connection that appears on the channel that was selected.

    ../_images/smartrf_bleconfig.png

    Settings for BLE configuration.

  1. Click ‘OK’, then press ‘Start All’. -The ‘Incoming Packets’ indicator should turn green, and the ‘Outgoing Packets’ indicator should turn blue. Shown below.~

    ../_images/smartrf_indicators.png

Wireshark Setup

  1. Create a new Wireshark desktop shortcut. Modify the Target setting by adding -i\\.\pipe\tiwspc_data -k to the end of the current target entry.

../_images/wireshark_modify_target.png

Figure 129. Modifying the target entry.

  1. Run Wireshark from the new shortcut.

  2. The packets should now be displayed.

../_images/wireshark_packets.png

Figure 130. Example BLE packets displayed using Wireshark.

Debugging guide for serial interfaces

The aim of this chapter is to give some pointers on what to check if some issues are seen when using the UART, SPI, or I2C interfaces.

Note: TI only supports how to use the serial interface modules and the TI supplied drivers for these interfaces. TI are not able to help on the usage of a non-TI device connected to I2C, SPI or UART.

I2C

  • The I2C interface needs an external pull-up resistor. On the LauchPad these are 3.3 kOhm.

  • Measure the waveform on the I2C interface with an oscilloscope to verify the SCL and SDA levels

  • Monitor the interface with a logic analyzer. Check that data on the bus is the same as the wanted data.

  • Check the interface by reading out the device ID of the sensor.

  • Check the slave address. The I2C module uses a 7-bit address. The last 8th bit is the data direction bit. This last bit is appended automatically by the driver/HW. The Slave address given to the driver has therefore to be 7-bit.

  • Ensure that the readCount and writeCount is according to the register size used. If the result register in the sensor is 16-bit, the readCount has to be set to 2.

SPI

  • Monitor the interface with a logic analyzer. Compare the waveform with the waveform given in the datasheet for the device you are communicating with.

  • Check that the CSn is set correctly.

  • Check that the frame format is set correctly. Check if the device you are communicating with uses SPO = 1 or 0 and SPH = 1 or 0.

UART

  • Make sure to connect the TX pin of one device to the RX pin of the other device, and vice versa. If flow control is enabled, then the same applies towards the CTS and RTS pins.

  • Verify all communication settings between devices, including baud rate, data length, stop/parity bits and flow control.

  • Evaluate the interface with a logic analyzer or oscilloscope, using an analyzer tool if possible to convert the waveforms into their numerical counterpart.

Low Power Optimizations

If the device seems to be drawing too much current for your application, the following section will guide through the most common issues.

Note

Please refer to EnergyTrace User Guide as well as the Current Consumption Application Note for how to setup device for current consumption testing.

  • Check if the debugger is currently detached from the device. If using the XDS110 as debuger make sure to only connect the Ground and Power pins (this can be accomplished with jumper cables).

../_images/Mod_LP_Config_2.png

Figure 131. Modular LP EnergyTrace stand-alone Configuration

Warning

Confirm that the device has been power cycled since last time it was connected to the debugger.

  • Isolate the CC23xx from all peripheral devices (such as LEDS, External Flash, etc..) as these leakage currents might be the cause of higher power consumption than expected. If using a Launchpad confirm all jumpers are removed.

  • Isolate threads in the application until the thread with high power consumption is found. Once found, start isolating which peripherals (UART, I2C, SPI, ADC, Timers) are used in the thread and check if one of these could be the source of the issue. If any peripheral is set to start a transfer in blocking mode, the CC23xx will not be able to go into standby if the transfer never finished. Ex, if UART is set to restart receiving in blocking mode, the device will not go into standby until the expected data is received.

Debugging LF/HF Clock Output

As mentioned in the CC23xx SimpleLink Wireless MCU Technical Reference Manual, the DTB can be used to access internal signals. The LF (Low Frequency) and HF (High Frequency) crystal clock signals can be mapped to pins on the LaunchPad for signal debugging, for example to analyze the clock accuracy or to correlate against sniffer log events.

The code snippet below shows how to use DIO19 for observing the HF crystal or LF crystal clock signals, for example with a logic analyzer.

Initialize these IOs in your main function with the following content:

Listing 145. Map HF or LF crystal clock to DIO19
 /*******************************************************************************
 * INCLUDES
 */
 #include <ti/drivers/GPIO.h>
 #include DeviceFamily_constructPath(inc/hw_types.h)
 #include DeviceFamily_constructPath(inc/hw_memmap.h)
 #include DeviceFamily_constructPath(inc/hw_ckmd.h)
 #include DeviceFamily_constructPath(inc/hw_ioc.h)
 #include DeviceFamily_constructPath(inc/hw_pmctl.h)

 // ...

 int main()
 {
     // ...

     /*
      * Add the following after Board_init();
      * Be sure IOID used below is not used by any entries in PIN or
      * GPIO tables from the board files.
      * The clock source can be switched with constant clockSrc.
      */

     uint8_t clockSrc = 0xC; //for HF crystal clock divided by 8
     //  uint8_t clockSrc = 0xF; //for LF crystal clock

     // drive output low first
     GPIO_setConfig(19, GPIO_CFG_OUTPUT | GPIO_CFG_OUT_LOW);

     // Configure the IOC.IOC19.PORTCFG MMR to select DTB
     HWREG(IOC_BASE + IOC_O_IOC19) &= ~IOC_IOC19_PORTCFG_M;
     HWREG(IOC_BASE + IOC_O_IOC19) |= IOC_IOC19_PORTCFG_DTB;

     // Make sure the DTB mux selects in IOC (and if required in
     // source clock IP) are reset that zero is driven on DTB0.
     // ULLSEL mux select (select CKMD)
     HWREG(IOC_BASE + IOC_O_DTBCFG) &= ~IOC_DTBCFG_ULLSEL_M;
     HWREG(IOC_BASE + IOC_O_DTBCFG) |= 0x1 << IOC_DTBCFG_ULLSEL_S; // 0x1 to route CKMD to DTB0

     // Enable IOC.DTBOE.EN0
     HWREG(IOC_BASE + IOC_O_DTBOE) &= ~IOC_DTBOE_EN0_M;
     HWREG(IOC_BASE + IOC_O_DTBOE) |= IOC_DTBOE_EN0_EN;

     // select which clock (CKMD) to output on DTB0 (DTB[0])
     HWREG(CKMD_BASE + CKMD_O_DTBCTL) &= ~CKMD_DTBCTL_CLKSEL_M;
     HWREG(CKMD_BASE + CKMD_O_DTBCTL) |= (clockSrc) << CKMD_DTBCTL_CLKSEL_S;

     // enable DTB output
     HWREG(CKMD_BASE + CKMD_O_DTBCTL) &= ~CKMD_DTBCTL_EN_M;
     HWREG(CKMD_BASE + CKMD_O_DTBCTL) |= CKMD_DTBCTL_EN;

     // ...
 }

Note

The clock source can be selected with the variable clockSrc. Please refer to the DTBCTL register field description in the CC23xx SimpleLink Wireless MCU Technical Reference Manual for the clock source. The HF crystal clock should be mapped as a divided clock, as the IO pin output frequency is limited.

Note

Alternatively DTB0 can be mapped to DIO12 by setting DTBCFG.PADSEL bit field to 0x5. Other pins cannot output DBT0 signals.

When the HF crystal clock divided by 8 is selected in the above example, the output signal of 6 MHz can be observed (48 MHz / 8 = 6 MHz). When the LF crystal clock is selected in the above example, then the output signal of 32.768 kHz can be expected.

The HF crystal clock is automatically disabled when the device enters standby mode and the clock is re-enabled when the device wakes up from standby. As a result, only short bursts of HF crystal clock might be observed in a typical Bluetooth LE application (such as basic_ble). These bursts represent the active mode phases of the device. For enabling permanent HF crystal clock output please select Power Policy Function PowerCC23X0_doWFI in the SysConfig - TI DRIVERS - Power module. Alternatively the device is also permanently in active mode during a debug session in CCS.

../_images/syscfg_power_policy_do_wfi_cc2340.png

Figure 132. Power Policy Function in SysConfig

Note

The LF crystal clock is permanently enabled in standby mode.