CC26xx Driver Library
pka.c File Reference
#include "pka.h"

Macros

#define MAX(x, y)    (((x) > (y)) ? (x) : (y))
 
#define MIN(x, y)    (((x) < (y)) ? (x) : (y))
 
#define INRANGE(x, y, z)    ((x) > (y) && (x) < (z))
 
#define PKA_MAX_CURVE_SIZE_32_BIT_WORD   12
 
#define PKA_MAX_LEN_IN_32_BIT_WORD   PKA_MAX_CURVE_SIZE_32_BIT_WORD
 
#define PKA_NO_POINTER_REG   0xFF
 

Functions

static uint32_t PKAWritePkaParam (const uint8_t *param, uint32_t paramLength, uint32_t paramOffset, uint32_t ptrRegOffset)
 
static uint32_t PKAWritePkaParamExtraOffset (const uint8_t *param, uint32_t paramLength, uint32_t paramOffset, uint32_t ptrRegOffset)
 
static uint32_t PKAGetBigNumResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)
 
static uint32_t PKAGetBigNumResultRemainder (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)
 
static uint32_t PKAGetECCResult (uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length)
 
uint32_t PKAGetOpsStatus (void)
 Gets the PKA operation status. More...
 
bool PKAArrayAllZeros (const uint8_t *array, uint32_t arrayLength)
 Checks whether and array only consists of zeros. More...
 
void PKAZeroOutArray (const uint8_t *array, uint32_t arrayLength)
 Zeros-out an array. More...
 
uint32_t PKABigNumModStart (const uint8_t *bigNum, uint32_t bigNumLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr)
 Starts a big number modulus operation. More...
 
uint32_t PKABigNumModGetResult (uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr)
 Gets the result of the big number modulus operation. More...
 
uint32_t PKABigNumDivideStart (const uint8_t *dividend, uint32_t dividendLength, const uint8_t *divisor, uint32_t divisorLength, uint32_t *resultQuotientMemAddr, uint32_t *resultRemainderMemAddr)
 Starts a big number divide operation. More...
 
uint32_t PKABigNumDivideGetQuotient (uint8_t *resultBuf, uint32_t *length, uint32_t resultQuotientMemAddr)
 Gets the quotient of the big number divide operation. More...
 
uint32_t PKABigNumDivideGetRemainder (uint8_t *resultBuf, uint32_t *length, uint32_t resultQuotientMemAddr)
 Gets the remainder of the big number divide operation. More...
 
uint32_t PKABigNumCmpStart (const uint8_t *bigNum1, const uint8_t *bigNum2, uint32_t length)
 Starts the comparison of two big numbers. More...
 
uint32_t PKABigNumCmpGetResult (void)
 Gets the result of the comparison operation of two big numbers. More...
 
uint32_t PKABigNumInvModStart (const uint8_t *bigNum, uint32_t bigNumLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr)
 Starts a big number inverse modulo operation. More...
 
uint32_t PKABigNumInvModGetResult (uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr)
 Gets the result of the big number inverse modulo operation. More...
 
uint32_t PKABigNumMultiplyStart (const uint8_t *multiplicand, uint32_t multiplicandLength, const uint8_t *multiplier, uint32_t multiplierLength, uint32_t *resultPKAMemAddr)
 Starts the multiplication of two big numbers. More...
 
uint32_t PKABigNumMultGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)
 Gets the result of the big number multiplication. More...
 
uint32_t PKABigNumAddStart (const uint8_t *bigNum1, uint32_t bigNum1Length, const uint8_t *bigNum2, uint32_t bigNum2Length, uint32_t *resultPKAMemAddr)
 Starts the addition of two big numbers. More...
 
uint32_t PKABigNumSubGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)
 Gets the result of the subtraction operation on two big numbers. More...
 
uint32_t PKABigNumSubStart (const uint8_t *minuend, uint32_t minuendLength, const uint8_t *subtrahend, uint32_t subtrahendLength, uint32_t *resultPKAMemAddr)
 Starts the subtraction of one big number from another. More...
 
uint32_t PKABigNumAddGetResult (uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)
 Gets the result of the addition operation on two big numbers. More...
 
uint32_t PKAEccMultiplyStart (const uint8_t *scalar, const uint8_t *curvePointX, const uint8_t *curvePointY, const uint8_t *prime, const uint8_t *a, const uint8_t *b, uint32_t length, uint32_t *resultPKAMemAddr)
 Starts ECC multiplication. More...
 
uint32_t PKAEccMontgomeryMultiplyStart (const uint8_t *scalar, const uint8_t *curvePointX, const uint8_t *prime, const uint8_t *a, uint32_t length, uint32_t *resultPKAMemAddr)
 Starts ECC Montgomery multiplication. More...
 
uint32_t PKAEccMultiplyGetResult (uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length)
 Gets the result of ECC multiplication. More...
 
uint32_t PKAEccAddStart (const uint8_t *curvePoint1X, const uint8_t *curvePoint1Y, const uint8_t *curvePoint2X, const uint8_t *curvePoint2Y, const uint8_t *prime, const uint8_t *a, uint32_t length, uint32_t *resultPKAMemAddr)
 Starts the ECC addition. More...
 
uint32_t PKAEccAddGetResult (uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length)
 Gets the result of the ECC addition. More...
 
uint32_t PKAEccVerifyPublicKeyWeierstrassStart (const uint8_t *curvePointX, const uint8_t *curvePointY, const uint8_t *prime, const uint8_t *a, const uint8_t *b, const uint8_t *order, uint32_t length)
 Begins the validation of a public key against a Short-Weierstrass curve. More...
 

Variables

const PKA_EccPoint224 NISTP224_generator
 X coordinate of the generator point of the NISTP224 curve. More...
 
const PKA_EccParam224 NISTP224_prime
 Prime of the NISTP224 curve. More...
 
const PKA_EccParam224 NISTP224_a
 a constant of the NISTP224 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam224 NISTP224_b
 b constant of the NISTP224 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam224 NISTP224_order
 Order of the NISTP224 curve. More...
 
const PKA_EccPoint256 NISTP256_generator
 X coordinate of the generator point of the NISTP256 curve. More...
 
const PKA_EccParam256 NISTP256_prime
 Prime of the NISTP256 curve. More...
 
const PKA_EccParam256 NISTP256_a
 a constant of the NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam256 NISTP256_b
 b constant of the NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam256 NISTP256_order
 Order of the NISTP256 curve. More...
 
const PKA_EccPoint384 NISTP384_generator
 X coordinate of the generator point of the NISTP384 curve. More...
 
const PKA_EccParam384 NISTP384_prime
 Prime of the NISTP384 curve. More...
 
const PKA_EccParam384 NISTP384_a
 a constant of the NISTP384 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam384 NISTP384_b
 b constant of the NISTP384 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam384 NISTP384_order
 Order of the NISTP384 curve. More...
 
const PKA_EccPoint521 NISTP521_generator
 X coordinate of the generator point of the NISTP521 curve. More...
 
const PKA_EccParam521 NISTP521_prime
 Prime of the NISTP521 curve. More...
 
const PKA_EccParam521 NISTP521_a
 a constant of the NISTP521 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam521 NISTP521_b
 b constant of the NISTP521 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam521 NISTP521_order
 Order of the NISTP521 curve. More...
 
const PKA_EccPoint256 BrainpoolP256R1_generator
 X coordinate of the generator point of the BrainpoolP256R1 curve. More...
 
const PKA_EccParam256 BrainpoolP256R1_prime
 Prime of the BrainpoolP256R1 curve. More...
 
const PKA_EccParam256 BrainpoolP256R1_a
 a constant of the BrainpoolP256R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam256 BrainpoolP256R1_b
 b constant of the BrainpoolP256R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam256 BrainpoolP256R1_order
 Order of the BrainpoolP256R1 curve. More...
 
const PKA_EccPoint384 BrainpoolP384R1_generator
 X coordinate of the generator point of the BrainpoolP384R1 curve. More...
 
const PKA_EccParam384 BrainpoolP384R1_prime
 Prime of the BrainpoolP384R1 curve. More...
 
const PKA_EccParam384 BrainpoolP384R1_a
 a constant of the BrainpoolP384R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam384 BrainpoolP384R1_b
 b constant of the BrainpoolP384R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam384 BrainpoolP384R1_order
 Order of the BrainpoolP384R1 curve. More...
 
const PKA_EccPoint512 BrainpoolP512R1_generator
 X coordinate of the generator point of the BrainpoolP512R1 curve. More...
 
const PKA_EccParam512 BrainpoolP512R1_prime
 Prime of the BrainpoolP512R1 curve. More...
 
const PKA_EccParam512 BrainpoolP512R1_a
 a constant of the BrainpoolP512R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam512 BrainpoolP512R1_b
 b constant of the BrainpoolP512R1 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More...
 
const PKA_EccParam512 BrainpoolP512R1_order
 Order of the BrainpoolP512R1 curve. More...
 
const PKA_EccPoint256 Curve25519_generator
 X coordinate of the generator point of the Curve25519 curve. More...
 
const PKA_EccParam256 Curve25519_prime
 Prime of the Curve25519 curve. More...
 
const PKA_EccParam256 Curve25519_a
 a constant of the Curve25519 curve when expressed in Montgomery form (By^2 = x^3 + a*x^2 + x). More...
 
const PKA_EccParam256 Curve25519_b
 b constant of the Curve25519 curve when expressed in Montgomery form (By^2 = x^3 + a*x^2 + x). More...
 
const PKA_EccParam256 Curve25519_order
 Order of the Curve25519 curve. More...
 

Macro Definition Documentation

#define INRANGE (   x,
  y,
 
)    ((x) > (y) && (x) < (z))
#define MAX (   x,
 
)    (((x) > (y)) ? (x) : (y))
#define MIN (   x,
 
)    (((x) < (y)) ? (x) : (y))
#define PKA_MAX_CURVE_SIZE_32_BIT_WORD   12
#define PKA_MAX_LEN_IN_32_BIT_WORD   PKA_MAX_CURVE_SIZE_32_BIT_WORD
#define PKA_NO_POINTER_REG   0xFF

Function Documentation

static uint32_t PKAGetBigNumResult ( uint8_t *  resultBuf,
uint32_t *  resultLength,
uint32_t  resultPKAMemAddr 
)
static

Referenced by PKABigNumAddGetResult(), PKABigNumDivideGetQuotient(), PKABigNumInvModGetResult(), PKABigNumMultGetResult(), and PKABigNumSubGetResult().

659 {
660  uint32_t mswOffset;
661  uint32_t lswOffset;
662  uint32_t lengthInWords;
663  uint32_t i;
664  uint32_t *resultWordAlias = (uint32_t *)resultBuf;
665 
666  // Check the arguments.
667  ASSERT(resultBuf);
668  ASSERT((resultPKAMemAddr > PKA_RAM_BASE) &&
669  (resultPKAMemAddr < (PKA_RAM_BASE + PKA_RAM_TOT_BYTE_SIZE)));
670 
671  // Verify that the operation is complete.
672  if (HWREG(PKA_BASE + PKA_O_FUNCTION) & PKA_FUNCTION_RUN) {
674  }
675 
676  // Get the MSW register value.
677  mswOffset = HWREG(PKA_BASE + PKA_O_MSW);
678 
679  // If the result vector is zero, write back one zero byte so the caller does not need
680  // to handle a special error for the perhaps valid result of zero.
681  // They will only get the error status if they do not provide a buffer
682  if (mswOffset & PKA_MSW_RESULT_IS_ZERO_M) {
683  if (resultLength && resultBuf && *resultLength){
684 
685  resultBuf[0] = 0;
686  *resultLength = 1;
687 
688  return PKA_STATUS_SUCCESS;
689  }
690  else {
692  }
693  }
694 
695  // Get the length of the result
696  mswOffset = ((mswOffset & PKA_MSW_MSW_ADDRESS_M) + 1);
697  lswOffset = ((resultPKAMemAddr - PKA_RAM_BASE) >> 2);
698 
699  if (mswOffset >= lswOffset) {
700  lengthInWords = mswOffset - lswOffset;
701  }
702  else {
704  }
705 
706  // Check if the provided buffer length is adequate to store the result data.
707  if (resultLength && (*resultLength < lengthInWords * sizeof(uint32_t))) {
709  }
710 
711  // Copy the resultant length.
712  *resultLength = lengthInWords * sizeof(uint32_t);
713 
714  if (resultBuf) {
715  // Copy the result into the resultBuf.
716  for (i = 0; i < lengthInWords; i++) {
717  resultWordAlias[i]= HWREG(resultPKAMemAddr + sizeof(uint32_t) * i);
718  }
719  }
720 
721  return PKA_STATUS_SUCCESS;
722 }
#define PKA_STATUS_BUF_UNDERFLOW
Buffer underflow.
Definition: pka.h:123
#define PKA_STATUS_RESULT_ADDRESS_INCORRECT
The address of the result passed into one of the PKA*GetResult functions is incorrect.
Definition: pka.h:136
#define PKA_STATUS_OPERATION_BUSY
PKA operation is in progress.
Definition: pka.h:128
#define PKA_STATUS_SUCCESS
Success.
Definition: pka.h:120
#define ASSERT(expr)
Definition: debug.h:73
static uint32_t PKAGetBigNumResultRemainder ( uint8_t *  resultBuf,
uint32_t *  resultLength,
uint32_t  resultPKAMemAddr 
)
static

Referenced by PKABigNumDivideGetRemainder(), and PKABigNumModGetResult().

730 {
731  uint32_t regMSWVal;
732  uint32_t lengthInWords;
733  uint32_t i;
734  uint32_t *resultWordAlias = (uint32_t *)resultBuf;
735 
736  // Check the arguments.
737  ASSERT(resultBuf);
738  ASSERT((resultPKAMemAddr > PKA_RAM_BASE) &&
739  (resultPKAMemAddr < (PKA_RAM_BASE + PKA_RAM_TOT_BYTE_SIZE)));
740 
741  // Verify that the operation is complete.
742  if (HWREG(PKA_BASE + PKA_O_FUNCTION) & PKA_FUNCTION_RUN) {
744  }
745 
746  // Get the MSW register value.
747  regMSWVal = HWREG(PKA_BASE + PKA_O_DIVMSW);
748 
749  // If the result vector is zero, write back one zero byte so the caller does not need
750  // to handle a special error for the perhaps valid result of zero.
751  // They will only get the error status if they do not provide a buffer
752  if (regMSWVal & PKA_DIVMSW_RESULT_IS_ZERO_M) {
753  if (resultLength && resultBuf && *resultLength){
754 
755  resultBuf[0] = 0;
756  *resultLength = 1;
757 
758  return PKA_STATUS_SUCCESS;
759  }
760  else {
762  }
763  }
764 
765  // Get the length of the result
766  lengthInWords = ((regMSWVal & PKA_DIVMSW_MSW_ADDRESS_M) + 1) - ((resultPKAMemAddr - PKA_RAM_BASE) >> 2);
767 
768  // Check if the provided buffer length is adequate to store the result data.
769  if (resultLength && (*resultLength < lengthInWords * sizeof(uint32_t))) {
771  }
772 
773  // Copy the resultant length.
774  *resultLength = lengthInWords * sizeof(uint32_t);
775 
776 
777  if (resultBuf) {
778  // Copy the result into the resultBuf.
779  for (i = 0; i < lengthInWords; i++) {
780  resultWordAlias[i] = HWREG(resultPKAMemAddr + sizeof(uint32_t) * i);
781  }
782  }
783 
784  return PKA_STATUS_SUCCESS;
785 }
#define PKA_STATUS_BUF_UNDERFLOW
Buffer underflow.
Definition: pka.h:123
#define PKA_STATUS_OPERATION_BUSY
PKA operation is in progress.
Definition: pka.h:128
#define PKA_STATUS_SUCCESS
Success.
Definition: pka.h:120
#define ASSERT(expr)
Definition: debug.h:73
static uint32_t PKAGetECCResult ( uint8_t *  curvePointX,
uint8_t *  curvePointY,
uint32_t  resultPKAMemAddr,
uint32_t  length 
)
static

Referenced by PKAEccAddGetResult(), and PKAEccMultiplyGetResult().

793 {
794  uint32_t i = 0;
795  uint32_t *xWordAlias = (uint32_t *)curvePointX;
796  uint32_t *yWordAlias = (uint32_t *)curvePointY;
797  uint32_t lengthInWordsCeiling = 0;
798 
799  // Check for the arguments.
800  ASSERT(curvePoint);
801  ASSERT(curvePointX);
802  ASSERT(curvePointY);
803  ASSERT((resultPKAMemAddr > PKA_RAM_BASE) &&
804  (resultPKAMemAddr < (PKA_RAM_BASE + PKA_RAM_TOT_BYTE_SIZE)));
805 
806  // Verify that the operation is completed.
807  if (HWREG(PKA_BASE + PKA_O_FUNCTION) & PKA_FUNCTION_RUN) {
809  }
810 
811  if (HWREG(PKA_BASE + PKA_O_SHIFT)) {
812  return PKA_STATUS_FAILURE;
813  }
814 
815  // Check to make sure that the result vector is not the point at infinity.
816  if (HWREG(PKA_BASE + PKA_O_MSW) & PKA_MSW_RESULT_IS_ZERO) {
818  }
819 
820  if (curvePointX != NULL) {
821  // Copy the x co-ordinate value of the result from vector D into
822  // the curvePoint.
823  for (i = 0; i < (length / sizeof(uint32_t)); i++) {
824  xWordAlias[i] = HWREG(resultPKAMemAddr + sizeof(uint32_t) * i);
825  }
826 
827  // If the length is not a word-multiple, fill up a temporary word and copy that in
828  // to avoid a bus error.
829  if (length % sizeof(uint32_t)) {
830  uint32_t temp = 0;
831  uint8_t j;
832 
833  // Load the entire word line of the coordinate remainder
834  temp = HWREG(resultPKAMemAddr + sizeof(uint32_t) * i);
835 
836  // Write all remaining bytes to the coordinate
837  for (j = 0; j < length % sizeof(uint32_t); j++) {
838  curvePointX[i * sizeof(uint32_t) + j] = ((uint8_t *)&temp)[j];
839  }
840 
841  }
842  }
843 
844  lengthInWordsCeiling = (length % sizeof(uint32_t)) ? length / sizeof(uint32_t) + 1 : length / sizeof(uint32_t);
845 
846  resultPKAMemAddr += sizeof(uint32_t) * (2 + lengthInWordsCeiling + (lengthInWordsCeiling % 2));
847 
848  if (curvePointY != NULL) {
849  // Copy the y co-ordinate value of the result from vector D into
850  // the curvePoint.
851  for (i = 0; i < (length / sizeof(uint32_t)); i++) {
852  yWordAlias[i] = HWREG(resultPKAMemAddr + sizeof(uint32_t) * i);
853  }
854 
855  // If the length is not a word-multiple, fill up a temporary word and copy that in
856  // to avoid a bus error.
857  if (length % sizeof(uint32_t)) {
858  uint32_t temp = 0;
859  uint8_t j;
860 
861  // Load the entire word line of the coordinate remainder
862  temp = HWREG(resultPKAMemAddr + sizeof(uint32_t) * i);
863 
864  // Write all remaining bytes to the coordinate
865  for (j = 0; j < length % sizeof(uint32_t); j++) {
866  curvePointY[i * sizeof(uint32_t) + j] = ((uint8_t *)&temp)[j];
867  }
868  }
869  }
870 
871 
872  return PKA_STATUS_SUCCESS;
873 }
#define PKA_STATUS_FAILURE
Failure.
Definition: pka.h:121
#define PKA_STATUS_OPERATION_BUSY
PKA operation is in progress.
Definition: pka.h:128
#define PKA_STATUS_SUCCESS
Success.
Definition: pka.h:120
#define ASSERT(expr)
Definition: debug.h:73
#define PKA_STATUS_POINT_AT_INFINITY
The ECC operation resulted in the point at infinity.
Definition: pka.h:137
static uint32_t PKAWritePkaParam ( const uint8_t *  param,
uint32_t  paramLength,
uint32_t  paramOffset,
uint32_t  ptrRegOffset 
)
static

Referenced by PKABigNumAddStart(), PKABigNumCmpStart(), PKABigNumDivideStart(), PKABigNumInvModStart(), PKABigNumModStart(), PKABigNumMultiplyStart(), PKABigNumSubStart(), PKAEccMontgomeryMultiplyStart(), PKAEccMultiplyStart(), and PKAWritePkaParamExtraOffset().

578 {
579  uint32_t i;
580  uint32_t *paramWordAlias = (uint32_t *)param;
581  // Take the floor of paramLength in 32-bit words
582  uint32_t paramLengthInWords = paramLength / sizeof(uint32_t);
583 
584  // Only copy data if it is specified. We may wish to simply allocate another buffer and get
585  // the required offset.
586  if (param) {
587  // Load the number in PKA RAM
588  for (i = 0; i < paramLengthInWords; i++) {
589  HWREG(PKA_RAM_BASE + paramOffset + sizeof(uint32_t) * i) = paramWordAlias[i];
590  }
591 
592  // If the length is not a word-multiple, fill up a temporary word and copy that in
593  // to avoid a bus error. The extra zeros at the end should not matter, as the large
594  // number is little-endian and thus has no effect.
595  // We could have correctly calculated ceiling(paramLength / sizeof(uint32_t)) above.
596  // However, we would not have been able to zero-out the extra few most significant
597  // bytes of the most significant word. That would have resulted in doing maths operations
598  // on whatever follows param in RAM.
599  if (paramLength % sizeof(uint32_t)) {
600  uint32_t temp = 0;
601  uint8_t j;
602 
603  // Load the entire word line of the param remainder
604  temp = paramWordAlias[i];
605 
606  // Zero-out all bytes beyond the end of the param
607  for (j = paramLength % sizeof(uint32_t); j < sizeof(uint32_t); j++) {
608  ((uint8_t *)&temp)[j] = 0;
609  }
610 
611  HWREG(PKA_RAM_BASE + paramOffset + sizeof(uint32_t) * i) = temp;
612 
613  // Increment paramLengthInWords since we take the ceiling of length / sizeof(uint32_t)
614  paramLengthInWords++;
615  }
616  }
617 
618  // Update the A, B, C, or D pointer with the offset address of the PKA RAM location
619  // where the number will be stored.
620  switch (ptrRegOffset) {
621  case PKA_O_APTR:
622  HWREG(PKA_BASE + PKA_O_APTR) = paramOffset >> 2;
623  HWREG(PKA_BASE + PKA_O_ALENGTH) = paramLengthInWords;
624  break;
625  case PKA_O_BPTR:
626  HWREG(PKA_BASE + PKA_O_BPTR) = paramOffset >> 2;
627  HWREG(PKA_BASE + PKA_O_BLENGTH) = paramLengthInWords;
628  break;
629  case PKA_O_CPTR:
630  HWREG(PKA_BASE + PKA_O_CPTR) = paramOffset >> 2;
631  break;
632  case PKA_O_DPTR:
633  HWREG(PKA_BASE + PKA_O_DPTR) = paramOffset >> 2;
634  break;
635  }
636 
637  // Ensure 8-byte alignment of next parameter.
638  // Returns the offset for the next parameter.
639  return paramOffset + sizeof(uint32_t) * (paramLengthInWords + (paramLengthInWords % 2));
640 }
static uint32_t PKAWritePkaParamExtraOffset ( const uint8_t *  param,
uint32_t  paramLength,
uint32_t  paramOffset,
uint32_t  ptrRegOffset 
)
static

Referenced by PKABigNumDivideStart(), PKABigNumModStart(), PKAEccAddStart(), PKAEccMontgomeryMultiplyStart(), and PKAEccMultiplyStart().

648 {
649  // Ensure 16-byte alignment.
650  return (sizeof(uint32_t) * 2) + PKAWritePkaParam(param, paramLength, paramOffset, ptrRegOffset);
651 }
static uint32_t PKAWritePkaParam(const uint8_t *param, uint32_t paramLength, uint32_t paramOffset, uint32_t ptrRegOffset)
Definition: pka.c:577

Here is the call graph for this function: