File List
Here is a list of all files with brief descriptions:
 ADC.hAnalog to Digital Conversion (ADC) Input Driver
 ADCBuf.hAnalog to Digital Conversion Buffer (ADCBuf) Input Driver
 ADCBufCC26X2.hADCBuf driver implementation for a CC26X2 analog-to-digital converter
 ADCBufCC26XX.hADCBuf driver implementation for a CC26XX analog-to-digital converter
 ADCCC26XX.hADC driver implementation for the ADC peripheral on CC26XX
 AESCBC.hAESCBC driver header
 AESCBCCC26XX.hAESCBC driver implementation for the CC26XX family
 AESCCM.hAESCCM driver header
 AESCCMCC26XX.hAESCCM driver implementation for the CC26XX family
 AESCTR.hAESCTR driver header
 AESCTRCC26XX.hAESCTR driver implementation for the CC26XX family
 AESCTRDRBG.hAESCTRDRBG driver header
 AESCTRDRBGXX.hGeneric AESCTRDRBG implementation based on the AESCTR driver
 AESECB.hAESECB driver header
 AESECBCC26XX.hAESECB driver implementation for the CC26XX family
 AESGCM.hAESGCM driver header
 AESGCMCC26XX.hAESGCM driver implementation for the CC26XX family
 AnsiColor.h
 Board.hPortable board-specific symbols
 Codec1.hImplementation of TI Codec Type 1 (IMA ADPCM) encoding and decoding
 CryptoCC26XX.hCrypto driver implementation for a CC26XX Crypto controller
 CryptoKey.hThe CryptoKey type is an opaque representation of a cryptographic key
 CryptoKeyPlaintext.h
 CryptoResourceCC26XX.hShared resources to arbitrate access to the keyStore, AES, and SHA2 engine
 Display.hGeneric interface for text output
 DisplayDogm1286.h
 DisplayExt.hExtention of Display to access GrLib functionality in capable displays
 DisplayHost.hDisplay driver for printf-like output
 DisplaySharp.h
 DisplayUart.hDisplay.h implementation for UART output
 ECCParams.h
 ECDH.hTI Driver for Elliptic Curve Diffie-Hellman key agreement scheme
 ECDHCC26X2.hECDH driver implementation for the CC26X2 family
 ECDSA.hTI Driver for Elliptic Curve Digital Signature Algorithm
 ECDSACC26X2.hECDSA driver implementation for the CC26X2 family
 ECJPAKE.hTI Driver for Elliptic Curve Password Authenticated Key Exchange by Juggling
 ECJPAKECC26X2.hECJPAKE driver implementation for the CC26X2 family
 GPIO.hGeneral Purpose I/O driver interface
 GPIOCC26XX.hGPIO driver implementation for CC26xx/CC13xx devices
 GPTimerCC26XX.hGPTimer driver implementation for CC26XX/CC13XX
 I2C.hInter-Integrated Circuit (I2C) Driver
 I2CCC26XX.hI2C driver implementation for a CC26XX I2C controller
 I2S.hInter-Integrated Circuit Sound (I2S) Bus Driver
 I2SCC26XX.hI2S driver implementation for a CC26XX I2S controller
 LCDDogm1286.hLCD driver implementation for a DOGM128W-6 LCD display
 LCDDogm1286_util.h
 List.hLinked List interface for use in drivers
 NoRTOS.hNoRTOS framework module
 NVS.hNon-Volatile Storage driver interface
 NVSCC26XX.hNon-Volatile Storage driver for CC13XX/CC26XX devices
 NVSRAM.hRAM implementation of the NVS driver
 NVSSPI25X.hNon-Volatile Storage driver implementation for SPI flash peripherals
 PDMCC26XX.hPDM driver implementation for a CC26XX PDM controller
 PDMCC26XX_util.hPDM utility includes helper functions for configuring the CC26XX I2S controller
 PIN.hGeneric PIN & GPIO driver
 PINCC26XX.hDevice-specific pin & GPIO driver for CC26xx family [def]
 PKAResourceCC26XX.hShared resources to arbitrate access to the PKA engine
 Power.hPower Manager
 PowerCC26X2.hPower manager interface for CC26X2
 PowerCC26XX.hPower manager interface for CC26XX/CC13XX
 PWM.hPulse Width Modulation (PWM) driver
 PWMTimerCC26XX.hPWM driver implementation for CC26XX/CC13XX
 Random.hInterface to generate pseudo-random numbers
 RF.hRadio Frequency (RF) Core Driver for the CC13XX and CC26XX device family
 RingBuf.h
 SD.hSecure Digital (SD) Driver
 SDFatFS.hFile Allocation Table File System (FATFS) Driver
 SDSPI.hSD driver implementation built on the TI SPI driver
 SHA2.hSHA2 driver header
 SHA2CC26X2.hSHA2 driver implementation for the CC26X2 family
 SharpGrLib.h
 SPI.hSerial Peripheral Interface (SPI) Driver Interface
 SPICC26X2DMA.hSPI driver implementation for a CC26XX SPI controller using the UDMA controller
 SPICC26XXDMA.hSPI driver implementation for a CC26XX SPI controller using the UDMA controller
 spiffs.h
 SPIFFSNVS.hModule to enable the SPI Flash File System (SPIFFS) on the TI NVS driver
 TRNG.hTRNG driver header
 TRNGCC26XX.hTRNG driver implementation for the CC26XX family
 types.h
 UART.hUniversal Asynchronous Receiver-Transmitter (UART) Driver
 UARTCC26X0.hUART driver implementation for a CC26X0 UART controller
 UARTCC26X2.hUART driver implementation for a CC26X2 UART controller
 UARTCC26XX.hUART driver implementation for a CC26XX UART controller
 UDMACC26XX.hUDMACC26XX driver implementation
 unistd.h
 Watchdog.hWatchdog driver interface
 WatchdogCC26XX.hWatchdog driver implementation for CC13XX/CC26XX
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale