341 #ifndef ti_drivers_uart_UARTCC26X2__include 342 #define ti_drivers_uart_UARTCC26X2__include 351 #include <ti/drivers/dpl/ClockP.h> 352 #include <ti/drivers/dpl/HwiP.h> 353 #include <ti/drivers/dpl/SemaphoreP.h> 354 #include <ti/drivers/dpl/SwiP.h> 365 #define UARTCC26X2_FLOWCTRL_NONE 0 370 #define UARTCC26X2_FLOWCTRL_HARDWARE 1 403 #define UARTCC26X2_CMD_RETURN_PARTIAL_ENABLE (UART_CMD_RESERVED + 0) 412 #define UARTCC26X2_CMD_RETURN_PARTIAL_DISABLE (UART_CMD_RESERVED + 1) 420 #define UARTCC26X2_CMD_RX_FIFO_FLUSH (UART_CMD_RESERVED + 2) 426 #define UARTCC26X2_FIFO_SIZE 32 601 bool ctrlRxEnabled:1;
size_t readSize
Definition: UARTCC26X2.h:621
UARTCC26X2 Object.
Definition: UARTCC26X2.h:575
enum UART_Echo_ UART_Echo
UART echo settings.
Definition: UARTCC26X2.h:442
UARTCC26X2_FifoThreshold rxIntFifoThr
Definition: UARTCC26X2.h:565
UARTCC26X2_ErrorCallback errorFxn
Definition: UARTCC26X2.h:567
size_t readCount
Definition: UARTCC26X2.h:622
enum UART_PAR_ UART_PAR
UART parity type settings.
Definition: UARTCC26X2.h:441
size_t ringBufSize
Definition: UARTCC26X2.h:553
struct UARTCC26X2_Object * UARTCC26X2_Handle
enum UART_LEN_ UART_LEN
UART data length settings.
uint8_t rxPin
Definition: UARTCC26X2.h:555
enum UART_Mode_ UART_Mode
UART mode settings.
unsigned int powerMgrId
Definition: UARTCC26X2.h:642
HwiP_Struct hwi
Definition: UARTCC26X2.h:608
UARTCC26X2 Hardware attributes.
Definition: UARTCC26X2.h:535
UART_LEN dataLength
Definition: UARTCC26X2.h:613
unsigned char * ringBufPtr
Definition: UARTCC26X2.h:551
PIN_Handle hPin
Definition: UARTCC26X2.h:638
uint32_t status
Definition: UARTCC26X2.h:616
void(* UARTCC26X2_ErrorCallback)(UART_Handle handle, uint32_t error)
The definition of an optional callback function used by the UART driver to notify the application whe...
Definition: UARTCC26X2.h:458
UART Global configuration.
Definition: UART.h:678
uint8_t rtsPin
Definition: UARTCC26X2.h:561
SemaphoreP_Struct writeSem
Definition: UARTCC26X2.h:632
Definition: UARTCC26X2.h:440
size_t writeCount
Definition: UARTCC26X2.h:631
UART_STOP stopBits
Definition: UARTCC26X2.h:614
Device-specific pin & GPIO driver for CC26xx family [def].
unsigned int readTimeout
Definition: UARTCC26X2.h:624
RingBuf_Object ringBuffer
Definition: UARTCC26X2.h:619
UART_Callback writeCallback
Definition: UARTCC26X2.h:634
struct UARTCC26X2_HWAttrs UARTCC26X2_HWAttrs
UARTCC26X2 Hardware attributes.
uint8_t intPriority
Definition: UARTCC26X2.h:541
Definition: UARTCC26X2.h:444
UART_Callback readCallback
Definition: UARTCC26X2.h:625
struct UARTCC26X2_Object UARTCC26X2_Object
UARTCC26X2 Object.
ClockP_Struct timeoutClk
Definition: UARTCC26X2.h:611
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:635
Definition: UARTCC26X2.h:443
Definition: UARTCC26X2.h:445
Power notify object structure.
Definition: Power.h:443
const unsigned char * writeBuf
Definition: UARTCC26X2.h:629
Universal Asynchronous Receiver-Transmitter (UART) Driver.
uint32_t baseAddr
Definition: UARTCC26X2.h:537
int intNum
Definition: UARTCC26X2.h:539
uint32_t swiPriority
Swi priority. The higher the number, the higher the priority. The minimum priority is 0 and the maxim...
Definition: UARTCC26X2.h:547
underlying data structure for type PIN_State
Definition: PIN.h:707
UARTCC26X2_FifoThreshold
UART TX/RX interrupt FIFO threshold select.
Definition: UARTCC26X2.h:439
uint32_t flowControl
Definition: UARTCC26X2.h:549
enum UART_STOP_ UART_STOP
UART stop bit settings.
const UART_FxnTable UARTCC26X2_fxnTable
enum UART_ReturnMode_ UART_ReturnMode
UART return mode settings.
PIN_State pinState
Definition: UARTCC26X2.h:637
uint32_t baudRate
Definition: UARTCC26X2.h:612
SwiP_Struct writeSwi
Definition: UARTCC26X2.h:610
unsigned char * readBuf
Definition: UARTCC26X2.h:620
uint8_t txPin
Definition: UARTCC26X2.h:557
UARTCC26X2_FifoThreshold txIntFifoThr
Definition: UARTCC26X2.h:563
unsigned int writeTimeout
Definition: UARTCC26X2.h:633
size_t writeSize
Definition: UARTCC26X2.h:630
uint8_t ctsPin
Definition: UARTCC26X2.h:559
SemaphoreP_Struct readSem
Definition: UARTCC26X2.h:623
UART_PAR parityType
Definition: UARTCC26X2.h:615
bool readRetPartial
Definition: UARTCC26X2.h:626
void(* UART_Callback)(UART_Handle handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:421
enum UART_DataMode_ UART_DataMode
UART data mode settings.
Power_NotifyObj postNotify
Definition: UARTCC26X2.h:641
SwiP_Struct readSwi
Definition: UARTCC26X2.h:609