405 #ifndef ti_drivers_crypto_CryptoCC26XX__include 406 #define ti_drivers_crypto_CryptoCC26XX__include 417 #include <ti/devices/DeviceFamily.h> 418 #include DeviceFamily_constructPath(driverlib/crypto.h) 420 #if DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2 421 #warning "This driver is deprecated for the CC26x2 and CC13x2 families.\ 422 It is superceded by AESECB and AESCCM." 453 #define CRYPTOCC26XX_TIMEOUT 20 455 #define CRYPTOCC26XX_STATUS_SUCCESS 0 456 #define CRYPTOCC26XX_STATUS_ERROR -1 457 #define CRYPTOCC26XX_STATUS_UNDEFINEDCMD -2 459 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT 0 460 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY 1 461 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT 2 462 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY 3 463 #define CRYPTOCC26XX_OP_AES_ECB_ENCRYPT 4 464 #define CRYPTOCC26XX_OP_AES_ECB_DECRYPT 5 465 #define CRYPTOCC26XX_OP_AES_CBC_ENCRYPT 6 466 #define CRYPTOCC26XX_OP_AES_CBC_DECRYPT 7 469 #define CRYPTOCC26XX_OP_AES_CCM CRYPTOCC26XX_OP_AES_CCM_ENCRYPT 470 #define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY 471 #define CRYPTOCC26XX_OP_AES_CCMINV CRYPTOCC26XX_OP_AES_CCM_DECRYPT 472 #define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY 473 #define CRYPTOCC26XX_OP_AES_ECB CRYPTOCC26XX_OP_AES_ECB_ENCRYPT 474 #define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT CRYPTOCC26XX_OP_AES_ECB_DECRYPT 477 #include <ti/drivers/dpl/HwiP.h> 478 #include <ti/drivers/dpl/SemaphoreP.h> int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, const uint32_t *keySrc)
Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key...
CryptoCC26XX Transaction.
Definition: CryptoCC26XX.h:564
CryptoCC26XX Global Configuration.
Definition: CryptoCC26XX.h:769
CryptoCC26XX_Transaction * currentTransact
Definition: CryptoCC26XX.h:763
void CryptoCC26XX_Params_init(CryptoCC26XX_Params *params)
Function to initialize the CryptoCC26XX_Params struct to its defaults.
CryptoCC26XX AES-CCM Transaction.
Definition: CryptoCC26XX.h:620
struct CryptoCC26XX_Object CryptoCC26XX_Object
CryptoCC26XX Object.
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:695
int CryptoCC26XX_close(CryptoCC26XX_Handle handle)
Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle.
void * msgOut
Definition: CryptoCC26XX.h:650
struct CryptoCC26XX_AESCCM_Transaction CryptoCC26XX_AESCCM_Transaction
CryptoCC26XX AES-CCM Transaction.
CryptoCC26XX Parameters.
Definition: CryptoCC26XX.h:544
uint8_t keyIndex
Definition: CryptoCC26XX.h:697
void * msgIn
Definition: CryptoCC26XX.h:683
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:621
Definition: CryptoCC26XX.h:529
HwiP_Struct hwi
Definition: CryptoCC26XX.h:765
uint8_t CryptoCC26XX_Operation
CryptoCC26XX Operation Type.
Definition: CryptoCC26XX.h:519
uint8_t fieldLength
Definition: CryptoCC26XX.h:656
Definition: CryptoCC26XX.h:532
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:565
Definition: CryptoCC26XX.h:496
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:679
int CryptoCC26XX_loadKey(CryptoCC26XX_Handle handle, int keyIndex, const uint32_t *keySrc)
Function that writes a given key into a key store.
void * msgOut
Definition: CryptoCC26XX.h:699
uint8_t keyIndex
Definition: CryptoCC26XX.h:623
char * nonce
Definition: CryptoCC26XX.h:626
void * msgOut
Definition: CryptoCC26XX.h:684
struct CryptoCC26XX_Config CryptoCC26XX_Config
CryptoCC26XX Global Configuration.
void CryptoCC26XX_Transac_init(CryptoCC26XX_Transaction *trans, CryptoCC26XX_Operation opType)
Function to initialize the CryptoCC26XX_Transaction struct to its defaults.
int CryptoCC26XX_releaseKey(CryptoCC26XX_Handle handle, int *keyIndex)
Function that releases the specified CryptoCC26XX Key.
char * header
Definition: CryptoCC26XX.h:649
CryptoCC26XX Hardware Attributes.
Definition: CryptoCC26XX.h:731
int openCnt
Definition: CryptoCC26XX.h:760
void const * hwAttrs
Definition: CryptoCC26XX.h:774
uint16_t headerLength
Definition: CryptoCC26XX.h:669
Definition: CryptoCC26XX.h:502
uint16_t msgInLength
Definition: CryptoCC26XX.h:667
struct CryptoCC26XX_Params CryptoCC26XX_Params
CryptoCC26XX Parameters.
struct CryptoCC26XX_Config * CryptoCC26XX_Handle
A handle that is returned from a CryptoCC26XX_open() call.
Definition: CryptoCC26XX.h:483
void * msgIn
Definition: CryptoCC26XX.h:698
uint32_t timeout
Definition: CryptoCC26XX.h:761
Definition: CryptoCC26XX.h:534
CryptoCC26XX_Mode
CryptoCC26XX Mode Settings.
Definition: CryptoCC26XX.h:491
CryptoCC26XX AES-ECB Transaction.
Definition: CryptoCC26XX.h:694
char * msgIn
Definition: CryptoCC26XX.h:643
void CryptoCC26XX_init(void)
Function to initialize CryptoCC26XX driver. Users of this module must call init(). Multiple users/libraries may call init(), though subsequent calls may be benign.
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: CryptoCC26XX.h:750
int CryptoCC26XX_transact(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto operation (encryption or decryption) in blocking mode.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:680
CryptoCC26XX_KeyStore keyStore
Definition: CryptoCC26XX.h:762
uint8_t keyIndex
Definition: CryptoCC26XX.h:681
uint16_t msgInLength
Definition: CryptoCC26XX.h:685
int powerMngrId
Definition: CryptoCC26XX.h:735
void * object
Definition: CryptoCC26XX.h:771
Definition: CryptoCC26XX.h:535
Definition: CryptoCC26XX.h:531
uint8_t CryptoCC26XX_KeyStore
CryptoCC26XX Key.
Definition: CryptoCC26XX.h:553
CryptoCC26XX_Handle CryptoCC26XX_open(unsigned int index, bool exclusiveAccess, CryptoCC26XX_Params *params)
Function to initialize a given CryptoCC26XX peripheral specified by the particular index value...
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:696
void * nonce
Definition: CryptoCC26XX.h:682
CryptoCC26XX_KeyLocation
CryptoCC26XX Key Store Location.
Definition: CryptoCC26XX.h:527
int intNum
Definition: CryptoCC26XX.h:737
struct CryptoCC26XX_HWAttrs CryptoCC26XX_HWAttrs
CryptoCC26XX Hardware Attributes.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:566
Definition: CryptoCC26XX.h:533
struct CryptoCC26XX_Transaction CryptoCC26XX_Transaction
CryptoCC26XX Transaction.
uint32_t timeout
Definition: CryptoCC26XX.h:545
CryptoCC26XX Object.
Definition: CryptoCC26XX.h:758
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:622
uint32_t baseAddr
Definition: CryptoCC26XX.h:733
struct CryptoCC26XX_AESECB_Transaction CryptoCC26XX_AESECB_Transaction
CryptoCC26XX AES-ECB Transaction.
struct CryptoCC26XX_AESCBC_Transaction CryptoCC26XX_AESCBC_Transaction
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:530
int CryptoCC26XX_transactPolling(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in polling mode...
int CryptoCC26XX_transactCallback(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in callback mode...
uint8_t authLength
Definition: CryptoCC26XX.h:624
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:678
Definition: CryptoCC26XX.h:528