TI BLE-Stack for Bluetooth API Documentation
3.03.04.00
|
GAP Advertisement/Scan Response Data Token. More...
Data Fields | |
uint8 | adType |
ADTYPE value: Address Types. | |
uint8 | attrLen |
Number of bytes in the attribute data. | |
uint8 * | pAttrData |
pointer to Attribute data | |
GAP Advertisement/Scan Response Data Token.
These data items are stored as low byte first (OTA format). The data space for these items are passed in and maintained by the calling application