![]() |
![]() |
|
TI BLE-Stack for Bluetooth API Documentation
3.03.04.00
|
This module implements the Generic Access Protocol (GAP) For a detailed usage section describing how to send these commands and receive events, see the GAP Section of the User's Guide. More...
Modules | |
| GAP Callbacks | |
| GAP Constants | |
| GAP Structures | |
Files | |
| file | gap.h |
| GAP layer interface. | |
Functions | |
| bStatus_t | GAP_Authenticate (gapAuthParams_t *pParams, gapPairingReq_t *pPairReq) |
| Start Authentication. More... | |
| bStatus_t | GAP_Bond (uint16 connectionHandle, uint8 authenticated, uint8 secureConnections, smSecurityInfo_t *pParams, uint8 startEncryption) |
| Set up the connection's bound paramaters. More... | |
| bStatus_t | GAP_ConfigDeviceAddr (uint8 addrMode, uint8 *pStaticAddr) |
| Configure Device Address. More... | |
| bStatus_t | GAP_DeviceDiscoveryCancel (uint8 taskID) |
| Cancel an existing device discovery request. More... | |
| bStatus_t | GAP_DeviceDiscoveryRequest (gapDevDiscReq_t *pParams) |
| Start a device discovery scan. More... | |
| bStatus_t | GAP_DeviceInit (uint8 taskID, uint8 profileRole, uint8 maxScanResponses, uint8 *pIRK, uint8 *pSRK, uint32 *pSignCounter) |
| GAP Device Initialiation. More... | |
| bStatus_t | GAP_EndDiscoverable (uint8 taskID) |
| Stops advertising. More... | |
| bStatus_t | GAP_EstablishLinkReq (gapEstLinkReq_t *pParams) |
| Establish a link to a slave device. More... | |
| gapAdvDataToken_t * | GAP_GetAdvToken (uint8 adType) |
| Get Advertising Token. More... | |
| uint16 | GAP_GetParamValue (gapParamIDs_t paramID) |
| Get a GAP Parameter value. More... | |
| uint8 | GAP_isPairing (void) |
| Check if GAP is currently pairing. More... | |
| bStatus_t | GAP_MakeDiscoverable (uint8 taskID, gapAdvertisingParams_t *pParams) |
| Setup or change advertising. Also starts advertising. More... | |
| uint8 | GAP_NumActiveConnections (void) |
| Returns the number of active connections. More... | |
| bStatus_t | GAP_PasscodeUpdate (uint32 passcode, uint16 connectionHandle) |
| Update the passkey in a numeric value (not string). More... | |
| bStatus_t | GAP_PasskeyUpdate (uint8 *pPasskey, uint16 connectionHandle) |
| Update the passkey in string format. More... | |
| void | GAP_RegisterBondMgrCBs (gapBondMgrCBs_t *pCBs) |
| Register bond manager call backs. More... | |
| bStatus_t | GAP_RegisterConnEventCb (pfnGapConnEvtCB_t cb, GAP_CB_Action_t action, uint16_t connHandle) |
| void | GAP_RegisterForMsgs (uint8 taskID) |
| Register for GAP Messages. More... | |
| gapAdvDataToken_t * | GAP_RemoveAdvToken (uint8 adType) |
| Remove Advertising Token. More... | |
| bStatus_t | GAP_ResolvePrivateAddr (uint8 *pIRK, uint8 *pAddr) |
| Resolves a private address against an IRK. More... | |
| bStatus_t | GAP_SendSlaveSecurityRequest (uint16 connectionHandle, uint8 authReq) |
| Generate a Slave Requested Security message to the master. More... | |
| bStatus_t | GAP_SetAdvToken (gapAdvDataToken_t *pToken) |
| Set Advertising Token. More... | |
| bStatus_t | GAP_SetParamValue (gapParamIDs_t paramID, uint16 paramValue) |
| Set a GAP Parameter value. More... | |
| bStatus_t | GAP_Signable (uint16 connectionHandle, uint8 authenticated, smSigningInfo_t *pParams) |
| Set up the connection to accept signed data. More... | |
| bStatus_t | GAP_TerminateAuth (uint16 connectionHandle, uint8 reason) |
| Terminate Authnetication. More... | |
| bStatus_t | GAP_TerminateLinkReq (uint8 taskID, uint16 connectionHandle, uint8 reason) |
| Terminate a link connection. More... | |
| bStatus_t | GAP_UpdateAdvertisingData (uint8 taskID, uint8 adType, uint8 dataLen, uint8 *pAdvertData) |
| Setup or change advertising and scan response data. More... | |
| bStatus_t | GAP_UpdateAdvTokens (void) |
| Update Advertising Token. More... | |
| bStatus_t | GAP_UpdateLinkParamReq (gapUpdateLinkParamReq_t *pParams) |
| Update the link parameters to a Master or Slave device. More... | |
| bStatus_t | GAP_UpdateLinkParamReqReply (gapUpdateLinkParamReqReply_t *pParams) |
| Reply to a Connection Parameter Update Request sent from a peer device. More... | |
| void | GAP_UpdateResolvingList (uint8 *pIRK) |
| Update the resolving list. More... | |
This module implements the Generic Access Protocol (GAP) For a detailed usage section describing how to send these commands and receive events, see the GAP Section of the User's Guide.
| bStatus_t GAP_Authenticate | ( | gapAuthParams_t * | pParams, |
| gapPairingReq_t * | pPairReq | ||
| ) |
Start Authentication.
Start the Authentication process with the requested device. This function is used to Initiate/Allow pairing. Called by both master and slave device (Central and Peripheral).
| pParams | - Authentication parameters |
| pPairReq | - Enter these parameters if the Pairing Request was already received. NULL, if waiting for Pairing Request or if initiating. |
| bStatus_t GAP_Bond | ( | uint16 | connectionHandle, |
| uint8 | authenticated, | ||
| uint8 | secureConnections, | ||
| smSecurityInfo_t * | pParams, | ||
| uint8 | startEncryption | ||
| ) |
Set up the connection's bound paramaters.
| connectionHandle | - connection handle of the signing information |
| authenticated | - TRUE if bond is authenticated. |
| secureConnections | - TRUE if bond has Secure Connections strength. |
| pParams | - the connected device's security parameters |
| startEncryption | - whether or not to start encryption |
| bStatus_t GAP_ConfigDeviceAddr | ( | uint8 | addrMode, |
| uint8 * | pStaticAddr | ||
| ) |
Configure Device Address.
Setup the device's address type. If ADDRMODE_PRIVATE_RESOLVE is selected, the address will change periodically.
| addrMode | - GAP Addressing Modes |
| pStaticAddr | - Only used with ADDRMODE_STATIC or ADDRMODE_PRIVATE_NONRESOLVE type. NULL to auto generate otherwise the application can specify the address value |
| bStatus_t GAP_DeviceDiscoveryCancel | ( | uint8 | taskID | ) |
Cancel an existing device discovery request.
| taskID | - task to receive event |
| bStatus_t GAP_DeviceDiscoveryRequest | ( | gapDevDiscReq_t * | pParams | ) |
Start a device discovery scan.
| pParams | - Device Discovery parameters |
| bStatus_t GAP_DeviceInit | ( | uint8 | taskID, |
| uint8 | profileRole, | ||
| uint8 | maxScanResponses, | ||
| uint8 * | pIRK, | ||
| uint8 * | pSRK, | ||
| uint32 * | pSignCounter | ||
| ) |
GAP Device Initialiation.
Setup the device. Call just once on initialization.
| taskID | - task to receive event |
| profileRole | - GAP Profile Roles: GAP Profile Roles |
| maxScanResponses | - maximum number to scan responses we can receive during a device discovery. If 0,
|
| pIRK | - pointer to Identity Root Key, NULLKEY (all zeroes) if the app wants the GAP to generate the key. |
| pSRK | - pointer to Sign Resolving Key, NULLKEY if the app wants the GAP to generate the key. |
| pSignCounter | - 32 bit value used in the SM Signing algorithm that shall be initialized to zero and incremented with every new signing. This variable must also be maintained by the application. |
| bStatus_t GAP_EndDiscoverable | ( | uint8 | taskID | ) |
Stops advertising.
| taskID | - task to receive event |
| bStatus_t GAP_EstablishLinkReq | ( | gapEstLinkReq_t * | pParams | ) |
Establish a link to a slave device.
| pParams | - link establishment parameters |
| gapAdvDataToken_t* GAP_GetAdvToken | ( | uint8 | adType | ) |
Get Advertising Token.
Called to read a GAP Advertisement/Scan Response data token.
| adType | - Advertisement type to get |
| uint16 GAP_GetParamValue | ( | gapParamIDs_t | paramID | ) |
Get a GAP Parameter value.
| paramID | - parameter ID: GAP Parameter IDs |
| uint8 GAP_isPairing | ( | void | ) |
Check if GAP is currently pairing.
| bStatus_t GAP_MakeDiscoverable | ( | uint8 | taskID, |
| gapAdvertisingParams_t * | pParams | ||
| ) |
Setup or change advertising. Also starts advertising.
| taskID | - task to receive event |
| pParams | - advertising parameters |
| uint8 GAP_NumActiveConnections | ( | void | ) |
Returns the number of active connections.
| bStatus_t GAP_PasscodeUpdate | ( | uint32 | passcode, |
| uint16 | connectionHandle | ||
| ) |
Update the passkey in a numeric value (not string).
| passcode | - not string - range: 0 - 999,999. |
| connectionHandle | - connection handle. |
| bStatus_t GAP_PasskeyUpdate | ( | uint8 * | pPasskey, |
| uint16 | connectionHandle | ||
| ) |
Update the passkey in string format.
| pPasskey | - new passkey - pointer to numeric string (ie. "019655" ) This string's range is "000000" to "999999" |
| connectionHandle | - connection handle. |
| void GAP_RegisterBondMgrCBs | ( | gapBondMgrCBs_t * | pCBs | ) |
Register bond manager call backs.
| pCBs | - pointer to Bond Manager Callbacks. |
| bStatus_t GAP_RegisterConnEventCb | ( | pfnGapConnEvtCB_t | cb, |
| GAP_CB_Action_t | action, | ||
| uint16_t | connHandle | ||
| ) |
Register/Unregister a connection event callback
It is only possible to register for one connection handle of for all connection handles. In the case of unregistering, it does not matter what connHandle or cb is passed in as whatever is currently registered will be unregistered.
| cb | Function pointer to a callback. |
| action | Register or unregister the callback. |
| connHandle | if LINKDB_CONNHANDLE_ALL, apply to all connections. else, apply only for a specific connection. |
| void GAP_RegisterForMsgs | ( | uint8 | taskID | ) |
Register for GAP Messages.
Register a task ID to receive extra (unprocessed) HCI status and complete, and Host events.
| taskID | - Default task ID to send events. |
| gapAdvDataToken_t* GAP_RemoveAdvToken | ( | uint8 | adType | ) |
Remove Advertising Token.
Called to remove a GAP Advertisement/Scan Response data token.
| adType | - Advertisement type to remove |
| bStatus_t GAP_ResolvePrivateAddr | ( | uint8 * | pIRK, |
| uint8 * | pAddr | ||
| ) |
Resolves a private address against an IRK.
| pIRK | - pointer to the IRK |
| pAddr | - pointer to the Resolvable Private address |
| bStatus_t GAP_SendSlaveSecurityRequest | ( | uint16 | connectionHandle, |
| uint8 | authReq | ||
| ) |
Generate a Slave Requested Security message to the master.
This API can be used to initiate security as a slave.
| connectionHandle | - connection handle. |
| authReq | - Authentication Requirements: Bit 2: MITM, Bits 0-1: bonding (0 - no bonding, 1 - bonding) Bit 3: Secure Connections |
| bStatus_t GAP_SetAdvToken | ( | gapAdvDataToken_t * | pToken | ) |
Set Advertising Token.
Called to setup a GAP Advertisement / Scan Response data token.
| pToken | - Advertisement/Scan response token to write. |
| bStatus_t GAP_SetParamValue | ( | gapParamIDs_t | paramID, |
| uint16 | paramValue | ||
| ) |
Set a GAP Parameter value.
Use this function to change the default GAP parameter values.
| paramID | - parameter ID: GAP Parameter IDs |
| paramValue | - new param value |
| bStatus_t GAP_Signable | ( | uint16 | connectionHandle, |
| uint8 | authenticated, | ||
| smSigningInfo_t * | pParams | ||
| ) |
Set up the connection to accept signed data.
| connectionHandle | - connection handle of the signing information |
| authenticated | - TRUE if the signing information is authenticated, FALSE otherwise |
| pParams | - signing parameters |
| bStatus_t GAP_TerminateAuth | ( | uint16 | connectionHandle, |
| uint8 | reason | ||
| ) |
Terminate Authnetication.
Send a Pairing Failed message and end any existing pairing.
| connectionHandle | - connection handle. |
| reason | - Pairing Failed reason code. |
| bStatus_t GAP_TerminateLinkReq | ( | uint8 | taskID, |
| uint16 | connectionHandle, | ||
| uint8 | reason | ||
| ) |
Terminate a link connection.
| taskID | - requesting app's task id. |
| connectionHandle | - connection handle of link to terminate or GAP Special Connection Handles |
| reason | - terminate reason. |
| bStatus_t GAP_UpdateAdvertisingData | ( | uint8 | taskID, |
| uint8 | adType, | ||
| uint8 | dataLen, | ||
| uint8 * | pAdvertData | ||
| ) |
Setup or change advertising and scan response data.
| taskID | - task to receive event |
| adType | - TRUE - advertisement data, FALSE - scan response data |
| dataLen | - Octet length of advertData |
| pAdvertData | - advertising or scan response data |
| bStatus_t GAP_UpdateAdvTokens | ( | void | ) |
Update Advertising Token.
Called to rebuild and load Advertisement and Scan Response data from existing GAP Advertisement Tokens.
| bStatus_t GAP_UpdateLinkParamReq | ( | gapUpdateLinkParamReq_t * | pParams | ) |
Update the link parameters to a Master or Slave device.
| pParams | link update parameters |
| bStatus_t GAP_UpdateLinkParamReqReply | ( | gapUpdateLinkParamReqReply_t * | pParams | ) |
Reply to a Connection Parameter Update Request sent from a peer device.
The host should fill in the connection parameters it desires as well as whether or not this request was accepted. The controller will use the connection parameters passed into this command to respond over-the-air to the peer.
After the update procedure is complete, the calling task will receive a GAP_LINK_PARAM_UPDATE_EVENT of type gapLinkUpdateEvent_t
| pParams | - local device's desired connection parameters. |
| void GAP_UpdateResolvingList | ( | uint8 * | pIRK | ) |
Update the resolving list.
Based on whether the bond manager is included, this will call HCI_LE_SetAddressResolutionEnableCmd directly or go through the bond manager.
| pIRK | - pointer to Identity Root Key, NULLKEY (all zeroes) if the app wants the GAP to generate the key. |