#include <RFCC26X2.h>
§ startTime
uint32_t RF_ScheduleCmdParams::startTime |
Start time in RAT Ticks for the radio command.
§ startType
Start type for the start time.
§ allowDelay
uint32_t RF_ScheduleCmdParams::allowDelay |
Control word to define the policy of the scheduler if the timing of a command cannot be met. Only applicable on CC13x2 and CC26x2 devices. RF_AllowDelayNone: Reject the command. RF_AllowDelayAny: Append the command to the end of the queue.
§ endTime
uint32_t RF_ScheduleCmdParams::endTime |
End time in RAT Ticks for the radio command.
§ endType
End type for the end time.
§ duration
uint32_t RF_ScheduleCmdParams::duration |
Duration in RAT Ticks for the radio command.
§ activityInfo
uint32_t RF_ScheduleCmdParams::activityInfo |
Activity info provided by user.
§ coexPriority
Priority to use for coexistence request.
§ coexRequest
REQUEST line behavior to use for coexistence request.
The documentation for this struct was generated from the following file: