rflib
Modules | Data Structures | Typedefs | Enumerations | Functions
Rf_driver
Collaboration diagram for Rf_driver:

Modules

 Rf_driver_cc13x2_cc26x2
 

Data Structures

struct  RF_TxPowerTable_Value
 PA configuration value for a certain power level. More...
 
struct  RF_TxPowerTable_Entry
 TX power configuration entry in a TX power table. More...
 
struct  RF_Mode
 Specifies a RF core firmware configuration. More...
 
struct  RF_CoexOverride
 Runtime coexistence override parameters. More...
 
struct  RF_CoexOverride_BLEUseCases
 Coexistence override settings for BLE5 application scenarios. More...
 
union  RF_RadioSetup
 A unified type for radio setup commands of different PHYs. More...
 
union  RF_InfoVal
 Stores output parameters for RF_getInfo(). More...
 
struct  RF_ScheduleMapElement
 RF schedule map entry structure. More...
 
struct  RF_ScheduleMap
 RF schedule map structure. More...
 
struct  RF_Params
 RF driver configuration parameters. More...
 
struct  RF_Cmd_s
 
struct  RFCC26XX_HWAttrsV2
 RF Hardware attributes. More...
 
struct  RFCC26XX_SchedulerPolicy
 RF scheduler policy. More...
 
struct  RF_ScheduleCmdParams
 
struct  RF_AccessParams
 RF request access parameter struct. More...
 
struct  RF_RatConfigCapture
 RF_ratCapture parameter structure. More...
 
struct  RF_RatConfigCompare
 RF_ratCompare parameter structure. More...
 
struct  RF_RatConfigOutput
 RAT related IO parameter structure. More...
 
struct  RF_Object
 Stores the client's internal configuration and states. More...
 

Typedefs

typedef rfc_radioOp_t RF_Op
 Base type for all radio operation commands. More...
 
typedef uint64_t RF_EventMask
 Data type for events during command execution. More...
 
typedef uint32_t RF_ClientEventMask
 Event mask for combining RF_ClientEvent event flags in RF_Params::nClientEventMask. More...
 
typedef uint32_t RF_GlobalEventMask
 Event mask for combining RF_GlobalEvent event flags in RFCC26XX_HWAttrsV2::globalEventMask. More...
 
typedef int16_t RF_CmdHandle
 Command handle that is returned by RF_postCmd(). More...
 
typedef RF_ObjectRF_Handle
 A handle that is returned by to RF_open(). More...
 
typedef int8_t RF_RatHandle
 RAT handle that is returned by RF_ratCompare() or RF_ratCapture(). More...
 
typedef void(* RF_Callback) (RF_Handle h, RF_CmdHandle ch, RF_EventMask e)
 Handles events related to RF command execution. More...
 
typedef void(* RF_RatCallback) (RF_Handle h, RF_RatHandle rh, RF_EventMask e, uint32_t compareCaptureTime)
 Handles events related to the Radio Timer (RAT). More...
 
typedef void(* RF_ClientCallback) (RF_Handle h, RF_ClientEvent event, void *arg)
 Handles events related to a driver instance. More...
 
typedef void(* RF_GlobalCallback) (RF_Handle h, RF_GlobalEvent event, void *arg)
 Handles global events as part of PHY configuration. More...
 
typedef struct RF_Cmd_s RF_Cmd
 
typedef RF_ScheduleStatus(* RF_SubmitHook) (RF_Cmd *pCmdNew, RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue)
 Handles the queue sorting algorithm when a new command is submitted to the driver from any of the active clients. More...
 
typedef RF_ExecuteAction(* RF_ExecuteHook) (RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue, bool bConflict, RF_Cmd *conflictCmd)
 Defines the execution and conflict resolution hook at runtime. More...
 

Enumerations

enum  RF_TxPowerTable_PAType { RF_TxPowerTable_DefaultPA = 0, RF_TxPowerTable_HighPA = 1 }
 Selects a power amplifier path in a TX power value. More...
 
enum  RF_Priority { RF_PriorityHighest = 2, RF_PriorityHigh = 1, RF_PriorityNormal = 0 }
 Scheduling priority of RF operation commands. More...
 
enum  RF_PriorityCoex { RF_PriorityCoexDefault = 0, RF_PriorityCoexLow = 1, RF_PriorityCoexHigh = 2 }
 Priority level for coexistence priority signal. More...
 
enum  RF_RequestCoex { RF_RequestCoexDefault = 0, RF_RequestCoexAssertRx = 1, RF_RequestCoexNoAssertRx = 2 }
 Behavior for coexistence request signal. More...
 
enum  RF_Stat {
  RF_StatBusyError, RF_StatRadioInactiveError, RF_StatCmdDoneError, RF_StatInvalidParamsError,
  RF_StatCmdEnded, RF_StatError = 0x80, RF_StatCmdDoneSuccess, RF_StatCmdSch,
  RF_StatSuccess
}
 Status codes for various RF driver functions. More...
 
enum  RF_ClientEvent { RF_ClientEventPowerUpFinished = (1 << 0), RF_ClientEventRadioFree = (1 << 1), RF_ClientEventSwitchClientEntered = (1 << 2) }
 Client-related RF driver events. More...
 
enum  RF_GlobalEvent {
  RF_GlobalEventRadioSetup = (1 << 0), RF_GlobalEventRadioPowerDown = (1 << 1), RF_GlobalEventInit = (1 << 2), RF_GlobalEventCmdStart = (1 << 3),
  RF_GlobalEventCmdStop = (1 << 4), RF_GlobalEventCoexControl = (1 << 5), RF_GlobalEventTempNotifyFail = (1 << 6)
}
 Global RF driver events. More...
 
enum  RF_InfoType {
  RF_GET_CURR_CMD, RF_GET_AVAIL_RAT_CH, RF_GET_RADIO_STATE, RF_GET_SCHEDULE_MAP,
  RF_GET_CLIENT_LIST, RF_GET_CLIENT_SWITCHING_TIME
}
 Selects the entry of interest in RF_getInfo(). More...
 
enum  RF_StartType { RF_StartNotSpecified = 0, RF_StartAbs = 1 }
 Controls the behavior of the RF_scheduleCmd() API. More...
 
enum  RF_EndType { RF_EndNotSpecified = 0, RF_EndAbs = 1, RF_EndRel = 2, RF_EndInfinit = 3 }
 Controls the behavior of the RF_scheduleCmd() API. More...
 
enum  RF_ExecuteAction { RF_ExecuteActionNone = 0, RF_ExecuteActionRejectIncoming = 1, RF_ExecuteActionAbortOngoing = 2 }
 Controls the behavior of the state machine of the RF driver when a conflict is identified run-time between the commands waiting on the pend queue and the commands being actively executed by the radio. More...
 
enum  RF_ScheduleStatus {
  RF_ScheduleStatusError = -3, RF_ScheduleStatusNone = 0, RF_ScheduleStatusTop = 1, RF_ScheduleStatusMiddle = 2,
  RF_ScheduleStatusTail = 4, RF_ScheduleStatusPreempt = 8
}
 Describes the location within the pend queue where the new command was inserted by the scheduler. More...
 
enum  RF_AllowDelay { RF_AllowDelayNone = 0, RF_AllowDelayAny = UINT32_MAX }
 Controls the behavior of the RF_scheduleCmd() API. More...
 
enum  RF_RatSelectChannel { RF_RatChannelAny = -1, RF_RatChannel0 = 0, RF_RatChannel1 = 1, RF_RatChannel2 = 2 }
 Select the preferred RAT channel through the configuration of RF_ratCompare() or RF_ratCapture(). More...
 
enum  RF_RatCaptureSource { RF_RatCaptureSourceRtcUpdate = 20, RF_RatCaptureSourceEventGeneric = 21, RF_RatCaptureSourceRfcGpi0 = 22, RF_RatCaptureSourceRfcGpi1 = 23 }
 Selects the source signal for RF_ratCapture(). More...
 
enum  RF_RatCaptureMode { RF_RatCaptureModeRising = 0, RF_RatCaptureModeFalling = 1, RF_RatCaptureModeBoth = 2 }
 Selects the mode of RF_ratCapture(). More...
 
enum  RF_RatCaptureRepetition { RF_RatCaptureSingle = 0, RF_RatCaptureRepeat = 1 }
 Selects the repetition of RF_ratCapture(). More...
 
enum  RF_RatOutputMode {
  RF_RatOutputModePulse = 0, RF_RatOutputModeSet = 1, RF_RatOutputModeClear = 2, RF_RatOutputModeToggle = 3,
  RF_RatOutputModeAlwaysZero = 4, RF_RatOutputModeAlwaysOne = 5
}
 Selects the mode of the RAT_GPO[x] for RF_ratCompare() or RF_ratCapture(). More...
 
enum  RF_RatOutputSelect {
  RF_RatOutputSelectRatGpo1 = 1, RF_RatOutputSelectRatGpo2 = 2, RF_RatOutputSelectRatGpo3 = 3, RF_RatOutputSelectRatGpo4 = 4,
  RF_RatOutputSelectRatGpo5 = 5, RF_RatOutputSelectRatGpo6 = 6, RF_RatOutputSelectRatGpo7 = 7
}
 Selects GPO to be used with RF_ratCompare() or RF_ratCapture(). More...
 

Functions

RF_Handle RF_open (RF_Object *pObj, RF_Mode *pRfMode, RF_RadioSetup *pRadioSetup, RF_Params *params)
 Creates a a new client instance of the RF driver. More...
 
void RF_close (RF_Handle h)
 Close client connection to RF driver. More...
 
uint32_t RF_getCurrentTime (void)
 Return current radio timer value. More...
 
RF_CmdHandle RF_postCmd (RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent)
 Appends RF operation commands to the driver's command queue and returns a command handle. More...
 
RF_ScheduleStatus RF_defaultSubmitPolicy (RF_Cmd *pCmdNew, RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue)
 Sorts and adds commands to the RF driver internal command queue. More...
 
RF_ExecuteAction RF_defaultExecutionPolicy (RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue, bool bConflict, RF_Cmd *conflictCmd)
 Makes a final decision before dispatching a scheduled command. More...
 
void RF_ScheduleCmdParams_init (RF_ScheduleCmdParams *pSchParams)
 Initialize the configuration structure to default values to be used with the RF_scheduleCmd() API. More...
 
RF_CmdHandle RF_scheduleCmd (RF_Handle h, RF_Op *pOp, RF_ScheduleCmdParams *pSchParams, RF_Callback pCb, RF_EventMask bmEvent)
 Schedule an RF operation (chain) to the command queue. More...
 
RF_EventMask RF_pendCmd (RF_Handle h, RF_CmdHandle ch, RF_EventMask bmEvent)
 Synchronizes the calling task to an RF operation command ch and returns accumulated event flags. More...
 
RF_EventMask RF_runCmd (RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent)
 Runs synchronously an RF operation command or a chain of commands and returns the termination reason. More...
 
RF_EventMask RF_runScheduleCmd (RF_Handle h, RF_Op *pOp, RF_ScheduleCmdParams *pSchParams, RF_Callback pCb, RF_EventMask bmEvent)
 Runs synchronously a (chain of) RF operation(s) for dual or single-mode. More...
 
RF_Stat RF_cancelCmd (RF_Handle h, RF_CmdHandle ch, uint8_t mode)
 Abort/stop/cancel single command in command queue. More...
 
RF_Stat RF_flushCmd (RF_Handle h, RF_CmdHandle ch, uint8_t mode)
 Abort/stop/cancel command and any subsequent commands in command queue. More...
 
RF_Stat RF_runImmediateCmd (RF_Handle h, uint32_t *pCmdStruct)
 Send any Immediate command.
More...
 
RF_Stat RF_runDirectCmd (RF_Handle h, uint32_t cmd)
 Send any Direct command.
More...
 
void RF_yield (RF_Handle h)
 Signal that radio client is not going to issue more commands in a while.
More...
 
void RF_Params_init (RF_Params *params)
 Function to initialize the RF_Params struct to its defaults. More...
 
RF_Stat RF_getInfo (RF_Handle h, RF_InfoType type, RF_InfoVal *pValue)
 Get value for some RF driver parameters.
More...
 
int8_t RF_getRssi (RF_Handle h)
 Get RSSI value. More...
 
RF_OpRF_getCmdOp (RF_Handle h, RF_CmdHandle cmdHnd)
 Get command structure pointer. More...
 
void RF_RatConfigCompare_init (RF_RatConfigCompare *channelConfig)
 Initialize the configuration structure to be used to set up a RAT compare event. More...
 
void RF_RatConfigCapture_init (RF_RatConfigCapture *channelConfig)
 Initialize the configuration structure to be used to set up a RAT capture event. More...
 
void RF_RatConfigOutput_init (RF_RatConfigOutput *ioConfig)
 Initialize the configuration structure to be used to set up a RAT IO. More...
 
RF_RatHandle RF_ratCompare (RF_Handle rfHandle, RF_RatConfigCompare *channelConfig, RF_RatConfigOutput *ioConfig)
 Setup a Radio Timer (RAT) channel in compare mode. More...
 
RF_RatHandle RF_ratCapture (RF_Handle rfHandle, RF_RatConfigCapture *channelConfig, RF_RatConfigOutput *ioConfig)
 Setup a Radio Timer (RAT) channel in capture mode. More...
 
RF_Stat RF_ratDisableChannel (RF_Handle rfHandle, RF_RatHandle ratHandle)
 Disable a RAT channel. More...
 
RF_Stat RF_control (RF_Handle h, int8_t ctrl, void *args)
 Set RF control parameters. More...
 
RF_Stat RF_requestAccess (RF_Handle h, RF_AccessParams *pParams)
 Request radio access.
More...
 
RF_TxPowerTable_Value RF_getTxPower (RF_Handle h)
 Returns the currently configured transmit power configuration. More...
 
RF_Stat RF_setTxPower (RF_Handle h, RF_TxPowerTable_Value value)
 Updates the transmit power configuration of the RF core. More...
 
int8_t RF_TxPowerTable_findPowerLevel (RF_TxPowerTable_Entry table[], RF_TxPowerTable_Value value)
 Retrieves a power level in dBm for a given power configuration value. More...
 
RF_TxPowerTable_Value RF_TxPowerTable_findValue (RF_TxPowerTable_Entry table[], int8_t powerLevel)
 Retrieves a power configuration value for a given power level in dBm. More...
 
RF_Stat RF_enableHPOSCTemperatureCompensation (void)
 Enables temperature monitoring and temperature based drift compensation. More...
 

Detailed Description

Typedef Documentation

§ RF_Op

Base type for all radio operation commands.

All radio operation commands share a common part. That includes the command id, a status field, chaining properties and a start trigger. Whenever an RF operation command is used with the RF driver, it needs to be casted to an RF_Op.

More information about RF operation commands can be found in the Proprietary RF User's Guide.

See also
RF_runCmd(), RF_postCmd(), RF_pendCmd()

§ RF_EventMask

typedef uint64_t RF_EventMask

Data type for events during command execution.

Possible event flags are listed in RF_Core_Events and RF_Driver_Events.

§ RF_ClientEventMask

typedef uint32_t RF_ClientEventMask

Event mask for combining RF_ClientEvent event flags in RF_Params::nClientEventMask.

§ RF_GlobalEventMask

typedef uint32_t RF_GlobalEventMask

Event mask for combining RF_GlobalEvent event flags in RFCC26XX_HWAttrsV2::globalEventMask.

§ RF_CmdHandle

typedef int16_t RF_CmdHandle

Command handle that is returned by RF_postCmd().

A command handle is an integer number greater equals zero and identifies a command container in the RF driver's internal command queue. A client can dispatch a command with RF_postCmd() and use the command handle later on to make the RF driver interact with the command.

A negative value has either a special meaning or indicates an error.

See also
RF_pendCmd(), RF_flushCmd(), RF_cancelCmd(), RF_ALLOC_ERROR, RF_CMDHANDLE_FLUSH_ALL

§ RF_Handle

typedef RF_Object* RF_Handle

A handle that is returned by to RF_open().

RF_Handle is used for further RF client interaction with the RF driver. An invalid handle has the value NULL.

§ RF_RatHandle

typedef int8_t RF_RatHandle

RAT handle that is returned by RF_ratCompare() or RF_ratCapture().

An RF_RatHandle is an integer number with value greater than or equal to zero and identifies a Radio Timer Channel in the RF driver's internal RAT module. A client can interact with the RAT module through the RF_ratCompare(), RF_ratCapture() or RF_ratDisableChannel() APIs.

A negative value indicates an error. A typical example when RF_ratCompare() returns with RF_ALLOC_ERROR.

§ RF_Callback

typedef void(* RF_Callback) (RF_Handle h, RF_CmdHandle ch, RF_EventMask e)

Handles events related to RF command execution.

RF command callbacks notify the application of any events happening during RF command execution. Events may either refer to RF core interrupts (RF_Core_Events) or may be generated by the RF driver (RF_Driver_Events).

RF command callbacks are set up as parameter to RF_postCmd() or RF_runCmd() and provide:

  • the relevant driver client handle h which was returned by RF_open(),
  • the relevant radio operation command handle ch,
  • an event mask e containing the occurred events.

RF command callbacks are executed in Software Interrupt (SWI) context and must not perform any blocking operation. The priority is configurable via RFCC26XX_HWAttrsV2 in the board file or RF_CTRL_SET_SWI_PRIORITY in RF_control().

The RF_Callback function type is also used for signaling power events and errors. These are set in RF_Params::pPowerCb and RF_Params::pErrCb respectively. In case of a power event, ch can be ignored and e has RF_EventPowerUp set. In case of an error callback, ch contains an error code instead of a command handle and e has the RF_EventError flag set.

Note
Error and power callbacks will be replaced by RF_ClientCallback in future releases.

§ RF_RatCallback

typedef void(* RF_RatCallback) (RF_Handle h, RF_RatHandle rh, RF_EventMask e, uint32_t compareCaptureTime)

Handles events related to the Radio Timer (RAT).

The RF driver provides an interface to the Radio Timer through RF_ratCompare(), RF_ratCapture() and RF_ratDisableChannel() APIs. Each API call receives an optional input argument of the type RF_RatCallback. When a timer event occurs (compare, capture or error events), the registered callback is invoked.

The RF_RatCallback provides the following argument:

  • the relevant driver client handle h which was returned by RF_open(),
  • the relevant rat timer handle rh which the event is caused by,
  • an event mask e containing the occurred event (RF_EventRatCh or RF_EventError)
  • the captured value or the compare time compareCaptureTime read from the Radio Timer channel.

§ RF_ClientCallback

typedef void(* RF_ClientCallback) (RF_Handle h, RF_ClientEvent event, void *arg)

Handles events related to a driver instance.

The RF driver produces additional events that are not directly related to the execution of a certain command, but happen during general RF driver operations. This includes power-up events, client switching events and others.

A client callback provides the following arguments:

  • the relevant driver client handle h which was returned by RF_open(),
  • an event identifier event,
  • an optional argument arg depending on the event.

RF client callbacks are executed in Software Interrupt (SWI) context and must not perform any blocking operation. The priority is configurable via RFCC26XX_HWAttrsV2 in the board file or RF_CTRL_SET_SWI_PRIORITY in RF_control().

§ RF_GlobalCallback

typedef void(* RF_GlobalCallback) (RF_Handle h, RF_GlobalEvent event, void *arg)

Handles global events as part of PHY configuration.

The RF driver serves additional global, client independent events by invoking the RF_GlobalCallback function registered through RFCC26XX_HWAttrsV2::globalCallback in the board file. The function can subscribe to particular events through the RFCC26XX_HWAttrsV2::globalEventMask, and receives the following arguments:

  • the relevant driver client handle h which was returned by RF_open(),
  • an event identifier event,
  • an optional argument arg depending on the event.

If multiple events happen at the same time, the callback is always invoked separately for each event. Depending on the event, the callback might be invoked in SWI or HWI context.

§ RF_Cmd

typedef struct RF_Cmd_s RF_Cmd

§ RF_SubmitHook

typedef RF_ScheduleStatus(* RF_SubmitHook) (RF_Cmd *pCmdNew, RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue)

Handles the queue sorting algorithm when a new command is submitted to the driver from any of the active clients.

The function is invoked within the RF_scheduleCmd API.

The default algorithm is subscribed through the RFCC26XX_SchedulerPolicy::submitHook and implemented in the RF driver. The arguments are:

  • pCmdNew points to the command to be submitted.
  • pCmdBg is the running background command.
  • pCmdFg is the running foreground command.
  • pPendQueue points to the head structure of pend queue.
  • pDoneQueue points to the head structure of done queue.

In case the radio APIs do not distinguish between background and foreground contexts, the active operation will be returned within the pCmdBg pointer. If there are no commands being executed, both the pCmdBg and pCmdFg pointers are returned as NULL.

§ RF_ExecuteHook

typedef RF_ExecuteAction(* RF_ExecuteHook) (RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue, bool bConflict, RF_Cmd *conflictCmd)

Defines the execution and conflict resolution hook at runtime.

The function is invoked before a scheduled command is about to be executed. If a conflict is identified before the start-time of the next radio command in the pending queue, this information is passed to the hook. The return value of type RF_ExecuteAction determines the policy to be followed by the RF driver.

The arguments are:

  • pCmdBg is the running background command.
  • pCmdFg is the running foreground command.
  • pPendQueue points to the head structure of pend queue.
  • pDoneQueue points to the head structure of done queue.
  • bConflict whether the incoming command conflicts with ongoing.
  • conflictCmd command that conflicts with ongoing.

Enumeration Type Documentation

§ RF_TxPowerTable_PAType

Selects a power amplifier path in a TX power value.

RF_TxPowerTable_PAType selects one of the available power amplifiers on the RF core. It is usually included in a RF_TxPowerTable_Value.

Enumerator
RF_TxPowerTable_DefaultPA 

Default PA.

RF_TxPowerTable_HighPA 

High-power PA.

§ RF_Priority

Scheduling priority of RF operation commands.

When multiple RF driver instances are used at the same time, commands from different clients may overlap. If an RF operation with a higher priority than the currently running operation is scheduled by RF_scheduleCmd(), then the running operation is interrupted.

In single-client applications, RF_PriorityNormal should be used.

Enumerator
RF_PriorityHighest 

Highest priority. Only use this for urgent commands.

RF_PriorityHigh 

High priority. Use this for time-critical commands in synchronous protocols.

RF_PriorityNormal 

Default priority. Use this in single-client applications.

§ RF_PriorityCoex

Priority level for coexistence priority signal.

When the RF driver is configured for three-wire coexistence mode, one of the output wires will signal the priority level of the coexistence request. When RF operations are scheduled with RF_scheduleCmd(), the scheduler can be configured to override the default coexistence priority level for the RF operation.

The coexistence priority level is binary because it translates to a high/low output signal.

Enumerator
RF_PriorityCoexDefault 

Default priority. Use value configured by setup command.

RF_PriorityCoexLow 

Low priority. Override default value configured by setup command.

RF_PriorityCoexHigh 

High priority. Override default value configured by setup command.

§ RF_RequestCoex

Behavior for coexistence request signal.

When the RF driver is configured for three-wire coexistence mode, one of the output wires will signal the request level of the coexistence request. When RF operations are scheduled with RF_scheduleCmd(), the scheduler can be configured to override the default coexistence request line behavior for the RF operation in RX.

This override will be ignored if the option to set request for an entire chain is active.

Enumerator
RF_RequestCoexDefault 

Default request line behavior. Use value configured by setup command.

RF_RequestCoexAssertRx 

Assert REQUEST in RX. Override default value configured by setup command.

RF_RequestCoexNoAssertRx 

Do not assert REQUEST in RX. Override default value configured by setup command.

§ RF_Stat

enum RF_Stat

Status codes for various RF driver functions.

RF_Stat is reported as return value for RF driver functions which execute direct and immediate commands. Such commands are executed by RF_runDirectCmd() and RF_runImmediateCmd() in the first place, but also by some convenience functions like RF_cancelCmd(), RF_flushCmd(), RF_getInfo() and others.

Enumerator
RF_StatBusyError 

Command not executed because RF driver is busy.

RF_StatRadioInactiveError 

Command not executed because RF core is powered down.

RF_StatCmdDoneError 

Command finished with an error.

RF_StatInvalidParamsError 

Function was called with an invalid parameter.

RF_StatCmdEnded 

Cmd is found in the pool but was already ended.

RF_StatError 

General error specifier.

RF_StatCmdDoneSuccess 

Command finished with success.

RF_StatCmdSch 

Command successfully scheduled for execution.

RF_StatSuccess 

Function finished with success.

§ RF_ClientEvent

Client-related RF driver events.

Events originating in the RF driver but not directly related to a specific radio command, are called client events. Clients may subscribe to these events by specifying a callback function RF_Params::pClientEventCb. Events are activated by specifying a bitmask RF_Params::nClientEventMask. The callback is called separately for every event providing an optional argument.

void onClientEvent(RF_Handle h, RF_ClientEvent event, void* arg)
{
switch (event)
{
// Set output port
break;
default:
// Unsubscribed events must not be issued.
assert(false);
}
}
RF_Params params;
params.pClientEventCb = &onClientEvent;
RF_open(...);
Enumerator
RF_ClientEventPowerUpFinished 

The RF core has been powered up the radio setup has been finished.

RF_ClientEventRadioFree 

Radio becomes free after a command has been preempted by a high-priority command of another client. This event is only triggered on a client that has been preempted. Clients may use this event to retry running their low-priority RF operation.

RF_ClientEventSwitchClientEntered 

Signals the client that the RF driver is about to switch over from another client.

§ RF_GlobalEvent

Global RF driver events.

The RF driver provides an interface through the global RFCC26XX_hwAttrs struct to register a global, client independent callback. This callback is typically used to control board related configurations such as antenna switches.

void globalCallback(RF_Handle h, RF_GlobalEvent event, void* arg)
{
switch (event)
{
{
RF_RadioSetup* setupCommand = (RF_RadioSetup*)arg;
// Select antenna path
if (setupCommand->common.commandNo == CMD_PROP_RADIO_DIV_SETUP) {
// Sub-1 GHz ...
} else {
// 2.4 GHz ...
}
}
break;
// Disable antenna switch
break;
default:
// Unsubscribed events must not be issued.
assert(false);
}
}

For the coexistence (coex) feature, some of the events are used to handle the I/O muxing of the GPIO signals for REQUEST, PRIORITY and GRANT.

void globalCallback(RF_Handle h, RF_GlobalEvent event, void* arg)
{
RF_Cmd* pCurrentCmd = (RF_Cmd*)arg;
if (event & RF_GlobalEventInit) {
// Initialize and mux coex I/O pins to RF Core I/O signals
}
else if (event & RF_GlobalEventCmdStart) {
if (pCurrentCmd->coexPriority != RF_PriorityCoexDefault){
// Release PRIORITY pin from RF Core and set it to value of coexPriority
}
}
else if (event & RF_GlobalEventCmdStop) {
if (pCurrentCmd->coexPriority != RF_PriorityCoexDefault) {
// Mux PRIORITY pin to RF Core signal to return to default priority level
}
}
}
See also
RF_GlobalCallback
Enumerator
RF_GlobalEventRadioSetup 

The RF core is being reconfigured through a setup command. The arg argument is a pointer to the setup command. HWI context.

RF_GlobalEventRadioPowerDown 

The RF core is being powered down. The arg argument is empty. SWI context.

RF_GlobalEventInit 

RF_open() is called for the first time (number of registered clients changes from 0 to 1). The arg argument is empty. Task context.

RF_GlobalEventCmdStart 

A command chain is being dispatched to the radio. The arg argument is a pointer to the current command. HWI context.

RF_GlobalEventCmdStop 

Command termination event is handled. The arg argument is a pointer to the current command. HWI context.

RF_GlobalEventCoexControl 

Change to coex configuration is requested The arg argument is pointer to at least 8-bit wide int with value 1=enable, or 0=disable Task/HWI context.

RF_GlobalEventTempNotifyFail 

Registration of temperature notification was unsuccessful (failure returned from temperature driver) The arg argument is empty. HWI context

§ RF_InfoType

Selects the entry of interest in RF_getInfo().

Enumerator
RF_GET_CURR_CMD 

Retrieve a command handle of the current command.

RF_GET_AVAIL_RAT_CH 

Create a bitmask showing available RAT channels.

RF_GET_RADIO_STATE 

Show the current RF core power state. 0: Radio OFF, 1: Radio ON.

RF_GET_SCHEDULE_MAP 

Deprecated. Not supported.

RF_GET_CLIENT_LIST 

Provide the client list.

RF_GET_CLIENT_SWITCHING_TIME 

Provide the client to client switching times.

§ RF_StartType

Controls the behavior of the RF_scheduleCmd() API.

Enumerator
RF_StartNotSpecified 
RF_StartAbs 

§ RF_EndType

enum RF_EndType

Controls the behavior of the RF_scheduleCmd() API.

Enumerator
RF_EndNotSpecified 
RF_EndAbs 
RF_EndRel 
RF_EndInfinit 

§ RF_ExecuteAction

Controls the behavior of the state machine of the RF driver when a conflict is identified run-time between the commands waiting on the pend queue and the commands being actively executed by the radio.

Enumerator
RF_ExecuteActionNone 

Execute if no conflict, let current command finish if conflict.

RF_ExecuteActionRejectIncoming 

Abort the incoming command, letting the ongoing command finish.

RF_ExecuteActionAbortOngoing 

Abort the ongoing command and run dispatcher again.

§ RF_ScheduleStatus

Describes the location within the pend queue where the new command was inserted by the scheduler.

Enumerator
RF_ScheduleStatusError 
RF_ScheduleStatusNone 
RF_ScheduleStatusTop 
RF_ScheduleStatusMiddle 
RF_ScheduleStatusTail 
RF_ScheduleStatusPreempt 

§ RF_AllowDelay

Controls the behavior of the RF_scheduleCmd() API.

Enumerator
RF_AllowDelayNone 
RF_AllowDelayAny 

§ RF_RatSelectChannel

Select the preferred RAT channel through the configuration of RF_ratCompare() or RF_ratCapture().

If RF_RatChannelAny is provided within the channel configuration (default), the API will allocate the first available channel. Otherwise, it tries to allocate the requested channel, and if it is not available, returns with RF_ALLOC_ERROR.

Enumerator
RF_RatChannelAny 

Chose the first available channel.

RF_RatChannel0 

Use RAT user channel 0.

RF_RatChannel1 

Use RAT user channel 1.

RF_RatChannel2 

Use RAT user channel 2.

§ RF_RatCaptureSource

Selects the source signal for RF_ratCapture().

The source of a capture event can be selected through the source field of the RF_RatConfigCapture configuration structure.

Enumerator
RF_RatCaptureSourceRtcUpdate 

Selects the RTC update signal source.

RF_RatCaptureSourceEventGeneric 

Selects the Generic event of Event Fabric as source.

RF_RatCaptureSourceRfcGpi0 

Selects the RFC_GPI[0] as source. This can be used i.e. to capture events on a GPIO. This requires that the GPIO is connected to RFC_GPO[0] from the GPIO driver.

RF_RatCaptureSourceRfcGpi1 

Selects the RFC_GPO[1] as source. This can be used i.e. to capture events on a GPIO. This requires that the GPIO is connected to RFC_GPO[1] from the GPIO driver.

§ RF_RatCaptureMode

Selects the mode of RF_ratCapture().

The trigger mode of a capture event can be selected through the mode field of RF_RatConfigCapture configuration structure.

Enumerator
RF_RatCaptureModeRising 

Rising edge of the selected source will trigger a capture event.

RF_RatCaptureModeFalling 

Falling edge of the selected source will trigger a capture event.

RF_RatCaptureModeBoth 

Both rising and falling edges of the selected source will generate capture events.

§ RF_RatCaptureRepetition

Selects the repetition of RF_ratCapture().

The configuration of a capture channel also defines whether the channel should be freed or automatically rearmed after a capture event occurred. In the latter case, the user needs to free the channel manually through the RF_ratDisableChannel() API.

Enumerator
RF_RatCaptureSingle 

Free the channel after the first capture event.

RF_RatCaptureRepeat 

Rearm the channel after each capture events.

§ RF_RatOutputMode

Selects the mode of the RAT_GPO[x] for RF_ratCompare() or RF_ratCapture().

In case of compare mode, the channel can generate an output signal of the selected mode on the configured RAT_GPO[x] interface, and can be interconnected with other subsystems through the RFC_GPO[x] or Event Fabric. An example use case is to generate a pulse on a GPIO.

In case of capture mode, the channel can also generate an output signal of the selected mode on the configured RAT_GPO[x] interface. Note that the configuration of this output event is independent of the source signal of the capture event. An example use case is to generate a pulse on a GPIO on each raising edge of another GPIO source.

Enumerator
RF_RatOutputModePulse 

Generates a one-clock period width pulse.

RF_RatOutputModeSet 

Sets the output high on a RAT event.

RF_RatOutputModeClear 

Sets the output low on a RAT event.

RF_RatOutputModeToggle 

Inverts the polarity of the output.

RF_RatOutputModeAlwaysZero 

Sets the output low independently of any RAT events.

RF_RatOutputModeAlwaysOne 

Sets the output high independently of any RAT events.

§ RF_RatOutputSelect

Selects GPO to be used with RF_ratCompare() or RF_ratCapture().

RAT_GPO[0] - Reserved by the RF core. User shall not modify the configuration, but can observe the signal through any of RFC_GPO[0:3]. RAT_GPO[1] - Reserved by the RF core only if sync word detection is enabled. Otherwise can be used through RFC_GPO[0:3]. RAT_GPO[2:3] - Available and can be used through any of the RFC_GPO[0:3]. RAT_GPO[4:7] - Available and can be used through the Event fabric.

Enumerator
RF_RatOutputSelectRatGpo1 

Configure RAT_CHANNEL[x] to interface with RAT_GPO[1].

RF_RatOutputSelectRatGpo2 

Configure RAT_CHANNEL[x] to interface with RAT_GPO[2].

RF_RatOutputSelectRatGpo3 

Configure RAT_CHANNEL[x] to interface with RAT_GPO[3].

RF_RatOutputSelectRatGpo4 

Configure RAT_CHANNEL[x] to interface with RAT_GPO[4].

RF_RatOutputSelectRatGpo5 

Configure RAT_CHANNEL[x] to interface with RAT_GPO[5].

RF_RatOutputSelectRatGpo6 

Configure RAT_CHANNEL[x] to interface with RAT_GPO[6].

RF_RatOutputSelectRatGpo7 

Configure RAT_CHANNEL[x] to interface with RAT_GPO[7].

Function Documentation

§ RF_open()

RF_Handle RF_open ( RF_Object pObj,
RF_Mode pRfMode,
RF_RadioSetup pRadioSetup,
RF_Params params 
)

Creates a a new client instance of the RF driver.

This function initializes an RF driver client instance using pObj as storage. It does not power up the RF core. Once the client starts the first RF operation command later in the application, the RF core is powered up and set into a PHY mode specified by pRfMode. The chosen PHY is then configured by a radio setup command pRadioSetup. Whenever the RF core is powered up, the RF driver re-executes the radio setup command pRadioSetup. Additional driver behavior may be set by an optional params.

// Define parameters
RF_Params rfParams;
rfParams.nInactivityTimeout = 4;
RF_Params_init(&rfParams);
rfParams.nInactivityTimeout = 1701; // microseconds
RF_Handle rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
Note
Calling context : Task
Parameters
pObjPointer to a RF_Object that will hold the state for this RF client. The object must be in persistent and writable memory.
pRfModePointer to a RF_Mode struct holding PHY information
pRadioSetupPointer to the radio setup command used for this client. This is re-executed by the RF Driver on each power-up.
paramsPointer to an RF_Params object with the desired driver configuration. A NULL pointer results in the default configuration being loaded.
Returns
A handle for further RF driver calls on success. Otherwise NULL.

§ RF_close()

void RF_close ( RF_Handle  h)

Close client connection to RF driver.

Allows a RF client (high-level driver or application) to close its connection to the RF driver. RF_close pends on all commands in the command queue before closing the connection. If a client has access to the radio by using RF_RequestAccess API, and the same client calls RF_close, then the connection to the RF driver is closed immediately without waiting for the access duration to be over.

Note
Calling context : Task
Parameters
hHandle previously returned by RF_open()

§ RF_getCurrentTime()

uint32_t RF_getCurrentTime ( void  )

Return current radio timer value.

If the radio is powered returns the current radio timer value, if not returns a conservative estimate of the current radio timer value

Note
Calling context : Task/SWI/HWI
Returns
Current radio timer value

§ RF_postCmd()

RF_CmdHandle RF_postCmd ( RF_Handle  h,
RF_Op pOp,
RF_Priority  ePri,
RF_Callback  pCb,
RF_EventMask  bmEvent 
)

Appends RF operation commands to the driver's command queue and returns a command handle.

The RF operation pOp may either represent a single operation or may be the first operation in a chain. If the command queue is empty, the pCmd is dispatched immediately. If there are other operations pending, then pCmd is processed after all other commands have been finished. The RF operation command must be compatible to the RF_Mode selected by RF_open(), e.g. proprietary commands can only be used when the RF core is configured for proprietary mode.

The returned command handle is an identifier that can be used to control command execution later on, for instance with RF_pendCmd() or RF_cancelCmd(). It is a 16 Bit signed integer value, incremented on every new command. If the RF driver runs out of command containers, RF_ALLOC_ERROR is returned.

The priority ePri is only relevant in multi-client applications where commands of distinct clients may interrupt each other. Only commands started by RF_scheduleCmd() can preempt running commands. RF_postCmd() or RF_runCmd() do never interrupt a running command. In single-client applications, ePri is ignored and should be set to RF_PriorityNormal.

A callback function pCb might be specified to get notified about events during command execution. Events are subscribed by the bit mask bmEvent. Valid event flags are specified in RF_Core_Events and RF_Driver_Events. If no callback is set, RF_pendCmd() can be used to synchronize the current task to command execution. For this it is necessary to subscribe all relevant events. The termination events RF_EventLastCmdDone, RF_EventCmdCancelled, RF_EventCmdAborted and RF_EventCmdStopped are always implicitly subscribed.

The following limitations apply to the execution of command chains:

  • If TRIG_ABSTIME is used as a start trigger for the first command, TRIG_REL_FIRST_START can not be used for any other command. This is because the RF driver may insert a frequency-select command (CMD_FS) at the front of the chain when it performs an automatic power-up.
  • If a command chain has more than one CMD_FS, the first CMD_FS in the chain is cached. This CMD_FS is used on the next automatic power-up.
  • To avoid execution of cached CMD_FS and directly use a new CMD_FS on power up, place CMD_FS at the head of the command chain.
Note
Calling context : Task/SWI
See also
RF_pendCmd(), RF_runCmd(), RF_scheduleCmd(), RF_RF_cancelCmd(), RF_flushCmd(), RF_getCmdOp()
Parameters
hDriver handle previously returned by RF_open()
pOpPointer to the RF operation command.
ePriPriority of this RF command (used for arbitration in multi-client systems)
pCbCallback function called during command execution and upon completion. If RF_postCmd() fails, no callback is made.
bmEventBitmask of events that will trigger the callback or that can be pended on.
Returns
A handle to the RF command. Return value of RF_ALLOC_ERROR indicates error.

§ RF_defaultSubmitPolicy()

RF_ScheduleStatus RF_defaultSubmitPolicy ( RF_Cmd pCmdNew,
RF_Cmd pCmdBg,
RF_Cmd pCmdFg,
List_List *  pPendQueue,
List_List *  pDoneQueue 
)

Sorts and adds commands to the RF driver internal command queue.

Parameters
pCmdNewPointer to the command to be submitted.
pCmdBgRunning background command.
pCmdFgRunning foreground command.
pPendQueuePointer to the head structure of pend queue.
pDoneQueuePointer to the head structure of done queue..
Returns
RF_defaultSubmitPolicy identifies the success or failure of queuing.

§ RF_defaultExecutionPolicy()

RF_ExecuteAction RF_defaultExecutionPolicy ( RF_Cmd pCmdBg,
RF_Cmd pCmdFg,
List_List *  pPendQueue,
List_List *  pDoneQueue,
bool  bConflict,
RF_Cmd conflictCmd 
)

Makes a final decision before dispatching a scheduled command.

Parameters
pCmdBgRunning background command.
pCmdFgRunning foreground command.
pPendQueuePointer to the head structure of pend queue.
pDoneQueuePointer to the head structure of done queue.
bConflictWhether the incoming command conflicts with the ongoing.
conflictCmdCommand that conflicts with ongoing.
Returns
RF_defaultSubmitPolicy identifies the success or failure of queuing.

§ RF_ScheduleCmdParams_init()

void RF_ScheduleCmdParams_init ( RF_ScheduleCmdParams pSchParams)

Initialize the configuration structure to default values to be used with the RF_scheduleCmd() API.

Note
Calling context : Task/SWI/HWI
Parameters
pSchParamsPointer to the configuration structure.
Returns
none

§ RF_scheduleCmd()

RF_CmdHandle RF_scheduleCmd ( RF_Handle  h,
RF_Op pOp,
RF_ScheduleCmdParams pSchParams,
RF_Callback  pCb,
RF_EventMask  bmEvent 
)

Schedule an RF operation (chain) to the command queue.

Schedule an RF_Op to the RF command queue of the client with handle h.
The command can be the first in a chain of RF operations or a standalone RF operation. If a chain of operations are posted they are treated atomically, i.e. either all or none of the chained operations are run.
All operations must be posted in strictly increasing chronological order. Function returns immediately.

Limitations apply to the operations posted:

  • The operation must be in the set supported in the chosen radio mode when RF_open() was called
  • Only a subset of radio operations are supported
  • Only some of the trigger modes are supported with potential power saving (TRIG_NOW, TRIG_ABSTIME)
Note
Calling context : Task/SWI
Parameters
hHandle previously returned by RF_open()
pOpPointer to the RF_Op. Must normally be in persistent and writable memory
pSchParamsPointer to the schedule command parameter structure
pCbCallback function called upon command completion (and some other events). If RF_scheduleCmd() fails no callback is made
bmEventBitmask of events that will trigger the callback.
Returns
A handle to the RF command. Return value of RF_ALLOC_ERROR indicates error.

§ RF_pendCmd()

RF_EventMask RF_pendCmd ( RF_Handle  h,
RF_CmdHandle  ch,
RF_EventMask  bmEvent 
)

Synchronizes the calling task to an RF operation command ch and returns accumulated event flags.

After having dispatched an RF operation represented by ch with RF_postCmd(), the command is running in parallel on the RF core. Thus, it might be desirable to synchronize the calling task to the execution of the command. With RF_pendCmd(), the application can block until one of the events specified in bmEvent occurs or until the command finishes. The function consumes and returns all accumulated event flags that occurred during execution if they have been previously subscribed by RF_postCmd(). Possible events are specified in RF_Core_Events and RF_Driver_Events. The termination events RF_EventLastCmdDone, RF_EventCmdCancelled, RF_EventCmdAborted and RF_EventCmdStopped are always implicitly subscribed and can not be masked.

RF_pendCmd() may be called multiple times for the same command.

If RF_pendCmd() is called for a command handle representing a finished command, then only the RF_EventLastCmdDone flag is returned, regardless of how the command finished.

If the command has also a callback set, the callback is executed before RF_pendCmd() returns.

Example:

// Dispatch a command to the RF driver's command queue
RF_CmdHandle ch = RF_postCmd(driver, (RF_Op*)&CMD_PROP_RX, RF_PriorityNormal, NULL, RF_EventRxEntryDone);
assert(ch != RF_ALLOC_ERROR);
bool finished = false;
while (finished == false)
{
// Synchronize to events during command execution.
uint32_t events = RF_pendCmd(driver, ch, RF_EventRxEntryDone);
// Check events that happen during execution
if (events & RF_EventRxEntryDone)
{
// Process packet
}
{
finished = true;
}
// ...
}
Note
Calling context : Task
Parameters
hDriver handle previously returned by RF_open()
chCommand handle previously returned by RF_postCmd().
bmEventBitmask of events that make RF_pendCmd() return. Termination events are always implicitly subscribed.
Returns
Event flags accumulated during command execution.
See also
RF_postCmd()

§ RF_runCmd()

RF_EventMask RF_runCmd ( RF_Handle  h,
RF_Op pOp,
RF_Priority  ePri,
RF_Callback  pCb,
RF_EventMask  bmEvent 
)

Runs synchronously an RF operation command or a chain of commands and returns the termination reason.

This function appends an RF operation command or a chain of commands to the RF driver's command queue and then waits for it to complete. A command is completed if one of the termination events RF_EventLastCmdDone, RF_EventCmdCancelled, RF_EventCmdAborted, RF_EventCmdStopped occurred.

This function is a combination of RF_postCmd() and RF_pendCmd(). All options and limitations for RF_postCmd() apply here as well.

An application should always ensure that the command completed in the expected way and with an expected status code.

Note
Calling context : Task
Parameters
hDriver handle previously returned by RF_open()
pOpPointer to the RF operation command.
ePriPriority of this RF command (used for arbitration in multi-client systems)
pCbCallback function called during command execution and upon completion. If RF_runCmd() fails, no callback is made.
bmEventBitmask of events that will trigger the callback or that can be pended on.
Returns
The relevant termination event.
See also
RF_postCmd(), RF_pendCmd(), RF_cancelCmd(), RF_flushCmd()

§ RF_runScheduleCmd()

RF_EventMask RF_runScheduleCmd ( RF_Handle  h,
RF_Op pOp,
RF_ScheduleCmdParams pSchParams,
RF_Callback  pCb,
RF_EventMask  bmEvent 
)

Runs synchronously a (chain of) RF operation(s) for dual or single-mode.

Allows a (chain of) operation(s) to be scheduled to the command queue and then waits for it to complete.
A command is completed if one of the RF_EventLastCmdDone, RF_EventCmdCancelled, RF_EventCmdAborted, RF_EventCmdStopped occurred.

Note
Calling context : Task
Only one call to RF_pendCmd() or RF_runScheduleCmd() can be made at a time for each client
Parameters
hHandle previously returned by RF_open()
pOpPointer to the RF_Op. Must normally be in persistent and writable memory
pSchParamsPointer to the schedule command parameter structure
pCbCallback function called upon command completion (and some other events). If RF_runScheduleCmd() fails, no callback is made.
bmEventBitmask of events that will trigger the callback.
Returns
The relevant command completed event.

§ RF_cancelCmd()

RF_Stat RF_cancelCmd ( RF_Handle  h,
RF_CmdHandle  ch,
uint8_t  mode 
)

Abort/stop/cancel single command in command queue.

If command is running, aborts/stops it and posts callback for the aborted/stopped command.
If command has not yet run, cancels it it and posts callback for the canceled command.
If command has already run or been aborted/stopped/canceled, has no effect.
If RF_cancelCmd is called from a Swi context with same or higher priority than RF Driver Swi, when the RF core is powered OFF -> the cancel callback will be delayed until the next power-up cycle.

Note
Calling context : Task/SWI
Parameters
hHandle previously returned by RF_open()
chCommand handle previously returned by RF_postCmd().
mode1: Stop gracefully, 0: abort abruptly
Returns
RF_Stat indicates if command was successfully completed

§ RF_flushCmd()

RF_Stat RF_flushCmd ( RF_Handle  h,
RF_CmdHandle  ch,
uint8_t  mode 
)

Abort/stop/cancel command and any subsequent commands in command queue.

If command is running, aborts/stops it and then cancels all later commands in queue.
If command has not yet run, cancels it and all later commands in queue.
If command has already run or been aborted/stopped/canceled, has no effect.
The callbacks for all canceled commands are issued in chronological order.
If RF_flushCmd is called from a Swi context with same or higher priority than RF Driver Swi, when the RF core is powered OFF -> the cancel callback will be delayed until the next power-up cycle.

Note
Calling context : Task/SWI
Parameters
hHandle previously returned by RF_open()
chCommand handle previously returned by RF_postCmd().
mode1: Stop gracefully, 0: abort abruptly
Returns
RF_Stat indicates if command was successfully completed

§ RF_runImmediateCmd()

RF_Stat RF_runImmediateCmd ( RF_Handle  h,
uint32_t *  pCmdStruct 
)

Send any Immediate command.

Immediate Command is send to RDBELL, if radio is active and the RF_Handle points to the current client.
In other appropriate RF_Stat values are returned.

Note
Calling context : Task/SWI/HWI
Parameters
hHandle previously returned by RF_open()
pCmdStructPointer to the immediate command structure
Returns
RF_Stat indicates if command was successfully completed

§ RF_runDirectCmd()

RF_Stat RF_runDirectCmd ( RF_Handle  h,
uint32_t  cmd 
)

Send any Direct command.

Direct Command value is send to RDBELL immediately, if radio is active and the RF_Handle point to the current client.
In other appropriate RF_Stat values are returned.

Note
Calling context : Task/SWI/HWI
Parameters
hHandle previously returned by RF_open()
cmdDirect command value.
Returns
RF_Stat indicates if command was successfully completed.

§ RF_yield()

void RF_yield ( RF_Handle  h)

Signal that radio client is not going to issue more commands in a while.

Hint to RF driver that, irrespective of inactivity timeout, no new further commands will be issued for a while and thus the radio can be powered down at the earliest convenience. In case the RF_yield() is called within a callback, the callback will need to finish and return before the power down sequence is initiated. Posting new commands to the queue will cancel any pending RF_yield() request.

Note
Calling context : Task
Parameters
hHandle previously returned by RF_open()

§ RF_Params_init()

void RF_Params_init ( RF_Params params)

Function to initialize the RF_Params struct to its defaults.

Parameters
paramsAn pointer to RF_Params structure for initialization

Defaults values are: nInactivityTimeout = BIOS_WAIT_FOREVER nPowerUpDuration = RF_DEFAULT_POWER_UP_TIME

§ RF_getInfo()

RF_Stat RF_getInfo ( RF_Handle  h,
RF_InfoType  type,
RF_InfoVal pValue 
)

Get value for some RF driver parameters.

Note
Calling context : Task/SWI/HWI
Parameters
hHandle previously returned by RF_open()
typeRequest value parameter defined by RF_InfoType
pValuePointer to return parameter values specified by RF_InfoVal
Returns
RF_Stat indicates if command was successfully completed

§ RF_getRssi()

int8_t RF_getRssi ( RF_Handle  h)

Get RSSI value.

Note
Calling context : Task/SWI/HWI
Parameters
hHandle previously returned by RF_open()
Returns
RSSI value. Return value of RF_GET_RSSI_ERROR_VAL indicates error case.

§ RF_getCmdOp()

RF_Op* RF_getCmdOp ( RF_Handle  h,
RF_CmdHandle  cmdHnd 
)

Get command structure pointer.

Note
Calling context : Task/SWI/HWI
Parameters
hHandle previously returned by RF_open()
cmdHndCommand handle returned by RF_postCmd()
Returns
Pointer to the command structure.

§ RF_RatConfigCompare_init()

void RF_RatConfigCompare_init ( RF_RatConfigCompare channelConfig)

Initialize the configuration structure to be used to set up a RAT compare event.

Note
Calling context : Task/SWI/HWI
Parameters
channelConfigPointer to the compare configuration structure.
Returns
none

§ RF_RatConfigCapture_init()

void RF_RatConfigCapture_init ( RF_RatConfigCapture channelConfig)

Initialize the configuration structure to be used to set up a RAT capture event.

Note
Calling context : Task/SWI/HWI
Parameters
channelConfigPointer to the capture configuration structure.
Returns
none

§ RF_RatConfigOutput_init()

void RF_RatConfigOutput_init ( RF_RatConfigOutput ioConfig)

Initialize the configuration structure to be used to set up a RAT IO.

Note
Calling context : Task/SWI/HWI
Parameters
ioConfigPointer to the IO configuration structure.
Returns
none

§ RF_ratCompare()

RF_RatHandle RF_ratCompare ( RF_Handle  rfHandle,
RF_RatConfigCompare channelConfig,
RF_RatConfigOutput ioConfig 
)

Setup a Radio Timer (RAT) channel in compare mode.

The RF_ratCompare() API sets up one of the three available RAT channels in compare mode. When the compare event happens at the given compare time, the registered callback is invoked.

The RF driver handles power management. If the provided compare time is far into the future (and there is no other constraint set i.e. due to radio command execution), the RF core will be powered OFF and the device will enter the lowest possible power state. The RF core will be automatically powered ON just before the registered compare event. The callback function is served upon expiration of the allocated channel. The function is invoked with event type RF_EventRatCh and runs in SWI context.

The API generates a "one-shot" compare event. Since the channel is automatically freed before the callback is served, the same channel can be reallocated from the callback itself through a new API call.

In case there were no available channels at the time of API call, the function returns with RF_ALLOC_ERROR and no callback is invoked.

In case a runtime error occurs after the API successfully allocated a channel, the registered callback is invoked with event type RF_EventError. A typical example is when the provided compare time is in the past and rejected by the RF core itself.

The events issued by the RAT timer can be output from the timer module through the RAT_GPO interface, and can be interconnected with other parts of the system through the RFC_GPO or the Event Fabric. The mapping between the allocated RAT channel and the selected RAT_GPO can be controlled through the optional ioConfig argument of RF_ratCompare(). The possible RAT_GPO[x] are defined in RF_RatOutputSelect.

Note
Calling context : Task/SWI
Parameters
rfHandleHandle previously returned by RF_open().
channelConfigPointer to configuration structure needed to set up a channel in compare mode.
ioConfigPointer to a configuration structure to set up the RAT_GPOs for the allocated channel (optional).
Returns
Allocated RAT channel. If allocation fails, RF_ALLOC_ERROR is returned.
See also
RF_RatConfigCompare_init(), RF_RatConfigOutput_init(), RF_ratDisableChannel(), RF_ratCapture()

§ RF_ratCapture()

RF_RatHandle RF_ratCapture ( RF_Handle  rfHandle,
RF_RatConfigCapture channelConfig,
RF_RatConfigOutput ioConfig 
)

Setup a Radio Timer (RAT) channel in capture mode.

The RF_ratCapture() API sets up one of the three available RAT channels in capture mode. The registered callback is invoked on the capture event.

The RF driver handles power management. If the RF core is OFF when the RF_ratCapture() is called, it will be powered ON immediately and the RAT channel will be configured to capture mode. As long as at least one of the three RAT channels are in capture mode, the RF core will be kept ON. The callback function is served upon a capture event occurs. The function is invoked with event type RF_EventRatCh and runs in SWI context.

In case the channel is configured into single capture mode, the channel is automatically freed before the callback is called. In repeated capture mode, the channel remains allocated and automatically rearmed.

In case there were no available channels at the time of API call, the function returns with RF_ALLOC_ERROR and no callback is invoked.

In case a runtime error occurs after the API successfully allocated a channel, the registered callback is invoked with event type RF_EventError. A typical example is when the provided compare time is in the past and rejected by the RF core itself.

The events issued by the RAT timer can be output from the timer module through the RAT_GPO interface, and can be interconnected with other parts of the system through the RFC_GPO or the Event Fabric. The mapping between the allocated RAT channel and the selected RAT_GPO can be controlled through the optional ioConfig argument of RF_ratCapture(). The possible RAT_GPO[x] are defined in RF_RatOutputSelect. Note that this configuration is independent of the source signal of the capture event.

Note
Calling context : Task/SWI
Parameters
rfHandleHandle previously returned by RF_open().
channelConfigPointer to configuration structure needed to set up a channel in compare mode.
ioConfigPointer to a configuration structure to set up the RAT_GPO for the allocated channel (optional).
Returns
Allocated RAT channel. If allocation fails, RF_ALLOC_ERROR is returned.
See also
RF_RatConfigCapture_init(), RF_RatConfigOutput_init() , RF_ratDisableChannel(), RF_ratCompare()

§ RF_ratDisableChannel()

RF_Stat RF_ratDisableChannel ( RF_Handle  rfHandle,
RF_RatHandle  ratHandle 
)

Disable a RAT channel.

The RF_RatHandle returned by the RF_ratCompare() or RF_ratCapture() APIs can be used for further interaction with the Radio Timer. Passing the handle to RF_ratDisableChannel() will abort a compare/capture event, and the provided channel is deallocated. No callback is invoked. This API can be called both if the RF core is ON or OFF. After the channel is freed, the next radio event will be rescheduled. A typical use case if a channel is configured in repeated capture mode, and the application decides to abort this operation.

Note
Calling context : Task/SWI
Parameters
rfHandleHandle previously returned by RF_open().
ratHandleRF_RatHandle returned by RF_ratCompare() or RF_ratCapture().
Returns
RF_Stat indicates if command was successfully completed.
See also
RF_ratCompare(), RF_ratCapture()

§ RF_control()

RF_Stat RF_control ( RF_Handle  h,
int8_t  ctrl,
void *  args 
)

Set RF control parameters.

Note
Calling context : Task
Parameters
hHandle previously returned by RF_open()
ctrlControl codes
argsPointer to control arguments
Returns
RF_Stat indicates if API call was successfully completed.

§ RF_requestAccess()

RF_Stat RF_requestAccess ( RF_Handle  h,
RF_AccessParams pParams 
)

Request radio access.

Scope:

  1. Only supports request access which start immediately.
  2. The RF_AccessParams duration should be less than a pre-defined value RF_REQ_ACCESS_MAX_DUR_US in RFCC26X2_multiMode.c.
  3. The RF_AccessParams priority should be set RF_PriorityHighest.
  4. Single request for a client at anytime.
  5. Command from different client are blocked until the radio access period is completed.
Note
Calling context : Task
Parameters
hHandle previously returned by RF_open()
pParamsPointer to RF_AccessRequest parameters
Returns
RF_Stat indicates if API call was successfully completed.

§ RF_getTxPower()

RF_TxPowerTable_Value RF_getTxPower ( RF_Handle  h)

Returns the currently configured transmit power configuration.

This function returns the currently configured transmit power configuration under the assumption that it has been previously set by RF_setTxPower(). The value might be used for reverse lookup in a TX power table. If no power has been programmed, it returns an invalid value.

// error, value not valid
}
Parameters
hHandle previously returned by RF_open()
Returns
PA configuration struct
See also
RF_setTxPower(), RF_TxPowerTable_findPowerLevel()

§ RF_setTxPower()

RF_Stat RF_setTxPower ( RF_Handle  h,
RF_TxPowerTable_Value  value 
)

Updates the transmit power configuration of the RF core.

This function programs a new TX power value and returns a status code. The API will return with RF_StatBusyError if there are still pending commands in the internal queue. In case of success, RF_StatSuccess is returned and the new configuration becomes effective from the next radio operation.

Some devices provide an integrated high-power PA in addition to the Default PA. On these devices the API accepts configurations for both, and if value selects a different PA, the globalCallback is invoked. The implementation of globalCallback is board specific and can be used to reconfigure the external RF switches (if any).

Parameters
hHandle previously returned by RF_open()
valueTX power configuration value.
Returns
RF_StatSuccess on success, otherwise an error code.
See also
RF_getTxPower(), RF_TxPowerTable_Value, RF_TxPowerTable_findValue()

§ RF_TxPowerTable_findPowerLevel()

int8_t RF_TxPowerTable_findPowerLevel ( RF_TxPowerTable_Entry  table[],
RF_TxPowerTable_Value  value 
)

Retrieves a power level in dBm for a given power configuration value.

RF_TxPowerTable_findPowerLevel() searches in a lookup table for a given transmit power configuration value and returns the power level in dBm if a matching configuration is found. If value can not be found, RF_TxPowerTable_INVALID_DBM is returned.

This function does a reverse lookup compared to RF_TxPowerTable_findValue() and has O(n). It is assumed that table is terminated by a RF_TxPowerTable_TERMINATION_ENTRY.

Parameters
tableList of RF_TxPowerTable_Entry entries, terminated by RF_TxPowerTable_TERMINATION_ENTRY.
valuePower configuration value.
Returns
Human readable power level in dBm on success, otherwise RF_TxPowerTable_INVALID_DBM.

§ RF_TxPowerTable_findValue()

RF_TxPowerTable_Value RF_TxPowerTable_findValue ( RF_TxPowerTable_Entry  table[],
int8_t  powerLevel 
)

Retrieves a power configuration value for a given power level in dBm.

RF_TxPowerTable_findValue() searches in a lookup table for a given transmit power level powerLevel in dBm and returns a matching power configuration. If powerLevel can not be found, RF_TxPowerTable_INVALID_VALUE is returned.

This function performs a linear search in table and has O(n). It is assumed that table is defined in ascending order and is terminated by a RF_TxPowerTable_TERMINATION_ENTRY.

The following special values for powerLevel are also accepted:

Parameters
tableList of RF_TxPowerTable_Entry entries, terminated by RF_TxPowerTable_TERMINATION_ENTRY.
powerLevelHuman-readable power level in dBm.
Returns
PA configuration value on success. otherwise RF_TxPowerTable_INVALID_VALUE.

§ RF_enableHPOSCTemperatureCompensation()

RF_Stat RF_enableHPOSCTemperatureCompensation ( void  )

Enables temperature monitoring and temperature based drift compensation.

Returns
RF_StatSuccess if succesful or RF_StatInvalidParamsError if temperature notification fails to register.
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale