CC2640R2 to CC26x2

This section describes the main differences an Application Developer must be aware of between the CC2640R2 and the CC26x2 along with a porting guide to demonstrate the migration effort.

Features and Benefits

Increased Processing Power and Scalability

The CC26x2 is a wireless MCU with a dedicated Arm Cortex-M4F application processor that is pin-to-pin compatible to the CC2640R2 in the 7x7mm QFN package.

More memory is available with an increase of non-volatile memory from 275kB to 608kB. This breaks down into 352kB Flash memory + 256 KB ROM. RAM has also increased from 28 kB to 80 kB. The availability of this increased memory provides support for Over-the-Air Downloads (OAD), larger applications, and more simultaneous connections.

Other improvements include an additional UART and a 70% reduction in current consumption in the Sensor Controller.

Bluetooth 5.2 Enabled

If your project wasn’t already on a BLE5 platform, the CC26x2 will provide the ability to support the features of Bluetooth 5.2. This includes features such as higher throughput, longer range, advertising extensions, and improved coexistence with other wireless technology. For a full list of supported features, see Supported Bluetooth LE Stack Features.

Enhanced Security

With additional hardware security accelerators for AES-128/256, SHA-256, and ECC, CC26x2 saves five times the processing time and current consumption for implementing security algorithms. This is critical to enable strong network security.

CC26x2R LaunchPad Support

All example applications are compatible with the CC26x2R LaunchPad development kit. These features allow for a unified development experience and empowers developers to rapidly release to market.

For more information on this device, see the CC26x2R LaunchPad tool page.

Compatibility Notes

Due to a number of improvements and feature additions, the recommended migration path for customers is to start with a CC26x2 based project and migrate any custom application code and project configuration to the new project.

The following sections describe, in general terms, the software differences when migrating from CC2640R2 to CC26x2.

SysConfig

The SimpleLink CC13xx/CC26xx SDK leverages SysConfig to configure both the application and BLE5-Stack. For more information on the tool, see Get started with SysConfig.

Additionally, refer to SysConfig Migration for specific migration details. The above reference should be used as a guide to familiarize yourself with the changes that SysConfig introduces and does not need to be explicitly followed if you are starting with an unmodified BLE5-Stack 2.02.09.00 project.

Application TI-RTOS Build Configuration

Depending on the example project, the available application build configurations are:

Table 50. Project build configurations

Build Configuration

Description

Release

Turns off debug features (i.e. used in production)

Debug

Provides debug feature improvements: Enables exceptions, BIOS asserts, BIOS logging handling, places the BIOS in flash.

Each build configuration provided is user configurable. For CCS users, the build configuration can be modified in the SysConfig file located in the project directory.

Stack Build Configuration

All BLE5-Stack 2.02.09.00 applications configuration’s use a single project configuration. This build configuration yields additional flash footprint optimizations by the linker since the application and stack can share contiguous flash pages. This configuration is further discussed in the Single Project Configuration section of this User’s Guide.

Formerly, the BLE stack was configured using the build_config.opt command file. The BLE5-Stack 2.02.09.00 now uses SysConfig to configure the BLE5-Stack and generates the ti_build_config.opt.

For more information on this, see BLE5-Stack SysConfig Features.

Predefined Symbols

The predefined symbols have been moved from the project properties. Instead, SysConfig is used to configure and generate any relevant project defines inside ti_ble_app_config.opt.

For more information on this, see BLE5-Stack SysConfig Features.

GAP Role Removal

All GAP Roles source and header files (peripheral.c, peripheral.h, central.c, central.h, etc.) have been removed. With the GAP Role changes, GAP events are being handled differently. GAP events are now handle in the bleapputil_task.c file located in the commonBLEAppUtil folders. These events are pass in the app folder such as app_peripheral.c file and so on. This is where users should use these events.

Further discussion of this is in Porting BLE-Stack to BLE5-Stack.

Host Privacy

The design of the Host Privacy in BLE5-Stack 2.02.09.00 is a complete redesign of the former one on the CC2640R2.

In BLE5-Stack 2.02.09.00, the Host is responsible for the following tasks:

  • Configuring the privacy mode and own address type to conduct desired privacy operations on the controller

  • Performing pairing procedure to exchange device identity information including IRK, identity address, and address type

  • Updating peer device’s address information in the link DB after acquiring the identity information through pairing process

  • Managing resolving list by adding/removing resolving list entries or clearing

  • Storing resolving list to NV and restore it from, so that the privacy information is persistent across power cycles

Porting BLE-Stack to BLE5-Stack

This section will describe how to port from a BLEStack project to a BLE5Stack project.

Note

This example is specifically for CC2640R2 SDK 5.30 to CC13xx/CC26xx SDK 6.10 but the steps are similar for all cases. Individual differences can be found in the relevant Porting Guides

This guide will describe a way to port a project from CC2640R2 SDK 5.30 to a CC13xx/CC26xx SDK 6.10 project. If your project uses the BLE-Stack, please note that this guide won’t show how to add BLE5 features. However porting your project will allow the use of BLE5 features that are contained in CC13xx/CC26xx SDK 6.10.

See the following tables for API replacements:

Porting Steps

To minimize project configuration differences, start with an example project in the CC13xx/CC26xx SDK 6.10. For example, if your base project was simple_peripheral in the CC2640R2 SDK 5.30, use simple_peripheral in the CC13xx/CC26xx SDK 6.10 as the project base to implement application-level modifications on. In other words, no modifications will be made to the original project. All application specific code should be inserted into the CC13xx/CC26xx SDK 6.10 project.

Some of these application-level modifications are due to various API changes. To aid in this, the guide provides an API translation table: GAP Changes.

Be sure to utilize the IDE and Tools recommended by the SDK’s release notes. For API Descriptions see BLE Stack API Reference.

  1. Choose a CC13xx/CC26xx SDK 6.10 example Bluetooth LE project and open it in the preferred supported IDE

    We’re going to use simple_peripheral as the starting CC13xx/CC26xx SDK 6.10 sample project to provide context.

  2. Modify the SysConfig file in the project folder. Use the SysConfig tool to transfer your project settings from the original project.

    This includes:

    • Any modification to the example project’s original predefined symbols

    • Any stack modification done through predefined symbols

    • Desired Radio settings

    • TI Drivers initializations/settings

    • Board file configuration

    For more information, see Get started with SysConfig and BLE5-Stack SysConfig Features.

  3. Transfer any additional app specific predefined symbols into the example project

  4. Transfer modified application files into the example project

    Modify main.c in the CC13xx/CC26xx SDK 6.10 example to create or rename any tasks that were added or modified in the original project.

    In this example, the following files from the original project were moved into the target simple_peripheral example:

    • two_btn_menu.c and two_btn_menu.h

    • simple_peripheral.c and simple_peripheral.h

    • simple_peripheral_menu.c and simple_peripheral_menu.h

    • simple_gatt_profile.c and simple_gatt_profile.h

  5. Adjust the Application for the GAP Role Removal

    Note

    GAPRole_createTask() should not be brought over to main.c. See GAP Role Removal for more information.

    All GAP Roles source and header files (peripheral.c, peripheral.h, central.c, central.h, etc.) have been removed in CC13xx/CC26xx SDK 6.10. These files will produce build errors and should not be included in your app. This change will introduce a structure change in the application.

    The functionality of the roles have been broken into distinct GAP functions: Scanner, Advertiser, and Initiator.

    These functions of GAP can be independently controlled to allow the device to function as a desired GAP Role such as peripheral or central. For additional information about using these roles, it is suggested to refer to the GAP Roles section of the User Guide. If you formerly used the BLE-Stack, this section provides information about the legacy features that exist in your current application.

    Utilize the GAP Changes table to port application GAP functionality. For example, in this table you’ll find information such as TGAP_LIM_DISC_ADV_INT_MIN is now replaced with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN, GAPROLE_ADVERT_ENABLED is now done with GapAdv_enable() or that GAPRole_StartDevice() is replaced by GAP_DeviceInit() to start the GAP module.

    It is suggested to look at an existing example in the SDK. simple_peripheral or simple_central may need to be used to assist in the porting process of the application. For example, the initialization of GAP Advertiser can be found in simple_peripheral.

    After using the GAP Changes table and using a relevant CC13xx/CC26xx SDK 6.10 example project as a guide, such as simple_peripheral, the structure and changes will become clearer.

    In the context of simple_peripheral and using the rest of the guide, the following table provides an example of changes to understand and implement when porting: Sample Simple Peripheral App Changes.

  6. Adjust the Application for the GAP Bond Manager Changes

    See GAP Bond Manager Changes for additional changes.

    • Include icall_ble_api.h if Stack/ICall APIs are used. Add the following #include AFTER all other includes for source files using Stack/ICall APIs.

      In this example, add:

      #include "icall_ble_api.h"
      

      into the following files AFTER all other includes. In for the simple_peripheral port, add this into these files:

      • simple_peripheral.c

      • simple_gatt_profile.c

      For more information regarding icall_ble_api.h see ICall Translation and Include.

      Warning

      All Stack/ICall APIs are listed in icall_ble_api.h. If any APIs are used without icall_ble_api.h, build and or link errors may occur with erratic runtime behaviors!

  7. Replace GAP Event processing

    In addition to the GAP Role changes, GAP events are being handled differently. This used to be received by GAP Role (ie. SimpleBLEPeripheral_processStateChangeEvt), which would then call GAPBondMgr, and then translate the event to GAPRole specific events and pass it to the application through a callback (ie. SimpleBLEPeripheral_gapRoleCBs).

    GAP events are now returned to the application directly as RTOS events. If the GAPBondMgr is present, they will first be received by the GAPBondMgr to do some processing but it will still be received the same in the application. This is now configured with GAP_DeviceInit. GAP events are received by the application (when the bond manager exists) as stack messages of type GAP_MSG_EVENT.

    See the example for simple_peripheral from CC13xx/CC26xx SDK 6.10 in the snippets below:

    Listing 239. Register to receive GAP events
    // Entity ID globally used to check for source and/or destination of messages
    static ICall_EntityID selfEntity;
    //...
    
    // Event globally used to post local events and pend on system and
    // local events.
    static ICall_SyncHandle syncEvent;
    //...
    
    // Address mode
    static GAP_Addr_Modes_t addrMode = DEFAULT_ADDRESS_MODE;
    //...
    
    static void SimplePeripheral_init(void)
    {
     BLE_LOG_INT_TIME(0, BLE_LOG_MODULE_APP, "APP : ---- init ", SP_TASK_PRIORITY);
     // Create the menu
     SimplePeripheral_buildMenu();
    
     // ******************************************************************
     // N0 STACK API CALLS CAN OCCUR BEFORE THIS CALL TO ICall_registerApp
     // ******************************************************************
     // Register the current thread as an ICall dispatcher application
     // so that the application can send and receive messages.
     ICall_registerApp(&selfEntity, &syncEvent);
    
     //...
     BLE_LOG_INT_TIME(0, BLE_LOG_MODULE_APP, "APP : ---- call GAP_DeviceInit", GAP_PROFILE_PERIPHERAL);
     //Initialize GAP layer for Peripheral role and register to receive GAP events
     GAP_DeviceInit(GAP_PROFILE_PERIPHERAL, selfEntity, addrMode, &pRandomAddress);
    }
    
    Listing 240. Receiving GAP Events
    static void SimplePeripheral_processGapMessage(gapEventHdr_t *pMsg); // function definition to handle GAP messages
    
    static uint8_t SimplePeripheral_processStackMsg(ICall_Hdr *pMsg)
    {
      // Always dealloc pMsg unless set otherwise
      uint8_t safeToDealloc = TRUE;
    
      switch (pMsg->event)
      {
        case GAP_MSG_EVENT:
          SimplePeripheral_processGapMessage((gapEventHdr_t*) pMsg);
          break;
        //...
      }
    }
    
    //...
    static void SimplePeripheral_processGapMessage(gapEventHdr_t *pMsg)
    {
        switch(pMsg->opcode)
        {
            case GAP_DEVICE_INIT_DONE_EVENT:
            {
            //... etc.
    
  8. Adjust the Application for the GATT Profile Changes

    Due to changes in LinkDB defines (linkdb.h), custom GATT profiles may need to be modified in order to account for the new definitions.

    Prepend LINKDB_ to all constants starting with CONNHANDLE_, for example in simple_gatt_profile.c:

    // Initialize Client Characteristic Configuration attributes
    GATTServApp_InitCharCfg( LINKDB_CONNHANDLE_INVALID, simpleProfileChar4Config );
    

    See GAP GATT Server Changes and Link Database Changes for additional changes as required.

  9. Note that additional return parameters have been added to HCI_EXT_ConnEventNoticeCmd():

    /**
     * Report describing connection event Returned via a @ref pfnGapConnEvtCB_t.
     */
    typedef struct
    {
      GAP_ConnEvtStat_t     status;   //!< status of connection event
      uint16_t              handle;   //!< connection handle
      uint8_t               channel;  //!< BLE RF channel index (0-39)
      GAP_ConnEvtPhy_t      phy;      //!< PHY of connection event
      int8_t                lastRssi; //!< RSSI of last packet received
      /// Number of packets received for this connection event
      uint16_t              packets;
      /// Total number of CRC errors for the entire connection
      uint16_t              errors;
      /// Type of next BLE task
      GAP_ConnEvtTaskType_t nextTaskType;
      /// Time to next BLE task (in us). 0xFFFFFFFF if there is no next task.
      uint32_t              nextTaskTime;
    } Gap_ConnEventRpt_t;
    
    /** @} End GAP_Structs */
    
  10. Note that additional parameter (signalIdentifier) has been added to GAP_UpdateLinkParamReq:

    /**
     * Establish Link Request parameters
     *
     * This is used by @ref GAP_UpdateLinkParamReq
     */
    typedef struct
    {
      uint16_t connectionHandle; //!< Connection handle of the update
      uint16_t intervalMin;      //!< Minimum Connection Interval
      uint16_t intervalMax;      //!< Maximum Connection Interval
      uint16_t connLatency;      //!< Connection Latency
      uint16_t connTimeout;      //!< Connection Timeout
      uint8_t  signalIdentifier; //!< L2CAP Signal Identifier. Must be 0 for LL Update
    } gapUpdateLinkParamReq_t;
    
  11. HCI_EXT_ConnEventNoticeCmd() has been replaced with Gap_RegisterConnEventCb().

API Translation Tables

These tables describe BLE5Stack API replacements for BLEStack API’s.

Table 51. GAP Changes

Previous Implementation

New/Current implementation

Type

Name

Description / API / Parameter

GAP EVENT

GAP_ADV_DATA_UPDATE_DONE_EVENT

Check return status of GapAdv_loadByHandle() or GapAdv_loadByBuffer()

GAP EVENT

GAP_DEVICE_DISCOVERY_EVENT

This depends on how the scanner is configured but one or more of the following events will be received:

GAP EVENT

GAP_DEVICE_INFO_EVENT

GAP_EVT_ADV_REPORT or GAP_EVT_ADV_REPORT_FULL

GAP EVENT

GAP_END_DISCOVERABLE_DONE_EVENT

Check return status of GapAdv_disable() to see that advertising is successfully being cancelled. The GAP_EVT_ADV_END_AFTER_DISABLE will be sent after the last advertisement ends.

GAP EVENT

GAP_MAKE_DISCOVERABLE_DONE_EVENT

Check return status of GapAdv_enable() to see that advertising is successfully being started. The GAP_EVT_ADV_START_AFTER_ENABLE will be sent after the first advertisement starts.

GAP EVENT

GAP_RANDOM_ADDR_CHANGED_EVENT

Obsolete - Address Resolution is done controller

GAP PARAM

TGAP_GEN_DISC_ADV_MIN

Configured by durationOrMaxEvents parameter of GapAdv_enable()

GAP PARAM

TGAP_LIM_ADV_TIMEOUT

Configured by durationOrMaxEvents parameter of GapAdv_enable()

GAP PARAM

TGAP_GEN_DISC_SCAN

Configured by parameters of GapScan_enable()

GAP PARAM

TGAP_LIM_DISC_SCAN

Configured by parameters of GapScan_enable()

GAP PARAM

TGAP_GEN_DISC_SCAN_INT

Configured by interval parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_GEN_DISC_SCAN_WIND

Configured by window parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_LIM_DISC_SCAN_INT

Configured by interval parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_LIM_DISC_SCAN_WIND

Configured by window parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_CONN_EST_ADV_TIMEOUT

Configured by durationOrMaxEvents parameter of GapAdv_enable()

GAP PARAM

TGAP_CONN_PARAM_TIMEOUT

GAP_SetParamValue() with GAP_PARAM_CONN_PARAM_TIMEOUT

GAP PARAM

TGAP_LIM_DISC_ADV_INT_MIN

GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN

GAP PARAM

TGAP_LIM_DISC_ADV_INT_MAX

GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX

GAP PARAM

TGAP_GEN_DISC_ADV_INT_MIN

GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN

GAP PARAM

TGAP_GEN_DISC_ADV_INT_MAX

GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX

GAP PARAM

TGAP_CONN_ADV_INT_MIN

GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN

GAP PARAM

TGAP_CONN_ADV_INT_MAX

GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX

GAP PARAM

TGAP_CONN_SCAN_INT

Configured by interval parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_CONN_SCAN_WIND

Configured by window parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_CONN_HIGH_SCAN_INT

Configured by interval parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_CONN_HIGH_SCAN_WIND

Configured by window parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_GEN_DISC_SCAN_INT

Configured by interval parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_GEN_DISC_SCAN_WIND

Configured by window parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_LIM_DISC_SCAN_INT

Configured by interval parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_LIM_DISC_SCAN_WIND

Configured by window parameter of GapScan_setPhyParams()

GAP PARAM

TGAP_CONN_EST_INT_MIN

GapInit_setPhyParam() with INIT_PHYPARAM_CONN_INT_MIN

GAP PARAM

TGAP_CONN_EST_INT_MAX

GapInit_setPhyParam() with INIT_PHYPARAM_CONN_INT_MAX

GAP PARAM

TGAP_CONN_EST_SCAN_INT

GapInit_setPhyParam() with INIT_PHYPARAM_SCAN_INTERVAL

GAP PARAM

TGAP_CONN_EST_SCAN_WIND

GapInit_setPhyParam() with INIT_PHYPARAM_SCAN_WINDOW

GAP PARAM

TGAP_CONN_EST_SUPERV_TIMEOUT

GapInit_setPhyParam() with INIT_PHYPARAM_SUP_TIMEOUT

GAP PARAM

TGAP_CONN_EST_LATENCY

GapInit_setPhyParam() with INIT_PHYPARAM_CONN_LATENCY

GAP PARAM

TGAP_CONN_EST_MIN_CE_LEN

Obsolete - Not Used by Controller

GAP PARAM

TGAP_CONN_EST_MAX_CE_LEN

Obsolete - Not Used by Controller

GAP PARAM

TGAP_PRIVATE_ADDR_INT

GAP_SetParamValue() with GAP_PARAM_PRIVATE_ADDR_INT

GAP PARAM

TGAP_CONN_PAUSE_CENTRAL

Obsolete - Not Used by Controller

GAP PARAM

TGAP_CONN_PAUSE_PERIPHERAL

GAP_UpdateLinkParamReq()

GAP PARAM

TGAP_SM_TIMEOUT

GAP_SetParamValue() with GAP_PARAM_SM_TIMEOUT

GAP PARAM

TGAP_SM_MIN_KEY_LEN

GAP_SetParamValue() with GAP_PARAM_SM_MIN_KEY_LEN

GAP PARAM

TGAP_SM_MAX_KEY_LEN

GAP_SetParamValue() with GAP_PARAM_SM_MAX_KEY_LEN

GAP PARAM

TGAP_FILTER_ADV_REPORTS

Obsolete - Duplicate Filtering done in Controller

GAP PARAM

TGAP_SCAN_RSP_RSSI_MIN

GapScan_setParam() with SCAN_PARAM_FLT_MIN_RSSI

GAP PARAM

TGAP_REJECT_CONN_PARAMS

GAP_SetParamValue() with GAP_PARAM_LINK_UPDATE_DECISION

GAP PARAM

TGAP_AUTH_TASK_ID

GAP_SetParamValue() with GAP_PARAM_AUTH_TASK_ID

GAP PARAM

TGAP_VERIFY_CAR

DEPRECATED

GAP PARAM

TGAP_GGS_PARAMS

GAP_SetParamValue() with GAP_PARAM_GGS_PARAMS

GAP PARAM

GAPROLE_IRK, GAPCENTRALROLE_IRK

GapConfig_SetParameter() with GAP_CONFIG_PARAM_IRK

GAP PARAM

GAPROLE_SRK, GAPCENTRALROLE_SRK

GapConfig_SetParameter() with GAP_CONFIG_PARAM_SRK

GAP PARAM

GAPROLE_BD_ADDR, GAPCENTRALROLE_BD_ADDR

HCI_ReadBDADDRCmd()

GAP PARAM

GAPROLE_ADVERT_ENABLED, GAPROLE_ADV_NONCONN_ENABLED

GapAdv_enable() and GapAdv_disable()

GAP PARAM

GAPROLE_ADVERT_OFF_TIME

Configured by durationOrMaxEvents parameter of GapAdv_enable()

GAP PARAM

GAPROLE_ADVERT_DATA

Various API:

GAP PARAM

GAPROLE_SCAN_RSP_DATA

Various API:

GAP PARAM

GAPROLE_ADV_EVENT_TYPE

GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_PROPS

GAP PARAM

GAPROLE_ADV_DIRECT_TYPE

GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_PEER_ADDRESS_TYPE

GAP PARAM

GAPROLE_ADV_DIRECT_ADDR

GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_PEER_ADDRESS

GAP PARAM

GAPROLE_ADV_CHANNEL_MAP

GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP

GAP PARAM

GAPROLE_ADV_FILTER_POLICY

GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_FILTER_POLICY

GAP PARAM

GAPROLE_CONNHANDLE

Returned for each GAP event

GAP PARAM

GAPROLE_RSSI_READ_RATE

RSSI can be received by HCI_ReadRssiCmd()

GAP PARAM

GAPROLE_PARAM_UPDATE_ENABLE

GAP_UpdateLinkParamReq() can be called as desired

GAP PARAM

GAPROLE_MIN_CONN_INTERVAL

pParams.intervalMin parameter of GAP_UpdateLinkParamReq()

GAP PARAM

GAPROLE_MAX_CONN_INTERVAL

pParams.intervalMax parameter of GAP_UpdateLinkParamReq()

GAP PARAM

GAPROLE_SLAVE_LATENCY

pParams.connLatency parameter of GAP_UpdateLinkParamReq()

GAP PARAM

GAPROLE_TIMEOUT_MULTIPLIER

pParams.connTimeout parameter of GAP_UpdateLinkParamReq()

GAP PARAM

GAPROLE_STATE

Obsolete - GAP changes remove the need for this

GAP PARAM

GAPROLE_CONN_BD_ADDR, GAPROLE_BD_ADDR_TYPE

Returned in GAP_LINK_ESTABLISHED_EVENT, contained in stack message, gapEstLinkReqEvent_t when the link is established

Or use linkDB_GetInfo() at any time during the connection

GAP PARAM

GAPROLE_CONN_INTERVAL

Returned from linkDB_GetInfo(), as linkDBInfo_t.connInterval

GAP PARAM

GAPROLE_CONN_LATENCY

Returned from linkDB_GetInfo(), as linkDBInfo_t.connLatency

GAP PARAM

GAPROLE_CONN_TIMEOUT

Returned from linkDB_GetInfo(), as linkDBInfo_t.connTimeout

GAP PARAM

GAPCENTRALROLE_MAX_SCAN_RES

Configured by maxNumReport parameter of GapScan_enable()

GAP PARAM

GAPCENTRALROLE_LINK_PARAM_UPDATE_REQ_REPLY

GAP_SetParamValue() with GAP_PARAM_LINK_UPDATE_DECISION

GAP API

GAP_DeviceInit, GAPRole_StartDevice, GAPCentralRole_StartDevice

Declaration Change - Use GAP_DeviceInit() with parameter for roles desired

GAP API

GAPRole_RegisterAppCBs

Obsolete - Functionality moved to GAPBondMgr_Register()

GAP API

GAP_SetAdvToken

Obsolete - Advertisement Sets are Used

GAP API

GAP_GetAdvToken

Obsolete - Advertisement Sets are Used

GAP API

GAP_RemoveAdvToken

Obsolete - Advertisement Sets are Used

GAP API

GAP_UpdateAdvTokens

Obsolete - Advertisement Sets are Used

GAP API

GAPRole_SendUpdateParam, GAPCentralRole_UpdateLink

GAP_UpdateLinkParamReq()

GAP API

GAP_MakeDiscoverable

GapAdv_enable()

GAP API

GAP_UpdateAdvertisingData

Various API:

GAP API

GAP_EndDiscoverable

GapAdv_disable()

GAP API

GAP_DeviceDiscoveryRequest, GAPCentralRole_StartDiscovery

GapScan_enable()

GAP API

GAP_DeviceDiscoveryCancel, GAPCentralRole_CancelDiscovery

GapScan_disable()

GAP API

GAP_ResolvePrivateAddr

Obsolete - Address Resolution is done controller

GAP API

GAP_EstablishLinkReq, GAPCentralRole_EstablishLink

GapInit_connect(), or GapInit_connectWl() to use Filter Accept List

GAP API

GAP_TerminateLinkReq, GAPRole_TerminateConnection, GAPCentralRole_TerminateLink

GapInit_cancelConnect() for connection request, GAP_TerminateLinkReq() otherwise

GAP API

GAP_ConfigDeviceAddr

Obsolete - Only way to configure the device address is as parameters in GAP_DeviceInit()

GAP CB

gapRolesParamUpdateCB_t, paramUpdateAppDecision_t, passThroughToApp_t

These are handled through GAP_UPDATE_LINK_PARAM_REQ_EVENT, applies to the L2CAP Parameter Update Procedure as well.

GAP CB

gapRolesStateNotify_t, pfnGapCentralRoleEventCB_t

Moved into GAP Bond Manager callbacks, gapBondCBs_t

Table 52. GAP Bond Manager Changes

Previous Implementation

New/Current implementation

Type

Name

Description / API / Parameter

GAPBOND PARAM

GAPBOND_DEFAULT_PASSCODE

Use pfnPasscodeCB_t, shared default passcode defined in bcomdef.h B_APP_DEFAULT_PASSCODE

GAPBOND PARAM

GAPBOND_REMOTE_OOB_SC_ENABLED

Obsolete

GAPBOND PARAM

GAPBOND_REMOTE_OOB_SC_DATA

Obsolete

GAPBOND PARAM

GAPBOND_LOCAL_OOB_SC_ENABLED

Obsolete

GAPBOND PARAM

GAPBOND_LOCAL_OOB_SC_DATA

Obsolete

GAPBOND STATE

GAPBOND_PAIRING_STATE_BONDED

GAPBOND_PAIRING_STATE_ENCRYPTED

GAPBOND DEF

GBM_QUEUE_PAIRINGS

Removed, is now default behavior

GAPBOND DEF

GBM_GATT_NO_CLIENT

Configured by GATT_NO_CLIENT

GAPBOND DEF

SNP_SECURITY

Configured by GAPBONDMGR_NO_SIGNING

GAPBOND API

GAPBondMgr_LinkEst

Removed Application Access to API Handled Internally

GAPBOND API

GAPBondMgr_LinkTerm

Removed Application Access to API Handled Internally

GAPBOND API

GAPBondMgr_SlaveReqSecurity

GAPBondMgr_Pair(), allowing both Centrals and Peripherals to request pairing

GAPBOND API

GAPBondMgr_UpdateCharCfg

Removed Application Access to API Handled Internally

GAPBOND API

GAPBondMgr_ReadGattChar

Removed Application Access to API Handled Internally

GAPBOND API

GAPBondMgr_SupportsEnhancedPriv

Removed Application Access to API Handled Internally

GAPBOND API

GAPBondMgr_CheckNVLen

Removed Application Access to API Handled Internally

GAPBOND API

GAPBondMgr_syncResolvingList

Removed Application Access to API Handled Internally

Table 53. GAP GATT Server Changes

Previous Implementation

New/Current implementation

Type

Name

Description / API / Parameter

GGS PARAM

GGS_PERI_PRIVACY_FLAG_ATT

Obsolete

GGS PARAM

GGS_RECONNCT_ADDR_ATT

Obsolete

GGS PARAM

GGS_PERI_PRIVACY_FLAG_PROPS

Obsolete

GGS PARAM

GGS_W_PERMIT_PRIVACY_FLAG_ATT

Obsolete

GGS PARAM

GGS_TESTMODE_W_PERMIT_PRIVACY_FLAG

Obsolete

Table 54. Link Database Changes

Previous Implementation

New/Current implementation

Type

Name

Description / API / Parameter

LinkDB API

linkDB_Remove

API now accepts linkDBInfo_t in addition to connection handle

Table 55. Sample Simple Peripheral App Changes

Previous Implementation

BLE5-Stack 1.02.00 Implementation

SimpleBLEPeripheral_processStateChangeEvt

See SimplePeripheral_processGapMessage

SimpleBLEPeripheral_processAppMsg

Different events are now being handled. See SimplePeripheral_processAppMsg

SimpleBLEPeripheral_processStackMsg

See the guide’s step to Replace GAP Event processing

This is modified to process GAP_MSG_EVENT

SimpleBLEPeripheral_stateChangeCB gapRolesCBs_t SimpleBLEPeripheral_gapRoleCBs

See the guide’s step to Replace GAP Event processing

This is no longer used. GAP events are now returned to the application directly as the RTOS event, GAP_MSG_EVENT

GAP_SetParamValue(TGAP_CONN_PAUSE_PERIPHERAL, DEFAULT_CONN_PAUSE_PERIPHERAL)

GAP_UpdateLinkParamReq()

GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),&initialAdvertEnable)

In SimplePeripheral_processGapMessage by GapAdv_enable()

GAPRole_SetParameter(GAPROLE_ADVERT_OFF_TIME, sizeof(uint16_t),&advertOffTime)

In SimplePeripheral_processGapMessage by GapAdv_enable(). Configured by the third parameter durationOrMaxEvents

GAPRole_SetParameter(GAPROLE_SCAN_RSP_DATA, sizeof(scanRspData),scanRspData)

In SimplePeripheral_processGapMessage by GapAdv_loadByHandle(). with GAP_ADV_DATA_TYPE_SCAN_RSP set as the data type

GAPRole_SetParameter(GAPROLE_ADVERT_DATA, sizeof(advertData), advertData)

In SimplePeripheral_processGapMessage by GapAdv_loadByHandle() with GAP_ADV_DATA_TYPE_ADV set as the data type

GAPRole_SetParameter(GAPROLE_PARAM_UPDATE_ENABLE, sizeof(uint8_t), &enableUpdateRequest)

In SimplePeripheral_processGapMessage, parameter updates from a central device are handled in GAP_UPDATE_LINK_PARAM_REQ_EVENT and uses GAP_UpdateLinkParamReqReply()

GAPRole_SetParameter(GAPROLE_MIN_CONN_INTERVAL, sizeof(uint16_t), &desiredMinInterval)

In SimplePeripheral_processParamUpdate, set as DEFAULT_DESIRED_MIN_CONN_INTERVAL and applied with GAP_UpdateLinkParamReq()

GAPRole_SetParameter(GAPROLE_MAX_CONN_INTERVAL, sizeof(uint16_t), &desiredMaxInterval)

In SimplePeripheral_processParamUpdate, set as DEFAULT_DESIRED_MAX_CONN_INTERVAL and applied with GAP_UpdateLinkParamReq()

GAPRole_SetParameter(GAPROLE_SLAVE_LATENCY, sizeof(uint16_t), &desiredSlaveLatency)

In SimplePeripheral_processParamUpdate, set as DEFAULT_DESIRED_SLAVE_LATENCY and applied with GAP_UpdateLinkParamReq()

GAPRole_SetParameter(GAPROLE_TIMEOUT_MULTIPLIER, sizeof(uint16_t), &desiredConnTimeout)

In SimplePeripheral_processParamUpdate, set as DEFAULT_DESIRED_CONN_TIMEOUT and applied with GAP_UpdateLinkParamReq()

GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MIN, advInt) GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MIN, advInt)

GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN

GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MAX, advInt) GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MAX, advInt)

GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX

GAPBondMgr_SetParameter(GAPBOND_DEFAULT_PASSCODE, sizeof(uint32_t), &passkey)

Use pfnPasscodeCB_t, shared default passcode defined in bcomdef.h B_APP_DEFAULT_PASSCODE

GAPROLE_STATE

Obsolete - GAP changes remove the need for this

GAPROLE_CONNHANDLE

Returned for each GAP event