MCUboot Over-the-Air Download (OAD)

The following sections aim to describe the lower layers of OAD software that are common across all protocol stack implementations. This includes the OAD image header, the flash layout, Secure Bootloader, and the oad image tool.

Warning

The BLE-Stack OAD Profile does not implement or perform any security or authentication mechanisms as part of the firmware update process. System developers should take measures to adequately authenticate peer devices and only accept and/or apply firmware images transferred from trusted sources via the OAD Profile. TI recommends applications use Bluetooth LE Secure Connections (LESC) with Man-in-the-Middle (MITM) protection with peer devices when performing wireless firmware updates, although the use of the LESC feature does not itself guarantee image authenticity.

When using the Secure OAD feature along with recommended parameters, firmware images are authenticated on the device using ECDSA signature validation algorithms to ensure image authenticity prior to updating the running firmware image. Just as with the OAD Profile, TI recommends applications use Bluetooth LE Secure Connections with Man-in-the-Middle (MITM) protection with peer devices when performing wireless firmware updates.

The following sections aim to describe the BLE5-Stack specific application and profile layer of the OAD solution. The OAD application section will describe the BLE OAD process from a high level in terms of events and states, and the profile section will cover the actual structures that are sent over the air.

The SimpleLink Academy OAD Fundamentals Module covers the out of the box demo for OAD using the BLE5-Stack. It can be found here. This lab contains the following step by step instructions:

  • Anatomy of an OAD

    • Image Header

    • Boot Image Manager (BIM)

    • OAD Memory Layout

    • OAD Protocol/BLE Profile

  • Setting up the OAD Environment

    • OAD Distributor Setup

    • OAD Target Setup

    • Creating a Factory Image

  • Running the OAD Demo

    • Modifying the Image Version

    • OAD using BTool

    • Btool Image Header Dialog

  • Reverting to a Factory Image

The SimpleLink Academy OAD Advanced Module covers these advanced topics and instructions:

  • Adding OAD to an Existing Project

    • Project Changes

    • Code Changes

  • Advanced OAD Debugging

  • Creating a Production Image

    • Change to Release BIM

    • Secure OAD: Change default keys

    • Loading a Production Image

    • Combined Production Image

Mobile developers wishing to make applications that integrate the TI OAD should refer to the following sample implementations. These are intended as reference libraries that implement the TI OAD Downloader for Android and iOS.

Note

The above libraries do not implement full fledged applications, but instead are intended to be integrated as part of an end application.