![]() |
![]() |
TI BLE5-Stack API Documentation
2.02.09.00
|
Information pertaining to the linklinkDB info. More...
Data Fields | |
uint8 | addr [B_ADDR_LEN] |
Other Device's address. | |
uint8 | addrPriv [B_ADDR_LEN] |
Other Device's Private address. | |
uint8 | addrType |
Address type of connected device. | |
uint16 | connInterval |
The connection's interval (n * 1.23 ms) | |
uint16 | connLatency |
current connection latency | |
uint8 | connRole |
Connection formed as Master or Slave. | |
uint16 | connTimeout |
current connection timeout | |
uint16 | MTU |
The connection's MTU size. | |
uint8 | stateFlags |
LinkDB Connection State Flags | |
Information pertaining to the linklinkDB info.