MCUBoot Over-the-Air Download (OAD)¶
The following sections aim to describe the lower layers of OAD software that are common across all protocol stack implementations. This includes the OAD image header, the flash layout, Secure Bootloader, and the oad image tool.
Warning
The TI Wi-SUN FAN Stack OAD Profile does not implement or perform any security or authentication mechanisms as part of the firmware update process. System developers should take measures to adequately authenticate peer devices and only accept and/or apply firmware images transferred from trusted sources via the OAD Profile.
Attention
Due to memory constraints, the TI Wi-SUN FAN Stack does not support on-chip OAD on CC13x2 or CC13x2x7 devices.
The following sections aim to describe the TI Wi-SUN FAN Stack specific application and profile layer of the OAD solution. The OAD application section will describe the TI Wi-SUN FAN Stack process from a high level in terms of events and states, and the profile section will cover the actual structures that are sent over the air.