Post-Build Script imgtool¶
The compiler output requires a post-build step to generate a .bin file that can
be used by MCUboot. An MCUboot compatible image tool must be executed called
imgtool
. It is responsible for adding the MCUBoot image header, managing
keys and sign the image. More detailed description is provided on the
imgtool documentation page.
This tool requires Python3 and is included in the SimpleLink SDK in the folder
<simplelink-install-dir>\source\third_party\mcuboot\scripts
.
The script can be executed automatically after every build by adding below lines
as Post-Build steps
in Properties > Build
as shown below. This command
defines the image version. To update the version number, adjust the string
--version 1.0.0
.
1${CG_TOOL_ROOT}/bin/tiarmobjcopy ${ProjName}.out --output-target ihex ${ProjName}.hex
2${CG_TOOL_ROOT}/bin/tiarmobjcopy ${ProjName}.out --output-target binary ${ProjName}-noheader.bin
3${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/tools/common/mcuboot/imgtool sign --header-size 0x80 --align 4 --slot-size 0x56000 --pad --version 1.0.0 --pad-header --key ${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/source/third_party/mcuboot/root-ec-p256.pem ${ProjName}-noheader.bin ${ProjName}.bin
Figure 59. Post-Build steps included in CCS properties¶