rflib
Data Fields
rfc_CMD_HID_TX_s Struct Reference

HID Transmit Command with Auto Retransmission. More...

#include <rf_hid_cmd.h>

Collaboration diagram for rfc_CMD_HID_TX_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x5801. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   bAutoRetransmit:1
 0: Do not listen for ACK
1: Listen for ACK and retransmit if missing More...
 
   uint8_t   bVarLen:1
 0: Fixed length mode
1: Variable length mode More...
 
   uint8_t   hdrMode:1
 0: 9-bit header
1: 10-bit header More...
 
   uint8_t   bIncludeAddr:1
 0: Do not include address byte after sync word
1: Include address byte after sync word More...
 
   uint8_t   hdrConf:2
 0: Automatically generate header (no header byte in buffer)
1: Insert NO_ACK field from TX buffer
2: Insert SEQ field from TX buffer
3: Insert SEQ and NO_ACK field from TX buffer More...
 
   uint8_t   bFixedTxLen:1
 0: Use actual length in header when sending packet
1: Use fixed word in length field of header when sending packet (only for peer without variable length packets) More...
 
pktConf
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically remove ignored packets (RX) or empty ACKs (TX) from RX queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically remove packets with CRC error from Rx queue. More...
 
   uint8_t   bIncludeAddr:1
 If 1, the received address byte is included in the Rx queue. More...
 
   uint8_t   bIncludeHdr:1
 If 1, the received header is included in the Rx queue. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
rxConf
 Receive entry configuration. More...
 
uint32_t syncWord
 Sync word to send. More...
 
uint8_t address
 Address byte. More...
 
uint8_t seqNo
 Sequence number to use for next packet. More...
 
uint8_t maxAckLen
 Maximum length of ACKs. More...
 
uint8_t pktLen
 Length of transmitted packet. More...
 
uint8_t maxRetrans
 Maximum number of retransmissions. More...
 
struct {
   uint8_t   noAckVal:2
 0: Set automatic NO_ACK value to inverse of bAutoRetransmit
1: Set automatic NO_ACK value to bAutoRetransmit
2: Set automatic NO_ACK value to 0
3: Set automatic NO_ACK value to 1 More...
 
   uint8_t   bAlwaysAutoRetransmit:1
 0: Disable auto retransmit if transmitted NO_ACK was 1
1: Never disable auto retransmit More...
 
noAckMode
 
uint16_t retransDelay
 Number of RAT ticks from start of transmission of a packet to retransmission. More...
 
uint8_t * pPkt
 Pointer to transmit queue for packets. More...
 
dataQueue_tpRxQueue
 Pointer to receive queue for ACKs. More...
 
rfc_hidRxTxOutput_tpOutput
 Pointer to output structure. More...
 

Detailed Description

HID Transmit Command with Auto Retransmission.

Field Documentation

§ commandNo

uint16_t rfc_CMD_HID_TX_s::commandNo

The command ID number 0x5801.

§ status

uint16_t rfc_CMD_HID_TX_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t* rfc_CMD_HID_TX_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_HID_TX_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_HID_TX_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_HID_TX_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_HID_TX_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_HID_TX_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger

struct { ... } rfc_CMD_HID_TX_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_HID_TX_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_HID_TX_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition

struct { ... } rfc_CMD_HID_TX_s::condition

§ bFsOff

uint8_t rfc_CMD_HID_TX_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

§ bAutoRetransmit

uint8_t rfc_CMD_HID_TX_s::bAutoRetransmit

0: Do not listen for ACK
1: Listen for ACK and retransmit if missing

§ bVarLen

uint8_t rfc_CMD_HID_TX_s::bVarLen

0: Fixed length mode
1: Variable length mode

§ hdrMode

uint8_t rfc_CMD_HID_TX_s::hdrMode

0: 9-bit header
1: 10-bit header

§ bIncludeAddr

uint8_t rfc_CMD_HID_TX_s::bIncludeAddr

0: Do not include address byte after sync word
1: Include address byte after sync word

If 1, the received address byte is included in the Rx queue.

§ hdrConf

uint8_t rfc_CMD_HID_TX_s::hdrConf

0: Automatically generate header (no header byte in buffer)
1: Insert NO_ACK field from TX buffer
2: Insert SEQ field from TX buffer
3: Insert SEQ and NO_ACK field from TX buffer

§ bFixedTxLen

uint8_t rfc_CMD_HID_TX_s::bFixedTxLen

0: Use actual length in header when sending packet
1: Use fixed word in length field of header when sending packet (only for peer without variable length packets)

§ pktConf

struct { ... } rfc_CMD_HID_TX_s::pktConf

§ bAutoFlushIgnored

uint8_t rfc_CMD_HID_TX_s::bAutoFlushIgnored

If 1, automatically remove ignored packets (RX) or empty ACKs (TX) from RX queue.

§ bAutoFlushCrcErr

uint8_t rfc_CMD_HID_TX_s::bAutoFlushCrcErr

If 1, automatically remove packets with CRC error from Rx queue.

§ bIncludeHdr

uint8_t rfc_CMD_HID_TX_s::bIncludeHdr

If 1, the received header is included in the Rx queue.

§ bIncludeCrc

uint8_t rfc_CMD_HID_TX_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

§ bAppendRssi

uint8_t rfc_CMD_HID_TX_s::bAppendRssi

If 1, append an RSSI byte to the packet in the Rx queue.

§ bAppendStatus

uint8_t rfc_CMD_HID_TX_s::bAppendStatus

If 1, append a status byte to the packet in the Rx queue.

§ bAppendTimestamp

uint8_t rfc_CMD_HID_TX_s::bAppendTimestamp

If 1, append a timestamp to the packet in the Rx queue.

§ rxConf

struct { ... } rfc_CMD_HID_TX_s::rxConf

Receive entry configuration.

§ syncWord

uint32_t rfc_CMD_HID_TX_s::syncWord

Sync word to send.

§ address

uint8_t rfc_CMD_HID_TX_s::address

Address byte.

§ seqNo

uint8_t rfc_CMD_HID_TX_s::seqNo

Sequence number to use for next packet.

§ maxAckLen

uint8_t rfc_CMD_HID_TX_s::maxAckLen

Maximum length of ACKs.

§ pktLen

uint8_t rfc_CMD_HID_TX_s::pktLen

Length of transmitted packet.

§ maxRetrans

uint8_t rfc_CMD_HID_TX_s::maxRetrans

Maximum number of retransmissions.

§ noAckVal

uint8_t rfc_CMD_HID_TX_s::noAckVal

0: Set automatic NO_ACK value to inverse of bAutoRetransmit
1: Set automatic NO_ACK value to bAutoRetransmit
2: Set automatic NO_ACK value to 0
3: Set automatic NO_ACK value to 1

§ bAlwaysAutoRetransmit

uint8_t rfc_CMD_HID_TX_s::bAlwaysAutoRetransmit

0: Disable auto retransmit if transmitted NO_ACK was 1
1: Never disable auto retransmit

§ noAckMode

struct { ... } rfc_CMD_HID_TX_s::noAckMode

§ retransDelay

uint16_t rfc_CMD_HID_TX_s::retransDelay

Number of RAT ticks from start of transmission of a packet to retransmission.

§ pPkt

uint8_t* rfc_CMD_HID_TX_s::pPkt

Pointer to transmit queue for packets.

§ pRxQueue

dataQueue_t* rfc_CMD_HID_TX_s::pRxQueue

Pointer to receive queue for ACKs.

§ pOutput

rfc_hidRxTxOutput_t* rfc_CMD_HID_TX_s::pOutput

Pointer to output structure.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale