rflib
Data Fields
rfc_CMD_HID_RX_s Struct Reference

HID Recieve Command with Auto Ack. More...

#include <rf_hid_cmd.h>

Collaboration diagram for rfc_CMD_HID_RX_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x5802. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   bRepeatOk:1
 0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly More...
 
   uint8_t   bRepeatNok:1
 0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error More...
 
   uint8_t   hdrMode:1
 0: 9-bit header
1: 10-bit header More...
 
   uint8_t   bIncludeAddr:1
 0: Include address byte after sync word
1: Do not include address byte after sync word More...
 
   uint8_t   hdrConf:2
 0: Automatically generate header (no header byte in buffer) 1: Insert NO_ACK field from TX buffer 2: Insert SEQ field from TX buffer 3: Insert SEQ and NO_ACK field from TX buffer More...
 
pktConf
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically remove ignored packets (RX) or empty ACKs (TX) from RX queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically remove packets with CRC error from Rx queue. More...
 
   uint8_t   bIncludeAddr:1
 If 1, the received address byte is included in the Rx queue. More...
 
   uint8_t   bIncludeHdr:1
 If 1, the received header is included in the Rx queue. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
rxConf
 Receive entry configuration. More...
 
uint32_t syncWord0
 Sync word to listen for. More...
 
uint32_t syncWord1
 Alternative sync word if non-zero. More...
 
uint8_t numAddr
 Number of address entries. More...
 
uint8_t __dummy0
 
uint8_t __dummy1
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
endTrigger
 Trigger classifier for ending the operation. More...
 
ratmr_t endTime
 Time used together with endTrigger for ending the operation. More...
 
rfc_hidAddrEntry_tpAddrEntry
 Pointer to array of address entries. More...
 
dataQueue_tpRxQueue
 Pointer to receive queue. More...
 
rfc_hidRxTxOutput_tpOutput
 Pointer to output structure. More...
 

Detailed Description

HID Recieve Command with Auto Ack.

Field Documentation

§ commandNo

uint16_t rfc_CMD_HID_RX_s::commandNo

The command ID number 0x5802.

§ status

uint16_t rfc_CMD_HID_RX_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t* rfc_CMD_HID_RX_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_HID_RX_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_HID_RX_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_HID_RX_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_HID_RX_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_HID_RX_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger

struct { ... } rfc_CMD_HID_RX_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_HID_RX_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_HID_RX_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition

struct { ... } rfc_CMD_HID_RX_s::condition

§ bFsOff

uint8_t rfc_CMD_HID_RX_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

§ bRepeatOk

uint8_t rfc_CMD_HID_RX_s::bRepeatOk

0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly

§ bRepeatNok

uint8_t rfc_CMD_HID_RX_s::bRepeatNok

0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error

§ hdrMode

uint8_t rfc_CMD_HID_RX_s::hdrMode

0: 9-bit header
1: 10-bit header

§ bIncludeAddr

uint8_t rfc_CMD_HID_RX_s::bIncludeAddr

0: Include address byte after sync word
1: Do not include address byte after sync word

If 1, the received address byte is included in the Rx queue.

§ hdrConf

uint8_t rfc_CMD_HID_RX_s::hdrConf

0: Automatically generate header (no header byte in buffer) 1: Insert NO_ACK field from TX buffer 2: Insert SEQ field from TX buffer 3: Insert SEQ and NO_ACK field from TX buffer

§ pktConf

struct { ... } rfc_CMD_HID_RX_s::pktConf

§ bAutoFlushIgnored

uint8_t rfc_CMD_HID_RX_s::bAutoFlushIgnored

If 1, automatically remove ignored packets (RX) or empty ACKs (TX) from RX queue.

§ bAutoFlushCrcErr

uint8_t rfc_CMD_HID_RX_s::bAutoFlushCrcErr

If 1, automatically remove packets with CRC error from Rx queue.

§ bIncludeHdr

uint8_t rfc_CMD_HID_RX_s::bIncludeHdr

If 1, the received header is included in the Rx queue.

§ bIncludeCrc

uint8_t rfc_CMD_HID_RX_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

§ bAppendRssi

uint8_t rfc_CMD_HID_RX_s::bAppendRssi

If 1, append an RSSI byte to the packet in the Rx queue.

§ bAppendStatus

uint8_t rfc_CMD_HID_RX_s::bAppendStatus

If 1, append a status byte to the packet in the Rx queue.

§ bAppendTimestamp

uint8_t rfc_CMD_HID_RX_s::bAppendTimestamp

If 1, append a timestamp to the packet in the Rx queue.

§ rxConf

struct { ... } rfc_CMD_HID_RX_s::rxConf

Receive entry configuration.

§ syncWord0

uint32_t rfc_CMD_HID_RX_s::syncWord0

Sync word to listen for.

§ syncWord1

uint32_t rfc_CMD_HID_RX_s::syncWord1

Alternative sync word if non-zero.

§ numAddr

uint8_t rfc_CMD_HID_RX_s::numAddr

Number of address entries.

§ __dummy0

uint8_t rfc_CMD_HID_RX_s::__dummy0

§ __dummy1

uint8_t rfc_CMD_HID_RX_s::__dummy1

§ endTrigger

struct { ... } rfc_CMD_HID_RX_s::endTrigger

Trigger classifier for ending the operation.

§ endTime

ratmr_t rfc_CMD_HID_RX_s::endTime

Time used together with endTrigger for ending the operation.

§ pAddrEntry

rfc_hidAddrEntry_t* rfc_CMD_HID_RX_s::pAddrEntry

Pointer to array of address entries.

§ pRxQueue

dataQueue_t* rfc_CMD_HID_RX_s::pRxQueue

Pointer to receive queue.

§ pOutput

rfc_hidRxTxOutput_t* rfc_CMD_HID_RX_s::pOutput

Pointer to output structure.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale