DisplayUart2 Attributes. More...
#include <DisplayUart2.h>
Data Fields | |
unsigned int | uartIdx |
unsigned int | baudRate |
unsigned int | mutexTimeout |
char * | strBuf |
uint16_t | strBufLen |
DisplayUart2 Attributes.
The DisplayUart2 driver uses a buffer for formatting messages, which is then passed to UART2_write(). The location and size of the buffer are specified in a DisplayUart2_HWAttrs structure. Access to the buffer is synchronized by a semaphore. The timeout for acquiring the semaphore is specified in the attributes.
unsigned int DisplayUart2_HWAttrs::uartIdx |
Index of uart in UART_config[]
unsigned int DisplayUart2_HWAttrs::baudRate |
Baud rate for uart
unsigned int DisplayUart2_HWAttrs::mutexTimeout |
Timeout for acquiring semaphore
char* DisplayUart2_HWAttrs::strBuf |
Buffer for formatting messages
uint16_t DisplayUart2_HWAttrs::strBufLen |
Size of buffer