Example Applications

This section provides an overview of the TI-OpenThread out-of-box example applications and instructions on how to run them.

Note

All TI-OpenThread example applications are supported for the following three boards: CC26X2R1_LAUNCHXL, CC1352R1_LAUNCHXL and CC1352P2_LAUNCHXL. By default the READMEs below will link to the CC26X2R1_LAUNCHXL board. If a different board is intended to be used, just replace the board name in the path to find the corresponding README document.

Project Configurations

Some example applications supports both an FTD and an MTD device configuration, and therefore two types of project configurations exist for such example applications: one with the <name>_ftd_* naming convention for the FTD configuration, and one with the <name>_mtd_* naming convention for the MTD naming convention. For example, the CLI example has both a cli_ftd_* and a cli_mtd_* project configuration for a FTD and MTD configuration, respectively.

All example applications support the GCC, IAR, and TI-CLANG toolchains, and therefore three project configurations exist for each example application: one with the *_gcc suffix which uses GCC, one with the *_iar suffix which uses IAR, and one with the *_ticlang suffix which uses TI-CLANG. For the respective IDE to use for each toolchain, see IDEs and Toolchains.

Both Thread device configuration and toolchain selection is configured separately, and therefore multiple projects are available for some example projects as a combination of said configurations.

Factory Reset

Some of the example applications contain convenience functionality to reset the non-volatile storage on the internal flash, as well as a reset to some stored factory image. Refer to each respective section for instructions on how to perform each kind of factory reset.

Reset of Non-Volatile Storage

Non-volatile storage (NVS) in the internal flash stores information about the Thread network which allows Thread devices to restart network operations after a reset without user intervention. However, in order for a Thread device to forget a Thread network it has been commissioned to, the NVS must be erased.

For the end-product examples, a convenience functionality has been added in order to easily erase NVS and quickly start fresh. Given that the running application supports this functionality, do the following steps to reset NVS:

  1. Hold down the right button (BTN-2) on the CC13xx or CC26xx LaunchPad.

  2. While holding down the right button, press the reset button.

  3. At startup the application will check the pin state and jump to the invalidate-NVS routine.

Warning

Reset of NVS does not erase the actual application image on the internal flash.

Revert to Factory Image

OAD-enabled examples can revert back to a factory image, if a factory image is present on the external flash. Given that a factory image is stored, do the following steps to reset to the factory image:

Given that the running application supports this functionality, do the following steps to reset to factory image:

  1. Hold down the left button (BTN-1) on the CC13xx or CC26xx LaunchPad.

  2. While holding down the left button, press the reset button.

  3. At startup the application will check the pin state and jump to the reset-to-factory-image routine.

Warning

Reverting to the factory image does not erase NVS in the internal flash.

The application should check that a valid factory image is present before reverting. This can be done by ensuring there is valid metadata in external flash page 0. See OAD External Flash Image Header for more information.

Common User Interface

The common user interface (CUI) is a module on application examples. Serial communication is utilized for the user to configure certain parameters, and to display various device information. The Thread application examples which use CUI implement the functionality in both its respective application file and tiop_ui.c.

The CUI consists of a series of circular menus that are navigated with the arrow keys. To enter a submenu, press the Enter key. Adjustable values on submenus (e.g. PAN ID, channel) may be changed using the keyboard (e.g. arrow keys, letters, numbers) and pressing Enter afterwards.

Note

When editing a value, the Esc key may be used to exit edit mode. While on a submenu, the Esc key may be used to return to the main menu.

The CUI is also dependent on the capabilities of the compiled device. For example, a Full Thread Device may form a network while a Minimal Thread Device must join a network.

It is recommended to use PuTTY as the serial terminal program for these sample applications because the serial output has been verified to be formatted correctly in this program. For serial port setup, select 115200 for baud rate and disable flow control.

Below is an overview of the menus common across all CUI-enabled examples.

../_images/cui-overview.png

Figure 22. CUI Overview

Help Screen

The initial screen displays the application name and leads to the Help Screen, which outlines the generic functionality of the keys throughout the application. The following sections describe the specific functionality of the keys for each menu screen.

../_images/Initial-screen.png

Figure 23. Initial screen

../_images/Help-screen.png

Figure 24. Help screen

Welcome and Help Screens

Key

Function

Comment

Left/Right Arrow Keys

Menu navigation

Move to previous/next screen

Enter

Help

Press Enter to show the help screen. Press Enter again to go back to the Welcome Screen.

Information Screen

The lower portion of the screen displays various information about the device such as the 64-bit unique identifier, network name, and PAN ID.

../_images/Info-screen.png

Figure 25. Info screen example

Device Info

The Device Info line shows information about the device.

  • EUI64: Extended Unique Identifier of the device (64 bits), which the device will use for commissioning.

  • PSKD: Pre-shared Key of Device, which the device will use for commissioning.

Nwk Info

The Nwk Info lines show information of the network which this device belongs to.

  • Network Name: The human-readable name of this network.

  • ExtPanID: The 64-bit extended PANID of this network.

  • Masterkey: The 128-bit masterkey in use by the network.

  • PAN ID: The 16-bit PAN ID of this network.

  • Channel: The 2.4 GHz channel occupied by this network.

  • Short Addr: The 16-bit network address assigned to this device.

Role Info

The role info line shows the current role of the device:

  • Disabled: Thread stack is disabled; the default initial state of the device on reset.

  • Detached: Device is not part of a Thread network.

  • Child: Device is operating as a child in its Thread network.

  • Router: Device is operating as a router in its Thread network.

  • Leader: Device is operating as the leader in its Thread network.

Conn Info

The conn info line shows the connection status of the device:

  • Disabled: No connection; the default initial state of the connection on reset.

  • Joining Nwk: Device is attempting to connect to a network.

  • Nwk Joined: Device has successfully joined a network.

  • Join Failure: Device failed an attempt to connect to a network.

APP Info

The app info line shows the application-specific state of the device. For more details, refer to the application’s respective README.

Config

The Configure menu contains sub-menus that allow the user to change common network parameters.

../_images/Config-screen.png

Figure 26. Configure Menu

PAN ID

The PAN ID menu allows the user to configure the PAN ID of the network to join or form. A value of 0xFFFF indicates an unspecified PAN ID. After this device is part of a network, this value indicates the PAN ID of that network, and changing this value is not valid.

../_images/Panid-screen.png

Figure 27. PAN ID Screen

PAN ID - view mode

Key

Function

Comment

Left/Right

Menu navigation

Move to previous/next screen

Enter

Select

Enter edit mode

PAN ID - edit mode

Key

Function

Comment

Left/Right

Digit navigation

Move to previous/next digit

Up/Down

Value change

Increase/decrease the value of the highlighted digit

Keyboard (hex values)

Value change

Set the selected byte of the PAN ID to the key pressed

Enter

Select

Save and enter view mode

Channel

The channel of the network that this device will attempt to attach or form. Once joined to a network, this value indicates the channel of that network.

../_images/Channel-screen.png

Figure 28. Channel Screen

Channel - view mode

Key

Function

Comment

Enter

Select

Enter edit mode

Channel - edit mode

Key

Function

Comment

Enter

Select

Save and enter view mode

Left/Right

Select digit

Move to previous/next digit

Number key

Set channel

Channel must be between 11 and 26 (inclusively)

NWK

The Network menu contains sub-menus that allow the user to start network operations.

../_images/Nwk-screen.png

Figure 29. Network Menu

Join

Start the network join process via the commissioner using the pre-configured PSKd. Press Enter on this menu to trigger this.

../_images/Join-screen.png

Figure 30. Join Menu

Attach

Application attempts to bring up the interface and setup the Thread network, using the current device dataset. Press Enter on this menu to trigger this.

../_images/Attach-screen.png

Figure 31. Attach Menu

App Menu

The App menu contain application-specific sub-menus and actions. Refer to the README of the respective application example for details on what actions are supported.

../_images/Appmenu-screen.png

Figure 32. App Menu

Reset

The Reset menu may be used to reset the OpenThread Instance without clearing out previous network data. Press Enter on this menu to trigger this.

../_images/Reset-screen.png

Figure 33. Reset Menu

NWK Reset

The Network Reset menu may be used to reset the OpenThread Instance and clear out the previous network data. Press Enter on this menu to trigger this.

../_images/Nwkreset-screen.png

Figure 34. NWK Reset Menu

End Product Examples

Door Lock

The door lock project presents a simple CoAP server representing a door lock. Only an MTD configuration is available. The door lock example is best used with a Sharp Memory LCD and microSD BoosterPack, but also can be used with only the basic UART log.

There are also OAD-enabled variants of the Door Lock example. For more information, please refer to Section Door Lock OAD.

Shade

The shade project presents a simple CoAP server representing window blinds. Only an MTD configuration is available. The shade example is best used with a Sharp Memory LCD and microSD BoosterPack, but also can be used with only the basic UART log.

Temperature Sensor

The Temperature Sensor project presents a simple CoAP server and client representing an embedded temperature sensor. Only an MTD configuration is available.

Thermostat

The thermostat project presents a simple CoAP server representing a thermostat. Only an FTD configuration is available. The thermostat example is best used with a Sharp Memory LCD and microSD BoosterPack, but also can be used with only the basic UART log.

Other Examples

Command Line Interface (CLI)

The CLI projects can be used to interact with and explore the different aspects of the Thread protocol. Both an FTD and MTD configuration is available. The CLI interface OpenThread presents is also used for certification with the Thread Group test harness.

Network Co-Processor (NCP)

The NCP project is used to connect the TI-OpenThread to a host processor. Only an FTD configuration is available. For more information about the interface between the NCP and host processor, see Section NCP Interface.

Border Router

The border router example is a basic implementation of a Thread Border Router, which bridges IP traffic from an external IP network to the Thread network and vice-versa. A Thread Border Router also enables off-mesh commissioning of new devices into the Thread network.

OAD Server

The OAD Server example is a C program meant to run on a Linux environment which is connected to a border router. For more information, see Section OAD Server.