|
#define | SPI_DMA_DONE_TX SPI_IMASK_DMA_DONE_TX |
| DMA Done 1 event for TX event mask. More...
|
|
#define | SPI_DMA_DONE_RX SPI_IMASK_DMA_DONE_RX |
| DMA Done 1 event for RX event mask. More...
|
|
#define | SPI_IDLE SPI_IMASK_IDLE |
| SPI Idle event mask. More...
|
|
#define | SPI_TXEMPTY SPI_IMASK_TXEMPTY |
| Transmit FIFO Empty event mask. More...
|
|
#define | SPI_TX SPI_IMASK_TX |
| Transmit FIFO event mask. More...
|
|
#define | SPI_RX SPI_IMASK_RX |
| Receive FIFO event. This interrupt is set if the selected Receive FIFO level has been reached. More...
|
|
#define | SPI_RTOUT SPI_IMASK_RTOUT |
| Enable SPI Receive Time-Out event mask. More...
|
|
#define | SPI_PER SPI_IMASK_PER |
| Parity error event mask. More...
|
|
#define | SPI_RXFIFO_OVF SPI_IMASK_RXFIFO_OVF |
| RXFIFO overflow event mask. More...
|
|
#define | SPI_BUSY SPI_STAT_BUSY_ACTIVE |
| Busy. More...
|
|
#define | SPI_RX_NOT_FULL SPI_STAT_RNF_NOT_FULL |
| Receive FIFO not full. More...
|
|
#define | SPI_RX_EMPTY SPI_STAT_RFE_EMPTY |
| Receive FIFO empty. More...
|
|
#define | SPI_TX_NOT_FULL SPI_STAT_TNF_NOT_FULL |
| Transmit FIFO not full. More...
|
|
#define | SPI_TX_EMPTY SPI_STAT_TFE_EMPTY |
| Transmit FIFO empty. More...
|
|
#define | SPI_STATUS_MASK 0x0000001F |
| Mask for bits above. More...
|
|
#define | SPI_FRF_MOTO_MODE_0 |
| Motorola format 3-wire, polarity 0, phase 0. More...
|
|
#define | SPI_FRF_MOTO_MODE_1 |
| Motorola format 3-wire, polarity 0, phase 1. More...
|
|
#define | SPI_FRF_MOTO_MODE_2 |
| Motorola format 3-wire, polarity 1, phase 0. More...
|
|
#define | SPI_FRF_MOTO_MODE_3 |
| Motorola format 3-wire, polarity 1, phase 1. More...
|
|
#define | SPI_FRF_MOTO_MODE_4 |
| Motorola format 4-wire, polarity 0, phase 0. More...
|
|
#define | SPI_FRF_MOTO_MODE_5 |
| Motorola format 4-wire, polarity 0, phase 1. More...
|
|
#define | SPI_FRF_MOTO_MODE_6 |
| Motorola format 4-wire, polarity 1, phase 0. More...
|
|
#define | SPI_FRF_MOTO_MODE_7 |
| Motorola format 4-wire, polarity 1, phase 1. More...
|
|
#define | SPI_FRF_TI SPI_CTL0_FRF_TI_SYNC |
| TI Sync frame format. More...
|
|
#define | SPI_FRF_NMW SPI_CTL0_FRF_MIRCOWIRE |
| MicroWire frame format. More...
|
|
#define | SPI_MODE_CONTROLLER SPI_CTL1_MS_ENABLE |
| SPI controller. More...
|
|
#define | SPI_MODE_PERIPHERAL SPI_CTL1_MS_DISABLE |
| SPI peripheral. More...
|
|
#define | SPI_MODE_PERIPHERAL_OD SPI_CTL1_SOD_ENABLE |
| output disabled More...
|
|
#define | SPI_DMA_TX SPI_DMACR_TXDMAE |
| Enable DMA for transmit. More...
|
|
#define | SPI_DMA_RX SPI_DMACR_RXDMAE |
| Enable DMA for receive. More...
|
|
|
void | SPIConfigSetExpClk (uint32_t ui32Base, uint32_t ui32SPIClk, uint32_t ui32Protocol, uint32_t ui32Mode, uint32_t ui32BitRate, uint32_t ui32DataWidth) |
| Configures the serial peripheral port. More...
|
|
static void | SPIEnable (uint32_t ui32Base) |
| Enables the serial peripheral port. More...
|
|
static void | SPIDisable (uint32_t ui32Base) |
| Disables the serial peripheral port. More...
|
|
void | SPIDataPut (uint32_t ui32Base, uint32_t ui32Data) |
| Puts a data element into the SPI transmit FIFO. More...
|
|
int32_t | SPIDataPutNonBlocking (uint32_t ui32Base, uint32_t ui32Data) |
| Puts a data element into the SPI transmit FIFO. More...
|
|
void | SPIDataGet (uint32_t ui32Base, uint32_t *pui32Data) |
| Gets a data element from the SPI receive FIFO. More...
|
|
int32_t | SPIDataGetNonBlocking (uint32_t ui32Base, uint32_t *pui32Data) |
| Gets a data element from the SPI receive FIFO. More...
|
|
static bool | SPIBusy (uint32_t ui32Base) |
| Determines whether the SPI transmitter is busy or not. More...
|
|
static uint32_t | SPIStatus (uint32_t ui32Base) |
| Get the status of the SPI data buffers. More...
|
|
void | SPIIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| Registers an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
|
|
void | SPIIntUnregister (uint32_t ui32Base) |
| Unregisters an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
|
|
static void | SPIIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Enables individual SPI interrupt sources. More...
|
|
static void | SPIIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Disables individual SPI interrupt sources. More...
|
|
static void | SPIIntClear (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Clears SPI interrupt sources. More...
|
|
static uint32_t | SPIIntStatus (uint32_t ui32Base, bool bMasked) |
| Gets the current interrupt status. More...
|
|
static void | SPIDMAEnable (uint32_t ui32Base, uint32_t ui32DMAFlags) |
| Enable SPI DMA operation. More...
|
|
static void | SPIDMADisable (uint32_t ui32Base, uint32_t ui32DMAFlags) |
| Disable SPI DMA operation. More...
|
|