Instance: AUX_TDC
Component: AUX_TDC
Base address: 0x400C4000
AUX Time To Digital Converter (AUX_TDC) is used to measure the time between two events with high resolution.
AUX_TDC consists of a state machine that operates at AUX bus rate and an asynchronous fast-counter which is clocked by the TDC clock. DDI_0_OSC:CTL0.ACLK_TDC_SRC_SEL configures TDC clock source. The fast-counter counts on both edges of the TDC clock to double the resolution.
See the Technical Reference Manual for event timing requirements.
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x400C 4000 |
|
RO |
32 |
0x0000 0006 |
0x0000 0004 |
0x400C 4004 |
|
RO |
32 |
0x0000 0002 |
0x0000 0008 |
0x400C 4008 |
|
RW |
32 |
0x0000 000F |
0x0000 000C |
0x400C 400C |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0x400C 4010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x400C 4014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0x400C 4018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x400C 401C |
|
RW |
32 |
0x0000 003F |
0x0000 0020 |
0x400C 4020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x400C 4024 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x400C 4000 | Instance | 0x400C 4000 |
Description | Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | |||||||||||||||||
1:0 | CMD | TDC commands.
|
WO | 0b00 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x400C 4004 | Instance | 0x400C 4004 |
Description | Status | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||||||||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||||||||||||||||||||||||||||||||||||||
7 | SAT | TDC measurement saturation flag. 0: Conversion has not saturated. 1: Conversion stopped due to saturation. This field is cleared when a new measurement is started or when CLR_RESULT is written to CTL.CMD. |
RO | 0 | ||||||||||||||||||||||||||||||||||||||
6 | DONE | TDC measurement complete flag. 0: TDC measurement has not yet completed. 1: TDC measurement has completed. This field clears when a new TDC measurement starts or when you write CLR_RESULT to CTL.CMD. |
RO | 0 | ||||||||||||||||||||||||||||||||||||||
5:0 | STATE | TDC state machine status.
|
RO | 0b00 0110 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x400C 4008 | Instance | 0x400C 4008 |
Description | Result Result of last TDC conversion. |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24:0 | VALUE | TDC conversion result. The result of the TDC conversion is given in number of clock edges of the clock source selected in DDI_0_OSC:CTL0.ACLK_TDC_SRC_SEL. Both rising and falling edges are counted. If TDC counter saturates, VALUE is slightly higher than SATCFG.LIMIT, as it takes a non-zero time to stop the measurement. Hence, the maximum value of this field becomes slightly higher than 2^24 if you configure SATCFG.LIMIT to R24. |
RO | 0b0 0000 0000 0000 0000 0000 0010 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x400C 400C | Instance | 0x400C 400C |
Description | Saturation Configuration | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||||||||||||||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||||||||||||||||||||||||||||||||||||||||||||
3:0 | LIMIT | Saturation limit. The flag STAT.SAT is set when the TDC counter saturates. Values not enumerated are not supported
|
RW | 0xF |
Address Offset | 0x0000 0010 | ||
Physical Address | 0x400C 4010 | Instance | 0x400C 4010 |
Description | Trigger Source Select source and polarity for TDC start and stop events. See the Technical Reference Manual for event timing requirements. |
||
Type | RW |
Address Offset | 0x0000 0014 | ||
Physical Address | 0x400C 4014 | Instance | 0x400C 4014 |
Description | Trigger Counter Stop-counter control and status. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
15:0 | CNT | Number of stop events to ignore when AUX_TDC:TRIGCNTCFG.EN is 1. Read CNT to get the remaining number of stop events to ignore during a TDC measurement. Write CNT to update the remaining number of stop events to ignore during a TDC measurement. The TDC measurement ignores updates of CNT if there are no more stop events left to ignore. When AUX_TDC:TRIGCNTCFG.EN is 1, TRIGCNTLOAD.CNT is loaded into CNT at the start of the measurement. |
RW | 0x0000 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x400C 4018 | Instance | 0x400C 4018 |
Description | Trigger Counter Load Stop-counter load. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
15:0 | CNT | Number of stop events to ignore when AUX_TDC:TRIGCNTCFG.EN is 1. To measure frequency of an event source: - Set start event equal to stop event. - Set CNT to number of periods to measure. Both 0 and 1 values measures a single event source period. To measure pulse width of an event source: - Set start event source equal to stop event source. - Select different polarity for start and stop event. - Set CNT to 0. To measure time from the start event to the Nth stop event when N > 1: - Select different start and stop event source. - Set CNT to (N-1). See the Technical Reference Manual for event timing requirements. When AUX_TDC:TRIGCNTCFG.EN is 1, CNT is loaded into TRIGCNT.CNT at the start of the measurement. |
RW | 0x0000 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x400C 401C | Instance | 0x400C 401C |
Description | Trigger Counter Configuration Stop-counter configuration. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | EN | Enable stop-counter. 0: Disable stop-counter. 1: Enable stop-counter. Change only while STAT.STATE is IDLE. |
RW | 0 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0x400C 4020 | Instance | 0x400C 4020 |
Description | Prescaler Control The prescaler can be used to count events that are faster than the AUX bus rate. It can be used to: - count pulses on a specified event from the asynchronous event bus. - prescale a specified event from the asynchronous event bus. To use the prescaler output as an event source in TDC measurements you must set both TRIGSRC.START_SRC and TRIGSRC.STOP_SRC to AUX_TDC_PRE. It is recommended to use the prescaler when the signal frequency to measure exceeds 1/10th of the AUX bus rate. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
7 | RESET_N | Prescaler reset. 0: Reset prescaler. 1: Release reset of prescaler. AUX_TDC_PRE event becomes 0 when you reset the prescaler. |
RW | 0 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
6 | RATIO | Prescaler ratio. This controls how often the AUX_TDC_PRE event is generated by the prescaler.
|
RW | 0 | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
5:0 | SRC | Prescaler event source. Select an event from the asynchronous AUX event bus to connect to the prescaler input. Configure only while RESET_N is 0.
|
RW | 0b11 1111 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0x400C 4024 | Instance | 0x400C 4024 |
Description | Prescaler Counter | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
15:0 | CNT | Prescaler counter value. Write a value to CNT to capture the value of the 16-bit prescaler counter into CNT. Read CNT to get the captured value. The read value gets 1 LSB uncertainty if the event source level rises when you release the reset. The read value gets 1 LSB uncertainty if the event source level rises when you capture the prescaler counter. Please note the following: - The prescaler counter is reset to 2 by PRECTL.RESET_N. - The captured value is 2 when the number of rising edges on prescaler input is less than 3. Otherwise, captured value equals number of event pulses - 1. |
RW | 0x0000 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |