Data Structures | |
union | ECC_NISTP256_Param |
Functions | |
void | ECC_initialize (ECC_State *state, uint32_t *workzone) |
Initialize elliptic curve parameters to default values and specify workzone. More... | |
void | ECC_init (ECC_State *state, uint32_t *workzone, uint8_t windowSize, const uint32_t *prime, const uint32_t *order, const uint32_t *a, const uint32_t *b, const uint32_t *generatorX, const uint32_t *generatorY) |
Initialize elliptic curve parameters to specified values and specify workzone. More... | |
uint8_t | ECC_generateKey (ECC_State *state, uint32_t *randEntropy, uint32_t *privateKey, uint32_t *publicKey_x, uint32_t *publicKey_y) |
Generate a public key. More... | |
uint8_t | ECC_ECDSA_sign (ECC_State *state, uint32_t *privateKey, uint32_t *hash, uint32_t *pmsn, uint32_t *r, uint32_t *s) |
Sign message digest. More... | |
uint8_t | ECC_ECDSA_verify (ECC_State *state, uint32_t *publicKey_x, uint32_t *publicKey_y, uint32_t *hash, uint32_t *r, uint32_t *s) |
Verify signature. More... | |
uint8_t | ECC_ECDH_computeSharedSecret (ECC_State *state, uint32_t *privateKey, uint32_t *publicKey_x, uint32_t *publicKey_y, uint32_t *sharedSecret_x, uint32_t *sharedSecret_y) |
Compute the shared secret. More... | |
uint8_t | ECC_validatePrivateKey (ECC_State *state, uint32_t *privateKey) |
Validate a private key against the currently set elliptic curve. More... | |
uint8_t | ECC_validatePublicKey (ECC_State *state, uint32_t *publicKey_x, uint32_t *publicKey_y) |
Validate a public key against the currently set elliptic curve. More... | |
Variables | |
const ECC_NISTP256_Param | ECC_NISTP256_generatorX |
X coordinate of the generator point of the ECC_NISTP256 curve. More... | |
const ECC_NISTP256_Param | ECC_NISTP256_generatorY |
Y coordinate of the generator point of the ECC_NISTP256 curve. More... | |
const ECC_NISTP256_Param | ECC_NISTP256_prime |
prime of the ECC_NISTP256 curve. More... | |
const ECC_NISTP256_Param | ECC_NISTP256_a |
a constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More... | |
const ECC_NISTP256_Param | ECC_NISTP256_b |
b constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More... | |
const ECC_NISTP256_Param | ECC_NISTP256_order |
order of the ECC_NISTP256 curve. More... | |
const ECC_NISTP256_Param | ECC_NISTP256_k_mont |
k in Montgomery domain of the ECC_NISTP256 curve. More... | |
const ECC_NISTP256_Param | ECC_NISTP256_a_mont |
a in Montgomery domain of the ECC_NISTP256 curve. More... | |
const ECC_NISTP256_Param | ECC_NISTP256_b_mont |
b in Montgomery domain of the ECC_NISTP256 curve. More... | |
const ECC_NISTP256_Param | ECC_NISTP256_gx_mont |
X coordinate of the generator point in Montgomery domain of the ECC_NISTP256 curve. More... | |
#define ECC_LENGTH_OFFSET_BYTES 4 |
Number of bytes for the length word prepended before all parameters passed into the ECC functions.
#define ECC_NISTP256_PARAM_LENGTH_BYTES 32 |
Length in bytes of NISTP256 curve parameters excluding the prepended length word.
#define ECC_NISTP256_PARAM_LENGTH_WITH_OFFSET_BYTES (ECC_NISTP256_PARAM_LENGTH_BYTES + ECC_LENGTH_OFFSET_BYTES) |
Length in bytes of NISTP256 curve parameters including the prepended length word.
#define STATUS_A_COEF_LENGTH_ZERO 0xC5 |
#define STATUS_A_COEF_TOO_LONG 0x5C |
#define STATUS_BAD_WINDOW_SIZE 0x66 |
#define STATUS_DIGEST_LENGTH_ZERO 0x72 |
#define STATUS_DIGEST_TOO_LONG 0x27 |
#define STATUS_ECC_KEY_LENGTH_ZERO 0x52 |
#define STATUS_ECC_KEY_TOO_LONG 0x25 |
#define STATUS_ECC_POINT_NOT_ON_CURVE 0x15 |
#define STATUS_ECC_POINT_ON_CURVE 0x16 |
#define STATUS_ECC_X_LARGER_THAN_PRIME 0x11 |
#define STATUS_ECC_X_ZERO 0x13 |
#define STATUS_ECC_Y_LARGER_THAN_PRIME 0x12 |
#define STATUS_ECC_Y_ZERO 0x14 |
#define STATUS_ECDH_COMMON_KEY_OK STATUS_SCALAR_MUL_OK |
#define STATUS_ECDH_KEYGEN_OK STATUS_SCALAR_MUL_OK |
#define STATUS_ECDSA_INVALID_SIGNATURE 0x5A |
#define STATUS_ECDSA_KEYGEN_OK STATUS_SCALAR_MUL_OK |
#define STATUS_ECDSA_SIGN_OK 0x32 |
#define STATUS_ECDSA_VALID_SIGNATURE 0xA5 |
#define STATUS_MODULUS_EVEN 0xDC |
#define STATUS_MODULUS_LARGER_THAN_255_WORDS 0xD2 |
#define STATUS_MODULUS_LENGTH_ZERO 0x08 |
#define STATUS_MODULUS_MSW_IS_ZERO 0x30 |
#define STATUS_ORDER_EVEN 0x82 |
#define STATUS_ORDER_LARGER_THAN_255_WORDS 0x28 |
#define STATUS_ORDER_LENGTH_ZERO 0x6C |
#define STATUS_ORDER_MSW_IS_ZERO 0x23 |
#define STATUS_ORDER_TOO_LONG 0xC6 |
#define STATUS_PRIVATE_KEY_LARGER_EQUAL_ORDER 0x18 |
#define STATUS_PRIVATE_KEY_ZERO 0x17 |
#define STATUS_PRIVATE_VALID 0x19 |
#define STATUS_SCALAR_LENGTH_ZERO 0x53 |
#define STATUS_SCALAR_MUL_OK 0x99 |
#define STATUS_SCALAR_TOO_LONG 0x35 |
#define STATUS_SIG_P1_LENGTH_ZERO 0x12 |
#define STATUS_SIG_P1_TOO_LONG 0x11 |
#define STATUS_SIG_P2_LENGTH_ZERO 0x21 |
#define STATUS_SIG_P2_TOO_LONG 0x22 |
#define STATUS_X_COORD_LENGTH_ZERO 0xC3 |
#define STATUS_X_COORD_TOO_LONG 0x3C |
#define STATUS_Y_COORD_LENGTH_ZERO 0x56 |
#define STATUS_Y_COORD_TOO_LONG 0x65 |
uint8_t ECC_ECDH_computeSharedSecret | ( | ECC_State * | state, |
uint32_t * | privateKey, | ||
uint32_t * | publicKey_x, | ||
uint32_t * | publicKey_y, | ||
uint32_t * | sharedSecret_x, | ||
uint32_t * | sharedSecret_y | ||
) |
Compute the shared secret.
[in,out] | state | Struct to keep track of the state of the operation |
[in] | privateKey | Pointer to private key |
[in] | publicKey_x | Pointer to public key X-coordinate |
[in] | publicKey_y | Pointer to public key Y-coordinate |
[out] | sharedSecret_x | Pointer to shared secret X-coordinate |
[out] | sharedSecret_y | Pointer to shared secret Y-coordinate |
uint8_t ECC_ECDSA_sign | ( | ECC_State * | state, |
uint32_t * | privateKey, | ||
uint32_t * | hash, | ||
uint32_t * | pmsn, | ||
uint32_t * | r, | ||
uint32_t * | s | ||
) |
Sign message digest.
[in,out] | state | Struct to keep track of the state of the operation |
[in] | privateKey | Pointer to the secret key |
[in] | hash | Pointer to the message |
[in] | pmsn | Pointer to random string |
[out] | r | Pointer to r component of signature |
[out] | s | Pointer to s component of signature |
uint8_t ECC_ECDSA_verify | ( | ECC_State * | state, |
uint32_t * | publicKey_x, | ||
uint32_t * | publicKey_y, | ||
uint32_t * | hash, | ||
uint32_t * | r, | ||
uint32_t * | s | ||
) |
Verify signature.
[in,out] | state | Struct to keep track of the state of the operation |
[in] | publicKey_x | Pointer to public key X-coordinate |
[in] | publicKey_y | Pointer to public key Y-coordinate |
[in] | hash | Pointer to hash of message digest |
[in] | r | Pointer to r component of signature |
[in] | s | Pointer to s component of signature |
uint8_t ECC_generateKey | ( | ECC_State * | state, |
uint32_t * | randEntropy, | ||
uint32_t * | privateKey, | ||
uint32_t * | publicKey_x, | ||
uint32_t * | publicKey_y | ||
) |
Generate a public key.
This is used for both ECDH and ECDSA.
[in,out] | state | Struct to keep track of the state of the operation |
[in] | randEntropy | Pointer to random string |
[out] | privateKey | Pointer to the private key. May be the same location as randEntropy . |
[out] | publicKey_x | Pointer to public key X-coordinate |
[out] | publicKey_y | Pointer to public key Y-coordinate |
void ECC_init | ( | ECC_State * | state, |
uint32_t * | workzone, | ||
uint8_t | windowSize, | ||
const uint32_t * | prime, | ||
const uint32_t * | order, | ||
const uint32_t * | a, | ||
const uint32_t * | b, | ||
const uint32_t * | generatorX, | ||
const uint32_t * | generatorY | ||
) |
Initialize elliptic curve parameters to specified values and specify workzone.
This function may be used to explicitly specify the curve parameters used by the ECC in ROM implementation.
All curve parameters must be prepended with a length word specifying the length of the parameter in 32-bit words excluding the length word itself. For NIST-P256, the length word is 8.
state | Struct to keep track of the state of the operation. |
workzone | Pointer to memory allocated for computations, input. See description at beginning of ECC section for memory requirements. |
windowSize | Window size of workzone . Default value is 3. |
prime | Curve prime |
order | Curve order |
a | Curve a value |
b | Curve b value |
generatorX | X coordinate of generator point |
generatorY | Y coordinate of generator point |
void ECC_initialize | ( | ECC_State * | state, |
uint32_t * | workzone | ||
) |
Initialize elliptic curve parameters to default values and specify workzone.
This function initializes the elliptic curve parameters to default values. The default elliptic curve used is NIST-P256.
The workzone defaults to an expected window size of 3.
This function can be called again to point the ECC workzone at a different memory buffer.
state | Struct to keep track of the state of the operation. |
workzone | Pointer to memory allocated for computations, input. See description at beginning of ECC section for memory requirements. |
uint8_t ECC_validatePrivateKey | ( | ECC_State * | state, |
uint32_t * | privateKey | ||
) |
Validate a private key against the currently set elliptic curve.
Validates that private
key is within [1, n-1] where n is the order of the elliptic curve.
[in,out] | state | Struct to keep track of the state of the operation |
privateKey | Pointer to public key X-coordinate, input. |
uint8_t ECC_validatePublicKey | ( | ECC_State * | state, |
uint32_t * | publicKey_x, | ||
uint32_t * | publicKey_y | ||
) |
Validate a public key against the currently set elliptic curve.
[in,out] | state | Struct to keep track of the state of the operation |
publicKey_x | Pointer to public key X-coordinate, input. | |
publicKey_y | Pointer to public key Y-coordinate, input. |
const ECC_NISTP256_Param ECC_NISTP256_a |
a constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b).
const ECC_NISTP256_Param ECC_NISTP256_a_mont |
a in Montgomery domain of the ECC_NISTP256 curve.
const ECC_NISTP256_Param ECC_NISTP256_b |
b constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b).
const ECC_NISTP256_Param ECC_NISTP256_b_mont |
b in Montgomery domain of the ECC_NISTP256 curve.
const ECC_NISTP256_Param ECC_NISTP256_generatorX |
X coordinate of the generator point of the ECC_NISTP256 curve.
const ECC_NISTP256_Param ECC_NISTP256_generatorY |
Y coordinate of the generator point of the ECC_NISTP256 curve.
const ECC_NISTP256_Param ECC_NISTP256_gx_mont |
X coordinate of the generator point in Montgomery domain of the ECC_NISTP256 curve.
const ECC_NISTP256_Param ECC_NISTP256_k_mont |
k in Montgomery domain of the ECC_NISTP256 curve.
const ECC_NISTP256_Param ECC_NISTP256_order |
order of the ECC_NISTP256 curve.
const ECC_NISTP256_Param ECC_NISTP256_prime |
prime of the ECC_NISTP256 curve.