SYS/BIOS
7.00
|
Timestamp services.
This module provides a portable API for getting a 32 or 64-bit timestamp.
This module calls a family-specific TimestampProvider function that does the real work.
Go to the source code of this file.
Functions | |
uint32_t | Timestamp_get32 (void) |
get 32-bit timestamp More... | |
void | Timestamp_get64 (Types_Timestamp64 *timestamp64) |
get 64-bit timestamp More... | |
void | Timestamp_getFreq (Types_FreqHz *freq) |
get timestamp frequency More... | |
uint32_t Timestamp_get32 | ( | void | ) |
get 32-bit timestamp
void Timestamp_get64 | ( | Types_Timestamp64 * | timestamp64 | ) |
get 64-bit timestamp
timestamp64 | pointer to a 64-bit timestamp structure |
void Timestamp_getFreq | ( | Types_FreqHz * | freq | ) |
get timestamp frequency
Get the frequency of the timestamp counter in Hz. This function fills in a Types_FreqHz structure with the high and low 64 bit frequency.
freq | pointer to a 64-bit frequency structure |