45 #ifndef ti_sysbios_runtime_Types__include 46 #define ti_sysbios_runtime_Types__include 57 #if defined (__TI_COMPILER_VERSION__) || defined(__ti_version__) 67 #define ti_sysbios_runtime_Types_long_names 68 #include "Types_defs.h" 110 typedef int (*Types_Fxn)();
113 static inline void * Types_iargToPtr(intptr_t a)
118 static inline void * Types_uargToPtr(uintptr_t a)
123 static inline Types_Fxn Types_iargToFxn(intptr_t a)
125 return ((Types_Fxn)a);
128 static inline Types_Fxn Types_uargToFxn(uintptr_t a)
130 return ((Types_Fxn)a);
144 static inline intptr_t Types_floatToArg(
float f)
152 static inline float Types_argToFloat(intptr_t a)
168 #undef ti_sysbios_runtime_Types_long_names 169 #include "Types_defs.h" uint32_t lo
least significant 32-bits of frequency
Definition: Types.h:106
uint32_t hi
most significant 32-bits of timestamp
Definition: Types.h:85
uint32_t lo
least significant 32-bits of timestamp
Definition: Types.h:89
uint32_t hi
most significant 32-bits of frequency
Definition: Types.h:102
64-bit frequency struct (in Hz)
Definition: Types.h:98
64-bit timestamp struct
Definition: Types.h:81