|
__STATIC_INLINE void | RFCClockEnable (void) |
| Enable the RF core clocks. More...
|
|
__STATIC_INLINE void | RFCClockDisable (void) |
| Disable the RF core clocks. More...
|
|
__STATIC_INLINE void | RFCCpeIntClear (uint32_t ui32Mask) |
| Clear HW interrupt flags. More...
|
|
__STATIC_INLINE void | RFCHwIntClear (uint32_t ui32Mask) |
| Clear CPE interrupt flags. More...
|
|
__STATIC_INLINE void | RFCCpe0IntSelect (uint32_t ui32Mask) |
| Select interrupt sources to CPE0 (assign to INT_RFC_CPE_0 interrupt vector). More...
|
|
__STATIC_INLINE void | RFCCpe1IntSelect (uint32_t ui32Mask) |
| Select interrupt sources to CPE1 (assign to INT_RFC_CPE_1 interrupt vector). More...
|
|
__STATIC_INLINE void | RFCCpeIntEnable (uint32_t ui32Mask) |
| Enable CPEx interrupt sources. More...
|
|
__STATIC_INLINE void | RFCCpe0IntSelectClearEnable (uint32_t ui32Mask) |
| Select, clear, and enable interrupt sources to CPE0. More...
|
|
__STATIC_INLINE void | RFCCpe1IntSelectClearEnable (uint32_t ui32Mask) |
| Select, clear, and enable interrupt sources to CPE1. More...
|
|
__STATIC_INLINE void | RFCHwIntEnable (uint32_t ui32Mask) |
| Enable HW interrupt sources. More...
|
|
__STATIC_INLINE void | RFCCpeIntDisable (uint32_t ui32Mask) |
| Disable CPE interrupt sources. More...
|
|
__STATIC_INLINE void | RFCHwIntDisable (uint32_t ui32Mask) |
| Disable HW interrupt sources. More...
|
|
uint32_t | NOROM_RFCCpeIntGetAndClear (uint32_t ui32Mask) |
| Get and clear CPE interrupt flags. More...
|
|
__STATIC_INLINE void | RFCAckIntClear (void) |
| Clear ACK interrupt flag. More...
|
|
uint32_t | NOROM_RFCDoorbellSendTo (uint32_t pOp) |
| Send a radio operation to the doorbell and wait for an acknowledgment. More...
|
|
void | NOROM_RFCSynthPowerDown (void) |
| This function implements a fast way to turn off the synthesizer. More...
|
|
void | NOROM_RFCCpePatchReset (void) |
| Reset previously patched CPE RAM to a state where it can be patched again. More...
|
|
uint8_t | NOROM_RFCOverrideSearch (const uint32_t *pOverride, const uint32_t pattern, const uint32_t mask, const uint8_t searchDepth) |
|
uint8_t | NOROM_RFCOverrideUpdate (rfc_radioOp_t *pOpSetup, uint32_t *pParams) |
| Function to update override list. More...
|
|
uint32_t | NOROM_RFCHwIntGetAndClear (uint32_t ui32Mask) |
| Get and clear HW interrupt flags. More...
|
|
__STATIC_INLINE bool | RFCGetPaType (void) |
| Get the type of currently selected PA. More...
|
|
__STATIC_INLINE uint32_t | RFCGetPaGain (void) |
| Get the gain of currently selected PA. More...
|
|
__STATIC_INLINE uint32_t | RFCGetPowerDomainStatus (void) |
| Get the power domain status of the radio core. More...
|
|
uint32_t | NOROM_RFCAnaDivTxOverride (uint8_t loDivider, uint8_t frontEndMode) |
| Function to calculate the proper override run-time for the High Gain PA. More...
|
|
void | NOROM_RFCRfTrimRead (rfc_radioOp_t *pOpSetup, rfTrim_t *rfTrim) |
| Read RF trim from flash using CM4. More...
|
|
void | NOROM_RFCRfTrimSet (rfTrim_t *rfTrim) |
| Write preloaded RF trim values directly into CPE. More...
|
|