SYS/BIOS  7.00
Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
Hwi.h File Reference

Detailed Description

Cortex M0 Hardware Interrupt Manager.

The Hardware Interrupt Manager provides APIs for managing hardware interrupts.

The user can dynamically assign routines that run when specific hardware interrupts occur.

Dynamic assignment of Hwi routines to interrupts at run-time is done using the Hwi_create() or Hwi_construct() functions.

Interrupt routines can be written completely in C, completely in assembly, or in a mix of C and assembly.

In order to support interrupt routines written completely in C, an interrupt dispatcher is provided that performs the requisite prolog and epilog for an interrupt routine so the interrupt function can safely inter-operate with the BIOS Task and Swi schedulers.

Some routines are assigned to interrupts by the other SYS/BIOS modules. For example, the Clock module configures its own timer interrupt handler. See the Clock Module for more details.

Runtime Hwi Creation

Below is an example of configuring an interrupt at runtime. Usually this code would be placed in main().

Hwi_Handle myHwi;
int main(int argc, char* argv[])
{
Hwi_Params hwiParams;
// set the argument you want passed to your ISR function
hwiParams.arg = 1;
//
// Configure interrupt 16 to invoke "myIsr".
// Automatically enables interrupt 16 by default
// set params.enableInt = false if you want to control
// when the interrupt is enabled using Hwi_enableInterrupt()
//
myHwi = Hwi_create(16, myIsr, &hwiParams, Error_IGNORE);
if (myHwi == NULL) {
// handle Hwi_create failure
}
}
void myIsr(uintptr_t arg)
{
// here when interrupt #16 goes off
}

Below is an example of configuring the same interrupt without requiring the use of a heap.

Hwi_Struct myHwiStruct;
Hwi_Handle myHwi;
int main(int argc, char* argv[])
{
Hwi_Params hwiParams;
// set the argument you want passed to your ISR function
hwiParams.arg = 1;
//
// Configure interrupt 16 to invoke "myIsr".
// Automatically enables interrupt 16 by default
// set params.enableInt = false if you want to control
// when the interrupt is enabled using Hwi_enableInterrupt()
//
myHwi = Hwi_construct(&myHwiStruct, 16, myIsr, &hwiParams, Error_IGNORE);
if (myHwi == NULL) {
// handle Hwi_create failure
}
}
void myIsr(uintptr_t arg)
{
// here when interrupt #16 goes off
}

The Cortex-M devices' Nested Vectored Interrupt Controller (NVIC) supports up to 256 interrupts/exceptions. In practice, most devices support much fewer (ie the SimpleLink CC13XX/CC26XX family of devices have around 50 total interrupts defined).

SYS/BIOS Interrupt IDs or interrupt numbers correspond to an interrupt's position in the interrupt vector table.

ID 0 corresponds to vector 0 which is used by the NVIC to hold the initial (reset) stack pointer value.

ID 1 corresponds to vector 1 which is the reset vector (ie _c_int00)

IDs 2-14 are hardwired to exceptions.

ID 15 is the SysTick timer interrupt.

ID's 16-255 are mapped to the NVIC's user interrupts 0-239 which are tied to platform specific interrupt sources.

Due to the M0's native automatic stacking of saved-by-caller C context on the way to an ISR, zero latency interrupt handlers are implemented using regular C functions (ie no 'interrupt' keyword is required).

Interrupt Masking Options

The NVIC interrupt controller is designed for priority based interrupts.

In this Hwi module, the Hwi_maskSetting instance configuration parameter is ignored. Effectively, only the Hwi_MaskingOption_LOWER is supported.

Interrupt Priorities

In general, the NVIC supports priority values of 0 thru 255.

In practice valid priorities values are device dependent and their nesting behaviors depend on the Hwi_priGroup setting.

See the Cortex M0 architecture reference manual for details on the behavior of interrupt priorities and their relationship to the Hwi_priGroup setting.

Interrupt Vector Tables

Tiva devices:

By default, two vector tables are created for Tiva devices:

A 15 entry boot vector table is placed at address 0x00000000 in FLASH.

A vector table of length Hwi_NUM_INTERRUPTS is placed at address 0x20000000 in RAM.

The FLASH boot vector table contains the reset vector and exception handler vectors used until the RAM based vector table is initialized.

The RAM vector table contains those same first 15 vectors plus the SysTick interrupt vector and the remainder of the user interrupt vectors.

During system startup, the NVIC Vector Table Offset Registor is intialized to point to the RAM vector table after it has been initialized.

Hook Functions

Sets of hook functions can be specified for the Hwi module using the configuration tool. Each set contains these hook functions:

Register: A function called before any statically-created Hwis are initialized at runtime. The register hook is called at boot time before main() and before interrupts are enabled.

Create: A function that is called when a Hwi is created. This includes hwis that are created statically and those created dynamically using Hwi_create.

Begin: A function that is called just prior to running a Hwi.

End: A function that is called just after a Hwi finishes.

Delete: A function that is called when a Hwi is deleted at run-time with Hwi_delete.

Register Function

The Register function is provided to allow a hook set to store its hookset ID. This id can be passed to "Hwi_setHookContext" and "Hwi_getHookContext" to set or get hookset- specific context. The Register function must be specified if the hook implementation needs to use "Hwi_setHookContext" or "Hwi_getHookContext". The registerFxn hook function is called during system initialization before interrupts have been enabled.

void myRegisterFxn(int id);

Create and Delete Functions

The create and delete functions are called whenever a Hwi is created or deleted. They are called with interrupts enabled (unless called at boot time or from main()).

void myCreateFxn(Hwi_Handle hwi, Error_Block *eb);
void myDeleteFxn(Hwi_Handle hwi);

Begin and End Functions

The beginFxn and endFxn function hooks are called with interrupts globally disabled, therefore any hook processing function will contribute to the overall system interrupt response latency. In order to minimize this impact, carefully consider the processing time spent in an Hwi beginFxn or endFxn function hook.

void myBeginFxn(Hwi_Handle hwi);
void myEndFxn(Hwi_Handle hwi);

Hook functions can only be configured statically.

To add a Hwi hook or set of Hwi hooks, the following syntax is used in the app.syscfg file:

const Hwi = scripting.addModule("/family/arm/v6m/Hwi");
Hwi.hwiHooks.create(1);
Hwi.hwiHooks[0].registerFxn = "myRegisterFxn";
Hwi.hwiHooks[0].createFxn = "myCreateFxn";
Hwi.hwiHooks[0].beginFxn = "myBeginFxn";
Hwi.hwiHooks[0].endFxn = "myEndFxn";
Hwi.hwiHooks[0].deleteFxn = "myDeleteFxn";

Leaving a subset of the hook functions undefined is ok.

Calling Context

Function Hwi Swi Task Main Startup
Hwi_clearInterrupt Y Y Y Y Y
Hwi_create N N Y Y N
Hwi_disable Y Y Y Y Y
Hwi_disableInterrupt Y Y Y Y N
Hwi_enable Y Y Y N N
Hwi_enableInterrupt Y Y Y Y N
Hwi_Params_init Y Y Y Y Y
Hwi_restore Y Y Y Y Y
Hwi_restoreInterrupt Y Y Y Y Y
Hwi_construct N N Y Y N
Hwi_delete N N Y Y N
Hwi_destruct N N Y Y N
Hwi_getHookContext Y Y Y Y N
Hwi_setFunc Y Y Y Y N
Hwi_setHookContext Y Y Y Y N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/runtime/Error.h>
Include dependency graph for Hwi.h:

Go to the source code of this file.

Data Structures

struct  Hwi_HookSet
 Hwi hook set type definition. More...
 
struct  Hwi_Hook
 
struct  Hwi_StackInfo
 Structure contains Hwi stack usage info. More...
 
struct  Hwi_NVIC
 Nested Vectored Interrupt Controller. More...
 
struct  Hwi_ExcContext
 Exception Context - Register contents at the time of an exception. More...
 
struct  Hwi_Module_State
 
struct  Hwi_Struct
 
struct  Hwi_Params
 

Macros

#define Hwi_E_badIntNum   "intnum: %d is out of range"
 Error raised Error raised if an attempt is made to create a Hwi with an interrupt number greater than Hwi_NUM_INTERRUPTS - 1. More...
 
#define Hwi_E_alreadyDefined   "Hwi already defined: intr# %d"
 Error raised when a Hwi is already defined. More...
 
#define Hwi_E_hwiLimitExceeded   "Too many interrupts defined"
 Error raised when the number of interrupts being created exceeds the number supported. More...
 
#define Hwi_E_exception   "hardware exception id = %d, pc = 0x%08x"
 Error raised when an exception occurs. More...
 
#define Hwi_E_noIsr   "no ISR, id = %d, pc = 0x%08x"
 Error raised when an uninitialized interrupt occurs. More...
 
#define Hwi_E_NMI   "NMI: %s"
 Error raised when NMI exception occurs. More...
 
#define Hwi_E_hardFault   "Hard-fault: %s"
 Error raised when hard fault exception occurs. More...
 
#define Hwi_E_memFault   "Mem-fault: %s, addresss: 0x%08x"
 Error raised when memory fault exception occurs. More...
 
#define Hwi_E_busFault   "Bus-fault: %s, address: 0x%08x"
 Error raised when bus fault exception occurs. More...
 
#define Hwi_E_usageFault   "Usage-fault: %s"
 Error raised when usage fault exception occurs. More...
 
#define Hwi_E_svCall   "SvCall: svNum = %d"
 Error raised when svCall exception occurs. More...
 
#define Hwi_E_debugMon   "Debug-monitor: %s"
 Error raised when debugMon exception occurs. More...
 
#define Hwi_E_reserved   "reserved %s %d"
 Error raised when reserved exceptions occur. More...
 
#define Hwi_E_stackOverflow   "ISR stack overflow"
 Error raised when the ISR stack has overflowed. More...
 

Typedefs

typedef struct Hwi_Struct Hwi_Struct
 
typedef struct Hwi_Struct Hwi_Object
 
typedef Hwi_StructHwi_Handle
 
typedef Hwi_StructHwi_Instance
 
typedef struct Hwi_HookSet Hwi_HookSet
 Hwi hook set type definition. More...
 
typedef struct Hwi_Module_State Hwi_Module_State
 
typedef struct Hwi_Params Hwi_Params
 
typedef struct Hwi_NVIC Hwi_NVIC
 Nested Vectored Interrupt Controller. More...
 
typedef struct Hwi_ExcContext Hwi_ExcContext
 Exception Context - Register contents at the time of an exception. More...
 
typedef struct Hwi_StackInfo Hwi_StackInfo
 Structure contains Hwi stack usage info. More...
 
typedef void(* Hwi_FuncPtr) (uintptr_t)
 Hwi create function type definition. More...
 
typedef void(* Hwi_VectorFuncPtr) (void)
 Hwi vector function type definition. More...
 
typedef void(* Hwi_ExceptionHookFuncPtr) (Hwi_ExcContext *arg1)
 Exception hook function type definition. More...
 
typedef Hwi_ExceptionHookFuncPtr Hwi_ExcHookFunc
 
typedef enum Hwi_MaskingOption Hwi_MaskingOption
 Shorthand interrupt masking options. More...
 
typedef void(* Hwi_ExcHandlerFuncPtr) (unsigned int *arg1, unsigned int arg2)
 Hwi exception handler function type definition. More...
 

Enumerations

enum  Hwi_MaskingOption {
  Hwi_MaskingOption_NONE,
  Hwi_MaskingOption_ALL,
  Hwi_MaskingOption_SELF,
  Hwi_MaskingOption_BITMASK,
  Hwi_MaskingOption_LOWER
}
 Interrupt masking options. More...
 

Functions

unsigned int Hwi_Disable ()
 Globally disable interrupts. More...
 
unsigned int Hwi_Enable ()
 Globally enable interrupts. More...
 
void Hwi_Restore (uint32_t key)
 restore global interrupts to the state they were in prior Hwi_disable(). More...
 
Hwi_Handle Hwi_create (int intNum, Hwi_FuncPtr hwiFxn, const Hwi_Params *prms, Error_Block *eb)
 
Hwi_Handle Hwi_construct (Hwi_Struct *obj, int intNum, Hwi_FuncPtr hwiFxn, const Hwi_Params *prms, Error_Block *eb)
 
void Hwi_delete (Hwi_Handle *handle)
 
void Hwi_destruct (Hwi_Struct *obj)
 
bool Hwi_getStackInfo (Hwi_StackInfo *stkInfo, bool computeStackDepth)
 Get Hwi stack usage Info. More...
 
void Hwi_post (unsigned int intNum)
 Generate an interrupt for test purposes. More...
 
unsigned int Hwi_disableInterrupt (unsigned int intNum)
 Disable a specific interrupt. More...
 
unsigned int Hwi_enableInterrupt (unsigned int intNum)
 Enable a specific interrupt. More...
 
void Hwi_restoreInterrupt (unsigned int intNum, unsigned int key)
 Restore a specific interrupt's enabled/disabled state. More...
 
void Hwi_clearInterrupt (unsigned int intNum)
 Clear a specific interrupt. More...
 
Hwi_FuncPtr Hwi_getFunc (Hwi_Handle hwi, uintptr_t *arg)
 Get Hwi function and arg. More...
 
void Hwi_setFunc (Hwi_Handle hwi, Hwi_FuncPtr fxn, uintptr_t arg)
 Overwrite Hwi function and arg. More...
 
void * Hwi_getHookContext (Hwi_Handle hwi, int id)
 Get hook instance's context for a Hwi. More...
 
void Hwi_setHookContext (Hwi_Handle hwi, int id, void *hookContext)
 Set hook instance's context for a Hwi. More...
 
uintptr_t Hwi_getIrp (Hwi_Handle hwi)
 Get address of interrupted instruction. More...
 
void Hwi_plug (unsigned int intNum, void *fxn)
 Plug a non dispatched interrupt vector with an ISR address. More...
 
Hwi_Handle Hwi_getHandle (unsigned int intNum)
 Returns Hwi_handle associated with intNum. More...
 
void Hwi_setPriority (unsigned int intNum, unsigned int priority)
 Set an interrupt's relative priority. More...
 
void Hwi_excSetBuffers (void *excContextBuffer, void *excStackBuffer)
 Set the exception context and stack buffer pointers. More...
 
void Hwi_reconfig (Hwi_Handle hwi, Hwi_FuncPtr fxn, const Hwi_Params *params)
 Reconfigure a dispatched interrupt. More...
 
void Hwi_Params_init (Hwi_Params *prms)
 
Hwi_Handle Hwi_Object_first (void)
 
Hwi_Handle Hwi_Object_next (Hwi_Object *obj)
 

Variables

volatile Hwi_NVIC Hwi_nvic
 Physical Nested Vectored Interrupt Controller Device. short name is "Hwi_nvic" long name is "ti_sysbios_family_arm_m3_Hwi_nvic". More...
 
const int Hwi_NUM_INTERRUPTS
 The Cortex M0 NVIC supports up to 256 interrupts/exceptions. More...
 
const int Hwi_NUM_PRIORITIES
 The Cortex M0 NVIC supports up to 256 interrupt priorities. More...
 
const Hwi_ExcHookFunc Hwi_excHookFunc
 User Exception hook function. More...
 
const unsigned int Hwi_disablePriority
 The priority that BASEPRI is set to by Hwi_disable(). More...
 
const unsigned int Hwi_priGroup
 The PRIGROUP setting. Default is 0. More...
 
const unsigned int Hwi_numSparseInterrupts
 If Hwi.dispatchTableSize is initialized by the user then Hwi.numSparseInterrupts is set to the value of Hwi.dispatchTableSize. More...
 

Macro Definition Documentation

§ Hwi_E_badIntNum

#define Hwi_E_badIntNum   "intnum: %d is out of range"

Error raised Error raised if an attempt is made to create a Hwi with an interrupt number greater than Hwi_NUM_INTERRUPTS - 1.

§ Hwi_E_alreadyDefined

#define Hwi_E_alreadyDefined   "Hwi already defined: intr# %d"

Error raised when a Hwi is already defined.

§ Hwi_E_hwiLimitExceeded

#define Hwi_E_hwiLimitExceeded   "Too many interrupts defined"

Error raised when the number of interrupts being created exceeds the number supported.

§ Hwi_E_exception

#define Hwi_E_exception   "hardware exception id = %d, pc = 0x%08x"

Error raised when an exception occurs.

§ Hwi_E_noIsr

#define Hwi_E_noIsr   "no ISR, id = %d, pc = 0x%08x"

Error raised when an uninitialized interrupt occurs.

§ Hwi_E_NMI

#define Hwi_E_NMI   "NMI: %s"

Error raised when NMI exception occurs.

§ Hwi_E_hardFault

#define Hwi_E_hardFault   "Hard-fault: %s"

Error raised when hard fault exception occurs.

§ Hwi_E_memFault

#define Hwi_E_memFault   "Mem-fault: %s, addresss: 0x%08x"

Error raised when memory fault exception occurs.

§ Hwi_E_busFault

#define Hwi_E_busFault   "Bus-fault: %s, address: 0x%08x"

Error raised when bus fault exception occurs.

§ Hwi_E_usageFault

#define Hwi_E_usageFault   "Usage-fault: %s"

Error raised when usage fault exception occurs.

§ Hwi_E_svCall

#define Hwi_E_svCall   "SvCall: svNum = %d"

Error raised when svCall exception occurs.

§ Hwi_E_debugMon

#define Hwi_E_debugMon   "Debug-monitor: %s"

Error raised when debugMon exception occurs.

§ Hwi_E_reserved

#define Hwi_E_reserved   "reserved %s %d"

Error raised when reserved exceptions occur.

§ Hwi_E_stackOverflow

#define Hwi_E_stackOverflow   "ISR stack overflow"

Error raised when the ISR stack has overflowed.

Typedef Documentation

§ Hwi_Struct

typedef struct Hwi_Struct Hwi_Struct

§ Hwi_Object

typedef struct Hwi_Struct Hwi_Object

§ Hwi_Handle

§ Hwi_Instance

§ Hwi_HookSet

typedef struct Hwi_HookSet Hwi_HookSet

Hwi hook set type definition.

The functions that make up a hookSet have certain restrictions. They cannot call any Hwi instance functions other than Hwi_getHookContext() and Hwi_setHookContext(). For all practical purposes, they should treat the Hwi_Handle passed to these functions as an opaque handle.

§ Hwi_Module_State

§ Hwi_Params

typedef struct Hwi_Params Hwi_Params

§ Hwi_NVIC

typedef struct Hwi_NVIC Hwi_NVIC

Nested Vectored Interrupt Controller.

§ Hwi_ExcContext

Exception Context - Register contents at the time of an exception.

§ Hwi_StackInfo

typedef struct Hwi_StackInfo Hwi_StackInfo

Structure contains Hwi stack usage info.

Used by getStackInfo() and viewGetStackInfo() functions

§ Hwi_FuncPtr

typedef void(* Hwi_FuncPtr) (uintptr_t)

Hwi create function type definition.

§ Hwi_VectorFuncPtr

typedef void(* Hwi_VectorFuncPtr) (void)

Hwi vector function type definition.

§ Hwi_ExceptionHookFuncPtr

typedef void(* Hwi_ExceptionHookFuncPtr) (Hwi_ExcContext *arg1)

Exception hook function type definition.

§ Hwi_ExcHookFunc

§ Hwi_MaskingOption

Shorthand interrupt masking options.

§ Hwi_ExcHandlerFuncPtr

typedef void(* Hwi_ExcHandlerFuncPtr) (unsigned int *arg1, unsigned int arg2)

Hwi exception handler function type definition.

Enumeration Type Documentation

§ Hwi_MaskingOption

Interrupt masking options.

Enumerator
Hwi_MaskingOption_NONE 

No interrupts are disabled (not support on cortexM devices)

Hwi_MaskingOption_ALL 

All interrupts are disabled (not support on cortexM devices)

Hwi_MaskingOption_SELF 

Only this interrupt is disabled (not support on cortexM devices)

Hwi_MaskingOption_BITMASK 

User supplies interrupt enable masks (not support on cortexM devices)

Hwi_MaskingOption_LOWER 

All current and lower priority interrupts are disabled. (default for all cortexM devices)

Function Documentation

§ Hwi_Disable()

unsigned int Hwi_Disable ( )

Globally disable interrupts.

Hwi_disable globally disables hardware interrupts and returns an opaque key indicating whether interrupts were globally enabled or disabled on entry to Hwi_disable(). The actual value of the key is target/device specific and is meant to be passed to Hwi_restore().

Call Hwi_disable before a portion of a function that needs to run without interruption. When critical processing is complete, call Hwi_restore or Hwi_enable to reenable hardware interrupts.

Servicing of interrupts that occur while interrupts are disabled is postponed until interrupts are reenabled. However, if the same type of interrupt occurs several times while interrupts are disabled, the interrupt's function is executed only once when interrupts are reenabled.

A context switch can occur when calling Hwi_enable or Hwi_restore if an enabled interrupt occurred while interrupts are disabled.

Hwi_disable may be called from main(). However, since Hwi interrupts are already disabled in main(), such a call has no effect.

Warning
The cortexM implementation of Hwi_disable() sets the basepri register to the value of Hwi_disablePriority.
If a Task switching API such as Semaphore_pend(), Semaphore_post(), Task_sleep(), Task_yield(), is invoked which results in a context switch while interrupts are disabled, an embedded call to Hwi_enable() occurs on the way to the new thread context which unconditionally re-enables interrupts. Interrupts will remain enabled until a subsequent Hwi_disable() invocation.
Return values
opaqueuint32_t key for use by Hwi_restore()

§ Hwi_Enable()

unsigned int Hwi_Enable ( )

Globally enable interrupts.

Hwi_enable()

Hwi_enable globally enables hardware interrupts and returns an opaque key indicating whether interrupts were globally enabled or disabled on entry to Hwi_enable(). The actual value of the key is target/device specific and is meant to be passed to Hwi_restore().

This function is called within BIOS_start() to enable interrupts after "main()" has been executed. Prior to BIOS_start(), interrupts are globally disabled.

Hardware interrupts are enabled unless a call to Hwi_disable() disables them.

Servicing of interrupts that occur while interrupts are disabled is postponed until interrupts are reenabled. However, if the same type of interrupt occurs several times while interrupts are disabled, the interrupt's function is executed only once when interrupts are reenabled.

A context switch can occur when calling Hwi_enable or Hwi_restore if an enabled interrupt occurred while interrupts are disabled.

Any call to Hwi_enable enables interrupts, even if Hwi_disable has been called several times.

Hwi_enable must not be called from within "main()".

§ Hwi_Restore()

void Hwi_Restore ( uint32_t  key)

restore global interrupts to the state they were in prior Hwi_disable().

Hwi_restore(key)

Globally restore interrupts.

Hwi_restore() globally restores interrupts to the state determined by the key argument provided by a previous invocation of Hwi_disable().

A context switch may occur when calling Hwi_restore if Hwi_restore() reenables interrupts and another Hwi occurred while interrupts were disabled.

The Hwi_disable() / Hwi_restore() pair may be called from within main(). However, since interrupts are globally disabled prior to main(), the call to Hwi_restore() has no effect.

  • key = enable/disable state to restore

§ Hwi_create()

Hwi_Handle Hwi_create ( int  intNum,
Hwi_FuncPtr  hwiFxn,
const Hwi_Params prms,
Error_Block eb 
)

§ Hwi_construct()

Hwi_Handle Hwi_construct ( Hwi_Struct obj,
int  intNum,
Hwi_FuncPtr  hwiFxn,
const Hwi_Params prms,
Error_Block eb 
)

§ Hwi_delete()

void Hwi_delete ( Hwi_Handle handle)

§ Hwi_destruct()

void Hwi_destruct ( Hwi_Struct obj)

§ Hwi_getStackInfo()

bool Hwi_getStackInfo ( Hwi_StackInfo stkInfo,
bool  computeStackDepth 
)

Get Hwi stack usage Info.

getStackInfo returns the Hwi stack usage info to its calling function by filling stack base address, stack size and stack peak fields in the Hwi_StackInfo structure.

getStackInfo accepts two arguments, a pointer to a structure of type Hwi_StackInfo and a boolean. If the boolean is set to true, the function computes the stack depth and fills the stack peak field in the StackInfo structure. If a stack overflow is detected, the stack depth is not computed. If the boolean is set to false, the function only checks for a stack overflow.

The isr stack is always checked for an overflow and a boolean is returned to indicate whether an overflow occured.

Below is an example of calling getStackInfo() API:

volatile bool swiStackOverflow = false;
void swi0Fxn(uintptr_t arg1, uintptr_t arg2)
{
Hwi_StackInfo stkInfo;
// Request stack depth
swiStackOverflow = Hwi_getStackInfo(&stkInfo, true);
// Alternately, we can omit the request for stack depth and
// request only the stack base and stack size (the check for
// stack overflow is always performed):
//
swiStackOverflow = Hwi_getStackInfo(&stkInfo, false);
if (swiStackOverflow) {
// isr Stack Overflow detected
}
}
void idleTask()
{
Swi_post(swi0);
}
int main(int argc, char* argv[])
{
swi0 = Swi_create(swi0Fxn, NULL, NULL);
return (0);
}
Parameters
stkInfopointer to stack info structure
computeStackDepthdecides whether to compute stack depth
Return values
booleanto indicate a stack overflow

§ Hwi_post()

void Hwi_post ( unsigned int  intNum)

Generate an interrupt for test purposes.

Parameters
intNumID of interrupt to generate

§ Hwi_disableInterrupt()

unsigned int Hwi_disableInterrupt ( unsigned int  intNum)

Disable a specific interrupt.

Disable a specific interrupt identified by an interrupt number.

Parameters
intNuminterrupt number to disable
Return values
keyto restore previous enable/disable state

§ Hwi_enableInterrupt()

unsigned int Hwi_enableInterrupt ( unsigned int  intNum)

Enable a specific interrupt.

Enables a specific interrupt identified by an interrupt number.

Parameters
intNuminterrupt number to enable
Return values
keyto restore previous enable/disable state

§ Hwi_restoreInterrupt()

void Hwi_restoreInterrupt ( unsigned int  intNum,
unsigned int  key 
)

Restore a specific interrupt's enabled/disabled state.

Restores a specific interrupt identified by an interrupt number. restoreInterrupt is generally used to restore an interrupt to its state before Hwi_disableInterrupt or Hwi_enableInterrupt was invoked.

Parameters
intNuminterrupt number to restore
keykey returned from enableInt or disableInt

§ Hwi_clearInterrupt()

void Hwi_clearInterrupt ( unsigned int  intNum)

Clear a specific interrupt.

Clears a specific interrupt's pending status. The implementation is family- specific.

Parameters
intNuminterrupt number to clear

§ Hwi_getFunc()

Hwi_FuncPtr Hwi_getFunc ( Hwi_Handle  hwi,
uintptr_t *  arg 
)

Get Hwi function and arg.

Parameters
hwiHwi handle
argpointer for returning hwi's ISR function argument
Return values
hwi'sISR function

§ Hwi_setFunc()

void Hwi_setFunc ( Hwi_Handle  hwi,
Hwi_FuncPtr  fxn,
uintptr_t  arg 
)

Overwrite Hwi function and arg.

Replaces a Hwi object's hwiFxn function originally provided in Hwi_create.

Precondition
Hwi_setFunc() is not thread safe. This means that the new value for for 'fxn' may be temporarily paired with the previous value for 'arg' if pre-emption occurs within the execution of Hwi_setFunc().

To guard against this condition, surround the Hwi_setFunc() call with calls to Hwi_disable() and Hwi_restore():

key = Hwi_disable();
Hwi_setFunc(newFunc, newArg);
Hwi_restore(key);
Parameters
hwiHwi handle
fxnpointer to ISR function
argargument to ISR function

§ Hwi_getHookContext()

void* Hwi_getHookContext ( Hwi_Handle  hwi,
int  id 
)

Get hook instance's context for a Hwi.

Parameters
hwiHwi handle
idhook id
Return values
hookinstance's context for hwi

§ Hwi_setHookContext()

void Hwi_setHookContext ( Hwi_Handle  hwi,
int  id,
void *  hookContext 
)

Set hook instance's context for a Hwi.

Parameters
hwiHwi handle
idhook id
hookContextvalue to write to context

§ Hwi_getIrp()

uintptr_t Hwi_getIrp ( Hwi_Handle  hwi)

Get address of interrupted instruction.

Parameters
hwiHwi handle
Return values
mostcurrent IRP of a Hwi

§ Hwi_plug()

void Hwi_plug ( unsigned int  intNum,
void *  fxn 
)

Plug a non dispatched interrupt vector with an ISR address.

Used internally by Hwi_create() and Hwi_construct().

This API is provided for external use primarily to allow users to plug the NMI vector (interrupt #2) at runtime.

Note
Interrupt vectors plugged using Hwi_plug() are NOT managed by the Hwi interrupt dispatcher. Consequently, it is not safe to call SYS/BIOS APIs from within these ISRs.
Parameters
intNuminterrupt number
fxnpointer to ISR function

§ Hwi_getHandle()

Hwi_Handle Hwi_getHandle ( unsigned int  intNum)

Returns Hwi_handle associated with intNum.

Parameters
intNuminterrupt number
Return values
Hwihandle

§ Hwi_setPriority()

void Hwi_setPriority ( unsigned int  intNum,
unsigned int  priority 
)

Set an interrupt's relative priority.

Valid priorities are 0 - 255. 0 is highest priority.

Warning
Setting the priority of a dispatched Hwi to a value higher than Hwi_disablePriority will make it become non-maskable by Hwi_disable. The behavior of your application after that will be unpredictable and will likely yield catastrophic results!
Parameters
intNumID of interrupt
prioritypriority

§ Hwi_excSetBuffers()

void Hwi_excSetBuffers ( void *  excContextBuffer,
void *  excStackBuffer 
)

Set the exception context and stack buffer pointers.

Parameters
excContextBufferAddress to place ExcContext
excStackBufferAddress to place ExcStack

§ Hwi_reconfig()

void Hwi_reconfig ( Hwi_Handle  hwi,
Hwi_FuncPtr  fxn,
const Hwi_Params params 
)

Reconfigure a dispatched interrupt.

Parameters
hwiHwi handle
fxnHwi function
paramspointer to Hwi params structure

§ Hwi_Params_init()

void Hwi_Params_init ( Hwi_Params prms)

§ Hwi_Object_first()

Hwi_Handle Hwi_Object_first ( void  )

§ Hwi_Object_next()

Hwi_Handle Hwi_Object_next ( Hwi_Object obj)

Variable Documentation

§ Hwi_nvic

volatile Hwi_NVIC Hwi_nvic

Physical Nested Vectored Interrupt Controller Device. short name is "Hwi_nvic" long name is "ti_sysbios_family_arm_m3_Hwi_nvic".

§ Hwi_NUM_INTERRUPTS

const int Hwi_NUM_INTERRUPTS

The Cortex M0 NVIC supports up to 256 interrupts/exceptions.

The actual number supported is device specific and provided by the catalog device specification.

§ Hwi_NUM_PRIORITIES

const int Hwi_NUM_PRIORITIES

The Cortex M0 NVIC supports up to 256 interrupt priorities.

The actual number supported is device specific and provided by the catalog device specification.

§ Hwi_excHookFunc

const Hwi_ExcHookFunc Hwi_excHookFunc

User Exception hook function.

Called just after the exception context has been initialized.

This function will be run on the ISR stack.

This function must run to completion.

It is called without any Task or Swi scheduling protection and therefore can not call any functions that may cause a Swi or Task scheduling operation (Swi_post(), Semaphore_post(), Event_post(), etc).

§ Hwi_disablePriority

const unsigned int Hwi_disablePriority

The priority that BASEPRI is set to by Hwi_disable().

All interrupts configured with equal or less priority (equal or higher number) than disablePriority are disabled by Hwi_disable. Interrupts configured with higher priority (smaller number) than Hwi.disablePriority are non-maskable (ie zero-latency).

The default setting is the second highest interrupt priority defined for the device (typically '0x20' for devices which support 8 priority values). This results in priority 0 (and all other values in the same priority group, ie 0x00 thru 0x1f) being the zero-latency, non-maskable interrupt priority. All other priorities are disabled with Hwi_disable().

The constant Hwi_disablePriority is configured within the app.syscfg file using the following syntax:

const Hwi = scripting.addModule("/family/arm/v6m/Hwi");
Hwi.disablePriority = 0x20;

§ Hwi_priGroup

const unsigned int Hwi_priGroup

The PRIGROUP setting. Default is 0.

This value will be written to the PRIGROUP field within the NVIC's Application Interrupt and Reset Control Register (Hwi_nvic.AIRCR). It defines how the 8 bit priority values are interpreted by the hardware.

Valid settings are 0-7.

The default setting of 0 causes bits 7-1 of an interrupt's priority value to be used as pre-emption priority, while bit 0 is used to determine which of two simultaneous interrupts with the same pre-emption priority will be serviced first.

For most TI MCU devices, this means that each of the 8 supported priority values are unique pre-emption priorities and are not subdivided into priority groups.

See the "AIRCR" register description in the Arm "Cortex M4 Devices Generic User Guide" for more details regarding priority groups.

The constant Hwi_priGroup is configured within the app.syscfg file using the following syntax:

const Hwi = scripting.addModule("/family/arm/v6m/Hwi");
Hwi.priGroup = 0;

§ Hwi_numSparseInterrupts

const unsigned int Hwi_numSparseInterrupts

If Hwi.dispatchTableSize is initialized by the user then Hwi.numSparseInterrupts is set to the value of Hwi.dispatchTableSize.

If Hwi.dispatchTableSize is NOT set by the user, the normal intNum-indexed Hwi dispatchTable mechanism is used by the dispatcher to find the corresponding Hwi object.

If Hwi.dispatchTableSize is set by the user, then a RAM-based fixed sized interrupt jump table is generated that contains a repeating pattern of the following 3 word assembly code snippets:

hwiX: ldr r3, hwiObjectX ldr pc, ti_sysbios_family_arm_v6m_Hwi_dispatch__I hwiObjectX: .word 0 hwiY: ldr r3, hwiObjectY ldr pc, ti_sysbios_family_arm_v6m_Hwi_dispatch__I hwiObjectY: .word 0

Each dispatched interrupt vector is then initialized to point to one of these tuples, and the address of the corresponding Hwi object is written into the hwiObjectX field.

The low level assembly code in Hwi_dispatch__I preserves the value of r3 when it calls Hwi_dispatchC(), which results in the Hwi object being passed as the arg3.

Depending on the boolean value of Hwi_numSparseInterrupts, the dispatcher either uses the value passed in arg3 as the Hwi object, or uses intNum to index into the standard dispatchTable to fetch the Hwi object.

© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale