![]() |
![]() |
TI Easylink API
4.30.00.11
|
Structure for EasyLink_init() containing pointers to all the commands necessary to define an RF setting. More...
#include <EasyLink.h>
Public Attributes | |
EasyLink_PhyType | EasyLink_phyType |
RF_Mode * | RF_pProp |
Pointer to RF Mode Command. | |
union { | |
rfc_CMD_PROP_RADIO_DIV_SETUP_t * RF_pCmdPropRadioDivSetup | |
rfc_CMD_PROP_RADIO_SETUP_t * RF_pCmdPropRadioSetup | |
} | RF_uCmdPropRadio |
rfc_CMD_FS_t * | RF_pCmdFs |
Pointer to a frequency setup command. | |
rfc_CMD_PROP_TX_t * | RF_pCmdPropTx |
Pointer to a RF TX command. | |
rfc_CMD_PROP_TX_ADV_t * | RF_pCmdPropTxAdv |
rfc_CMD_PROP_RX_ADV_t * | RF_pCmdPropRxAdv |
RF_TxPowerTable_Entry * | RF_pTxPowerTable |
Pointer to a Tx power table. | |
uint8_t | RF_txPowerTableSize |
Tx power table size. | |
Structure for EasyLink_init() containing pointers to all the commands necessary to define an RF setting.
EasyLink_PhyType EasyLink_RfSetting::EasyLink_phyType |
The PHY type that this RF setting defines
rfc_CMD_PROP_RX_ADV_t* EasyLink_RfSetting::RF_pCmdPropRxAdv |
Pointer to an advanced RF RX command
rfc_CMD_PROP_TX_ADV_t* EasyLink_RfSetting::RF_pCmdPropTxAdv |
Pointer to an advanced RF TX command
union { ... } EasyLink_RfSetting::RF_uCmdPropRadio |
Union containing either a pointer to a divided radio setup command or a pointer to a radio setup command