TI Easylink API
4.30.00.11
|
Files | |
file | EasyLink.h |
EasyLink RF API for CC13xx/CC26xx family. | |
Classes | |
struct | EasyLink_Params |
Structure for EasyLink_init() and EasyLink_Params_init() More... | |
struct | EasyLink_RfSetting |
Structure for EasyLink_init() containing pointers to all the commands necessary to define an RF setting. More... | |
struct | EasyLink_TxPacket |
Structure for the TX Packet. More... | |
struct | EasyLink_RxPacket |
Structure for the RX'ed Packet. More... | |
Macros | |
#define | EASYLINK_API_VERSION "EasyLink-v4.30.00" |
EasyLink API Version. | |
#define | EASYLINK_MAX_ADDR_SIZE 8 |
defines the Tx/Rx Max Address Size | |
#define | EASYLINK_MAX_ADDR_FILTERS 8 |
defines the Max number of Rx Address filters | |
#define | EASYLINK_WHITENING_MODE 2 |
defines the whitening mode | |
#define | EasyLink_RadioTime_To_ms(radioTime) (radioTime / (4000000/1000)) |
macro to convert from Radio Time Ticks to ms | |
#define | EasyLink_ms_To_RadioTime(ms) (ms*(4000000/1000)) |
macro to convert from ms to Radio Time Ticks | |
#define | EasyLink_us_To_RadioTime(us) (us*(4000000/1000000)) |
macro to convert from us to Radio Time Ticks | |
#define | EasyLink_PHY_CUSTOM 0 |
Phy Type defines so we can use them in checks. | |
#define | EasyLink_PHY_50KBPS2GFSK 1 |
#define | EasyLink_PHY_625BPSLRM 2 |
#define | EasyLink_PHY_2_4_200KBPS2GFSK 3 |
#define | EasyLink_PHY_5KBPSSLLR 4 |
#define | EasyLink_PHY_2_4_100KBPS2GFSK 5 |
#define | EasyLink_PHY_2_4_250KBPS2GFSK 6 |
#define | EasyLink_PHY_200KBPS2GFSK 7 |
#define | EASYLINK_DEFAULT_ADDR {0xAA} |
Defines the address that will accompany each packet sent from this device when EASYLINK_USE_DEFAULT_ADDR is true. It can also be thought of as this device's own address. Organized in little endian format (e.g.an address of 0xABCD should be defined as {0xCD,0xAB}) | |
#define | EASYLINK_USE_DEFAULT_ADDR false |
When false, the Easylink stack expects the application to provide an accompanying address for each EasyLink_TxPacket passed to the EasyLink_transmit(), EasyLink_transmitAsync(), and EasyLink_transmitCcaAsync() APIs. Otherwise, these APIs will use the address defined in EASYLINK_DEFAULT_ADDR. | |
#define | EASYLINK_MAX_DATA_LENGTH 128 |
Defines the largest Tx/Rx payload that the interface can support. | |
#define | EASYLINK_ADDR_SIZE 1 |
Defines the default address size for rx and tx operations. | |
#define | EASYLINK_ENABLE_ADDR_FILTERING true |
Enables of disables address filtering by default. | |
#define | EASYLINK_NUM_ADDR_FILTER 1 |
The table for setting the Rx Address Filters. | |
#define | EASYLINK_ADDR_FILTER_TABLE {0xAA} |
The table for setting the Rx Address Filters. | |
#define | EASYLINK_IDLE_TIMEOUT EasyLink_ms_To_RadioTime(1) |
Defines the time for the radio to return to idle after inactivity. | |
#define | EASYLINK_ENABLE_MULTI_CLIENT false |
Enables or disables the application to use multiple RF clients. | |
#define | EASYLINK_ASYNC_RX_TIMEOUT EasyLink_ms_To_RadioTime(0) |
Defines the relative time from async RX start to timeout. A value of 0 means no timeout. | |
#define | EASYLINK_MIN_CCA_BACKOFF_WINDOW 5 |
Minimum CCA back-off window in units of EASYLINK_CCA_BACKOFF_TIMEUNITS, as a power of 2. | |
#define | EASYLINK_MAX_CCA_BACKOFF_WINDOW 8 |
Maximum CCA back-off window in units of EASYLINK_CCA_BACKOFF_TIMEUNITS, as a power of 2. | |
#define | EASYLINK_CCA_BACKOFF_TIMEUNITS 250 |
The back-off time units in microseconds. | |
#define | EASYLINK_CS_RSSI_THRESHOLD_DBM -80 |
RSSI threshold for Clear Channel Assessment (CCA) | |
#define | EASYLINK_CHANNEL_IDLE_TIME_US 5000 |
Time for which the channel RSSI must remain below the specified threshold for the channel to be considered idle. | |
#define | EASYLINK_PARAM_CONFIG |
EasyLink default parameter configuration. More... | |
Typedefs | |
typedef uint32_t(* | EasyLink_GetRandomNumber) (void) |
EasyLink 32-bit Random number generator function type used in the clear channel assessment algorithm. | |
typedef void(* | EasyLink_ReceiveCb) (EasyLink_RxPacket *rxPacket, EasyLink_Status status) |
EasyLink Callback function type for Received packet, registered with EasyLink_ReceiveAsync() | |
typedef void(* | EasyLink_TxDoneCb) (EasyLink_Status status) |
EasyLink Callback function type for Tx Done registered with EasyLink_TransmitAsync() | |
Functions | |
void | EasyLink_Params_init (EasyLink_Params *params) |
Initializes the radio with specified Phy settings and RF client events. More... | |
EasyLink_Status | EasyLink_init (EasyLink_Params *params) |
Initializes the radio with specified Phy settings, CCA random number generator, and RF client events. More... | |
EasyLink_Status | EasyLink_getAbsTime (uint32_t *pui32AbsTime) |
Gets the absolute radio time. More... | |
EasyLink_Status | EasyLink_getRssi (int8_t *pi8Rssi) |
Gets the RSSI value of an ongoing Radio Operation. More... | |
EasyLink_Status | EasyLink_transmit (EasyLink_TxPacket *txPacket) |
Sends a Packet with blocking call. More... | |
EasyLink_Status | EasyLink_transmitAsync (EasyLink_TxPacket *txPacket, EasyLink_TxDoneCb cb) |
Sends a Packet with non blocking call. More... | |
EasyLink_Status | EasyLink_transmitCcaAsync (EasyLink_TxPacket *txPacket, EasyLink_TxDoneCb cb) |
Sends a Packet with non blocking call if the channel is idle. More... | |
EasyLink_Status | EasyLink_receive (EasyLink_RxPacket *rxPacket) |
Blocking call that waits for an Rx Packet. More... | |
EasyLink_Status | EasyLink_receiveAsync (EasyLink_ReceiveCb cb, uint32_t absTime) |
Enables Asynchronous Packet Rx with non blocking call. More... | |
EasyLink_Status | EasyLink_abort (void) |
Abort a previously call Async Tx/Rx. More... | |
EasyLink_Status | EasyLink_setFrequency (uint32_t ui32Frequency) |
Sets the Frequency. More... | |
uint32_t | EasyLink_getFrequency (void) |
Gets the Frequency. More... | |
EasyLink_Status | EasyLink_enableRxAddrFilter (uint8_t *pui8AddrFilterTable, uint8_t ui8AddrSize, uint8_t ui8NumAddrs) |
Enables the address filter. More... | |
EasyLink_Status | EasyLink_getIeeeAddr (uint8_t *ieeeAddr) |
Gets the IEEE address. More... | |
EasyLink_Status | EasyLink_setRfPower (int8_t i8TxPowerDbm) |
Sets the TX Power. More... | |
EasyLink_Status | EasyLink_getRfPower (int8_t *pi8TxPowerDbm) |
Gets the TX Power. More... | |
EasyLink_Status | EasyLink_setCtrl (EasyLink_CtrlOption Ctrl, uint32_t ui32Value) |
Sets advanced configuration options. More... | |
EasyLink_Status | EasyLink_getCtrl (EasyLink_CtrlOption Ctrl, uint32_t *pui32Value) |
Gets advanced configuration options. More... | |
Variables | |
EasyLink_RfSetting | EasyLink_supportedPhys [] |
Array containing all the supported EasyLink_rfSettings. | |
const uint8_t | EasyLink_numSupportedPhys |
Size of the EasyLink_supportedPhys array. | |
#define EASYLINK_PARAM_CONFIG |
EasyLink default parameter configuration.
enum EasyLink_Activity |
Activity table.
+-----------—+-----------------------------------—+ | Activity | Priority | +-----------—+---------—+---------—+---------—+ | | Normal | High | Urgent | | TX | 0X03090000 | 0X03090001 | 0X03090002 | | RX | 0X03070000 | 0X03070001 | 0X03070002 | +-----------—+-----------------------------------—+
Enumerator | |
---|---|
EasyLink_Activity_Tx | Activity code for the Tx operation. |
EasyLink_Activity_Rx | Activity code for the Rx operation. |
enum EasyLink_CtrlOption |
Advance configuration options.
Enumerator | |
---|---|
EasyLink_Ctrl_AddSize | Set the number of bytes in Addr for both Addr Filter and Tx/Rx operations |
EasyLink_Ctrl_Idle_TimeOut | Set a timeout value for inactivity on the radio, i.e. if the radio stays idle for this amount of time it is automatically powered down |
EasyLink_Ctrl_MultiClient_Mode | Set Multiclient mode for application that will use multiple RF clients. Must be set before calling EasyLink_init(). |
EasyLink_Ctrl_AsyncRx_TimeOut | Relative time in ticks from Async Rx start to TimeOut. A value of 0 means no timeout |
EasyLink_Ctrl_Cmd_Priority | Set the command priority with a value from EasyLink_Priority |
EasyLink_Ctrl_Test_Tone | Enable/Disable Test mode for Tone. |
EasyLink_Ctrl_Test_Signal | Enable/Disable Test mode for Signal. |
EasyLink_Ctrl_Rx_Test_Tone | Enable/Disable Rx Test mode for Tone. |
enum EasyLink_PhyType |
Phy Type passed to EasyLink_init()
enum EasyLink_Status |
EasyLink Status and error codes.
EasyLink_Status EasyLink_abort | ( | void | ) |
Abort a previously call Async Tx/Rx.
This function is a blocking call to abort a previous Async Tx/Rx
EasyLink_Status EasyLink_enableRxAddrFilter | ( | uint8_t * | pui8AddrFilterTable, |
uint8_t | ui8AddrSize, | ||
uint8_t | ui8NumAddrs | ||
) |
Enables the address filter.
This function enables the address filter to filter out address that are not in the address table provided.
pui8AddrFilterTable | A uint8 pointer to a variable size 2d array containing the addresses to filter on. |
ui8AddrSize | The size of the address elements |
ui8NumAddrs | The number of address elements |
EasyLink_Status EasyLink_getAbsTime | ( | uint32_t * | pui32AbsTime | ) |
Gets the absolute radio time.
This function returns the absolute radio time and can be used for monitoring or Tx/Rx events using the EasyLink_TxPacket and EasyLink_RxPacket::absTime field.
pui32AbsTime | Pointer to return the signed RSSI value (dBm) |
EasyLink_Status EasyLink_getCtrl | ( | EasyLink_CtrlOption | Ctrl, |
uint32_t * | pui32Value | ||
) |
Gets advanced configuration options.
This function allows getting some of the advanced configuration options
Ctrl | The control option to get |
pui32Value | Pointer to return the control option value |
uint32_t EasyLink_getFrequency | ( | void | ) |
Gets the Frequency.
This function gets Frequency in units of kHz. This function will return the value set in the Frequency Synthesizer, and may not be the same as set using EasyLink_setFrequency(). Note that this value does not include any offsets for deviations due to factors such as temperature and hence this API should not be used to get an accurate measure of frequency.
EasyLink_Status EasyLink_getIeeeAddr | ( | uint8_t * | ieeeAddr | ) |
Gets the IEEE address.
This function gets the IEEE address
ieeeAddr | pointer to an 8 element byte array to write the IEEE address to. |
EasyLink_Status EasyLink_getRfPower | ( | int8_t * | pi8TxPowerDbm | ) |
Gets the TX Power.
This function gets the Tx Power in dBm, values ranging from -10 to 14 dBm should be expect
pi8TxPowerDbm | Pointer to return the transmission power value (dBm) |
EasyLink_Status EasyLink_getRssi | ( | int8_t * | pi8Rssi | ) |
Gets the RSSI value of an ongoing Radio Operation.
This function returns the RSSI from an ongoing receiver radio operation. It is useful in receiver test modes to detect the presence of both modulated and unmodulated carrier waves
pi8Rssi | Pointer to return the signed RSSI value (dBm) |
EasyLink_Status EasyLink_init | ( | EasyLink_Params * | params | ) |
Initializes the radio with specified Phy settings, CCA random number generator, and RF client events.
This function configures the radio phy settings. If the ui32ModType is EasyLink_Phy_Custom then the configuration is taken from srf_settings.h. If a specific phy configuration is required (and not supported by any of the defined Phy types in EasyLink_PhyType then you can cut and past the RF setting from the SmartRF Studio code export tool. This will copy and use the RF_prop, RF_cmdPropRadioDivSetup and RF_cmdFs commands, as well as the Sync word from the RF_cmdPropTx and RF_cmdPropRx commands. The function configures the callback for client events. The client events that trigger the callback are set using the nClientEventMask type in EasyLink_Params. A pointer to the desired callback should be provided to the pClientEventCb type of the EasyLink_Params structure.
params | The descriptor for the Phy mode, random number generator, and event callback settings |
void EasyLink_Params_init | ( | EasyLink_Params * | params | ) |
Initializes the radio with specified Phy settings and RF client events.
This function configures the radio phy settings. If the ui32ModType is EasyLink_Phy_Custom then the configuration is taken from srf_settings.h. If a specific phy configuration is required (and not supported by any of the defined Phy types in EasyLink_PhyType then you can cut and past the RF setting from the SmartRF Studio code export tool. This will copy and use the RF_prop, RF_cmdPropRadioDivSetup and RF_cmdFs commands, as well as the Sync word from the RF_cmdPropTx and RF_cmdPropRx commands. The function configures the callback for client events. The client events that trigger the callback are set using the nClientEventMask type in EasyLink_Params. A pointer to the desired callback should be provided to the pClientEventCb type of the EasyLink_Params structure.
params | The descriptor for the Phy mode and event callback settings |
Default values are: ui32ModType = EasyLink_Phy_50kbps2gfsk RF_ClientCallback = NULL RF_ClientEventMask = 0 pGrnFxn = (EasyLink_GetRandomNumber)rand
EasyLink_Status EasyLink_receive | ( | EasyLink_RxPacket * | rxPacket | ) |
Blocking call that waits for an Rx Packet.
This function is a blocking call to wait for an Rx packet.
rxPacket | The descriptor for the packet to be Rx'ed. |
EasyLink_Status EasyLink_receiveAsync | ( | EasyLink_ReceiveCb | cb, |
uint32_t | absTime | ||
) |
Enables Asynchronous Packet Rx with non blocking call.
This function is a non blocking call to Rx a packet. The Rx is turned on and the Callback is called once a packet is received. The Rx will timeout if EasyLink_Ctrl_AsyncRx_TimeOut ctrl message is used to set the timeout to something other than 0.
cb | The rx function pointer. |
absTime | Start time of Rx (0: now !0: absolute radio time to start Rx) |
EasyLink_Status EasyLink_setCtrl | ( | EasyLink_CtrlOption | Ctrl, |
uint32_t | ui32Value | ||
) |
Sets advanced configuration options.
This function allows setting some of the advanced configuration options
Ctrl | The control option to be set |
ui32Value | The value to set the control option to |
EasyLink_Status EasyLink_setFrequency | ( | uint32_t | ui32Frequency | ) |
Sets the Frequency.
This function set the radio to the specified frequency. Note that this will be rounded to the nearest frequency supported by the Frequency Synthesizer.
ui32Frequency | Frequency in units of kHz |
EasyLink_Status EasyLink_setRfPower | ( | int8_t | i8TxPowerDbm | ) |
Sets the TX Power.
This function sets the Tx Power
i8TxPowerDbm | The Tx power in dBm's to be set.
|
EasyLink_Status EasyLink_transmit | ( | EasyLink_TxPacket * | txPacket | ) |
Sends a Packet with blocking call.
This function is a blocking call to send a packet. If the Tx is successfully scheduled then the function will block until the Tx is complete.
txPacket | The descriptor for the packet to be Tx'ed. |
EasyLink_Status EasyLink_transmitAsync | ( | EasyLink_TxPacket * | txPacket, |
EasyLink_TxDoneCb | cb | ||
) |
Sends a Packet with non blocking call.
This function is a non blocking call to send a packet. If the Tx is successfully scheduled then the callback will be call once the Tx is complete.
txPacket | The descriptor for the packet to be Tx'ed. |
cb | The tx done function pointer. |
EasyLink_Status EasyLink_transmitCcaAsync | ( | EasyLink_TxPacket * | txPacket, |
EasyLink_TxDoneCb | cb | ||
) |
Sends a Packet with non blocking call if the channel is idle.
This function is a non blocking call to send a packet. It will check for a clear channel prior to transmission. If the channel is busy it will backoff for a random period, in time units of EASYLINK_CCA_BACKOFF_TIMEUNITS, before reassessing. It does this a certain number (EASYLINK_MAX_CCA_BACKOFF_WINDOW - EASYLINK_MIN_CCA_BACKOFF_WINDOW) of times before quitting unsuccessfully and running to the callback. If the Tx is successfully scheduled then the callback will be called once the Tx is complete.
txPacket | The descriptor for the packet to be Tx'ed. |
cb | The tx done function pointer. |