rflib
Data Fields
rfc_ieeeCoexGlobalEnable_s Struct Reference

#include <rf_ieee_coex.h>

Data Fields

uint32_t __dummy0
 
uint32_t __dummy1
 
uint32_t __dummy2
 
uint32_t __dummy3
 
uint32_t __dummy4
 
uint32_t __dummy5
 
uint32_t __dummy6
 
uint32_t __dummy7
 
uint32_t __dummy8
 
uint32_t __dummy9
 
uint32_t __dummy10
 
uint32_t __dummy11
 
uint32_t __dummy12
 
uint32_t __dummy13
 
uint32_t __dummy14
 
uint32_t __dummy15
 
uint32_t __dummy16
 
uint32_t __dummy17
 
uint32_t __dummy18
 
uint32_t __dummy19
 
uint32_t __dummy20
 
uint32_t __dummy21
 
uint32_t __dummy22
 
uint32_t __dummy23
 
uint32_t __dummy24
 
uint32_t __dummy25
 
uint32_t __dummy26
 
uint32_t __dummy27
 
uint32_t __dummy28
 
uint32_t __dummy29
 
uint32_t __dummy30
 
uint32_t __dummy31
 
uint32_t __dummy32
 
uint32_t __dummy33
 
uint32_t __dummy34
 
uint16_t __dummy35
 
uint8_t __dummy36
 
uint8_t coExGlobalEnable
 0 = CoEx features disabled. All other values = CoEx enabled. More...
 

Field Documentation

§ __dummy0

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy0

§ __dummy1

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy1

§ __dummy2

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy2

§ __dummy3

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy3

§ __dummy4

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy4

§ __dummy5

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy5

§ __dummy6

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy6

§ __dummy7

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy7

§ __dummy8

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy8

§ __dummy9

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy9

§ __dummy10

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy10

§ __dummy11

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy11

§ __dummy12

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy12

§ __dummy13

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy13

§ __dummy14

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy14

§ __dummy15

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy15

§ __dummy16

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy16

§ __dummy17

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy17

§ __dummy18

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy18

§ __dummy19

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy19

§ __dummy20

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy20

§ __dummy21

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy21

§ __dummy22

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy22

§ __dummy23

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy23

§ __dummy24

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy24

§ __dummy25

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy25

§ __dummy26

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy26

§ __dummy27

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy27

§ __dummy28

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy28

§ __dummy29

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy29

§ __dummy30

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy30

§ __dummy31

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy31

§ __dummy32

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy32

§ __dummy33

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy33

§ __dummy34

uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy34

§ __dummy35

uint16_t rfc_ieeeCoexGlobalEnable_s::__dummy35

§ __dummy36

uint8_t rfc_ieeeCoexGlobalEnable_s::__dummy36

§ coExGlobalEnable

uint8_t rfc_ieeeCoexGlobalEnable_s::coExGlobalEnable

0 = CoEx features disabled. All other values = CoEx enabled.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale