TI-15.4 Stack API
3.40.00.09
|
#include <api_mac.h>
Data Fields | |
ApiMac_sAddr_t | dstAddr |
uint16_t | dstPanId |
ApiMac_addrType_t | srcAddrMode |
uint8_t | msduHandle |
ApiMac_txOptions_t | txOptions |
uint8_t | channel |
uint8_t | power |
uint8_t * | pIEList |
uint16_t | payloadIELen |
ApiMac_fhDispatchType_t | fhProtoDispatch |
uint32_t | includeFhIEs |
ApiMac_sData_t | msdu |
ApiMac_sec_t | sec |
uint8_t | gpOffset |
uint8_t | gpDuration |
MCPS data request type
ApiMac_sAddr_t _apimac_mcpsdatareq::dstAddr |
The address of the destination device
uint16_t _apimac_mcpsdatareq::dstPanId |
The PAN ID of the destination device
ApiMac_addrType_t _apimac_mcpsdatareq::srcAddrMode |
The source address mode
uint8_t _apimac_mcpsdatareq::msduHandle |
Application-defined handle value associated with this data request
ApiMac_txOptions_t _apimac_mcpsdatareq::txOptions |
TX options bit mask
uint8_t _apimac_mcpsdatareq::channel |
Transmit the data frame on this channel
uint8_t _apimac_mcpsdatareq::power |
Transmit the data frame at this power level
uint8_t* _apimac_mcpsdatareq::pIEList |
pointer to the payload IE list, excluding termination IEs
uint16_t _apimac_mcpsdatareq::payloadIELen |
length of the payload IE
ApiMac_fhDispatchType_t _apimac_mcpsdatareq::fhProtoDispatch |
Freq hopping Protocol Dispatch - RESERVED for future use, should be cleared.
uint32_t _apimac_mcpsdatareq::includeFhIEs |
Bitmap indicates which FH IE's need to be included
ApiMac_sData_t _apimac_mcpsdatareq::msdu |
Data buffer
ApiMac_sec_t _apimac_mcpsdatareq::sec |
Security Parameters
uint8_t _apimac_mcpsdatareq::gpOffset |
Transmit Delay for Green Power
uint8_t _apimac_mcpsdatareq::gpDuration |
Transmit Window for Green Power