TI-15.4 Stack API
3.40.00.09
|
#include <api_mac.h>
Data Fields | |
ApiMac_sAddr_t | srcAddr |
ApiMac_sAddr_t | dstAddr |
uint32_t | timestamp |
uint16_t | timestamp2 |
uint16_t | srcPanId |
uint16_t | dstPanId |
uint8_t | mpduLinkQuality |
uint8_t | correlation |
int8_t | rssi |
uint8_t | dsn |
uint16_t | payloadIeLen |
uint8_t * | pPayloadIE |
ApiMac_fhFrameType_t | fhFrameType |
ApiMac_fhDispatchType_t | fhProtoDispatch |
uint32_t | frameCntr |
ApiMac_sec_t | sec |
ApiMac_sData_t | msdu |
MCPS data indication type
ApiMac_sAddr_t _apimac_mcpsdataind::srcAddr |
The address of the sending device
ApiMac_sAddr_t _apimac_mcpsdataind::dstAddr |
The address of the destination device
uint32_t _apimac_mcpsdataind::timestamp |
The time, in backoffs, at which the data were received
uint16_t _apimac_mcpsdataind::timestamp2 |
The time, in internal MAC timer units, at which the data were received
uint16_t _apimac_mcpsdataind::srcPanId |
The PAN ID of the sending device
uint16_t _apimac_mcpsdataind::dstPanId |
The PAN ID of the destination device
uint8_t _apimac_mcpsdataind::mpduLinkQuality |
The link quality of the received data frame
uint8_t _apimac_mcpsdataind::correlation |
The raw correlation value of the received data frame
int8_t _apimac_mcpsdataind::rssi |
The received RF power in units dBm
uint8_t _apimac_mcpsdataind::dsn |
The data sequence number of the received frame
uint16_t _apimac_mcpsdataind::payloadIeLen |
length of the payload IE buffer (pPayloadIE)
uint8_t* _apimac_mcpsdataind::pPayloadIE |
Pointer to the start of payload IEs
ApiMac_fhFrameType_t _apimac_mcpsdataind::fhFrameType |
Frequency Hopping Frame Type
ApiMac_fhDispatchType_t _apimac_mcpsdataind::fhProtoDispatch |
Frequency hopping protocol dispatch - RESERVED for future use.
uint32_t _apimac_mcpsdataind::frameCntr |
Frame counter value of the received data frame (if used)
ApiMac_sec_t _apimac_mcpsdataind::sec |
Security Parameters
ApiMac_sData_t _apimac_mcpsdataind::msdu |
Data Buffer