Data Fields
ECDHCC26X1_Object Struct Reference

ECDHCC26X1 Object. More...

#include <ECDHCC26X1.h>

Collaboration diagram for ECDHCC26X1_Object:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
ECDH_CallbackFxn callbackFxn
 
ECDH_ReturnBehavior returnBehavior
 
ECC_State eccState
 
uint32_t eccWorkZone [171]
 

Detailed Description

ECDHCC26X1 Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool ECDHCC26X1_Object::isOpen

§ callbackFxn

ECDH_CallbackFxn ECDHCC26X1_Object::callbackFxn

§ returnBehavior

ECDH_ReturnBehavior ECDHCC26X1_Object::returnBehavior

§ eccState

ECC_State ECDHCC26X1_Object::eccState

§ eccWorkZone

uint32_t ECDHCC26X1_Object::eccWorkZone[171]

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale