ECDHCC26X1.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2020, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
52 #ifndef ti_drivers_ecdh_ECDHCC26X1__include
53 #define ti_drivers_ecdh_ECDHCC26X1__include
54 
55 #include <stdint.h>
56 #include <stdbool.h>
57 
58 #include <ti/drivers/ECDH.h>
59 
60 #include <ti/devices/DeviceFamily.h>
61 #include DeviceFamily_constructPath(driverlib/rom_ecc.h)
62 
63 #ifdef __cplusplus
64 extern "C" {
65 #endif
66 
73 typedef struct {
74  uint8_t dummy;
76 
82 typedef struct {
83  bool isOpen;
86  ECC_State eccState;
87  uint32_t eccWorkZone[171];
89 
90 #ifdef __cplusplus
91 }
92 #endif
93 
94 #endif /* ti_drivers_ecdh_ECDHCC26X1__include */
ECDHCC26X1 Hardware Attributes.
Definition: ECDHCC26X1.h:73
bool isOpen
Definition: ECDHCC26X1.h:83
uint8_t dummy
Definition: ECDHCC26X1.h:74
ECDH_CallbackFxn callbackFxn
Definition: ECDHCC26X1.h:84
ECDHCC26X1 Object.
Definition: ECDHCC26X1.h:82
ECDH_ReturnBehavior returnBehavior
Definition: ECDHCC26X1.h:85
void(* ECDH_CallbackFxn)(ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)
The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLB...
Definition: ECDH.h:636
ECC_State eccState
Definition: ECDHCC26X1.h:86
TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.
ECDH_ReturnBehavior
The way in which ECC function calls return after performing an encryption + authentication or decrypt...
Definition: ECDH.h:536
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale